SENSORS_XPLAINED_BOARD board header file.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
Common Sensor Service Configuration Constants | |
This module defines Common Sensor API configuration constants based upon a user-specified EXT_BOARD value. The Sensor Service determines which drivers and bus interface modules to use based upon these definitions. When EXT_BOARD defines a valid Sensors Xplained board constant, a catch-all constant named SENSORS_XPLAINED_BOARD is defined so that platform, service, and other code can be conditionally configured without testing for every particular Sensors Xplained board constant. All of the following boards are compatible with the Atmel Xplained MCU boards provided the required I/O peripheral pin mapping has been added and a call to the sensor_board_init() routine has been included in the board_init() routine.
This sensor board includes an InvenSense 3-axis gyro (ITG-3200), Bosch 3-axis accelerometer (BMA150), and AKM 3-axis magnetometer (AK8975). These sensors are interfaced via a TWI master bus mapped to pins on the J1 I/O expansion header on an Xplained development platform. When the EXT_BOARD value is set to SENSORS_XPLAINED_INERTIAL_1, the following are defined:
This sensor board includes an InvenSense 3-axis gyro (IMU-3000), Kionix 3-axis accelerometer (KXTF9), and Honeywell 3-axis magnetometer (HMC5883). These sensors are interfaced via a TWI master bus mapped to pins on the J1 I/O expansion header on an Xplained development platform. When the EXT_BOARD value is set to SENSORS_XPLAINED_INERTIAL_2, the following are defined:
This sensor board includes a Bosch barometric pressure sensor (BMP085). This sensor is interfaced via a TWI master bus mapped to pins on the J1 I/O expansion header on an Xplained development platform. When the EXT_BOARD value is set to SENSORS_XPLAINED_PRESSURE_1, the following are defined:
This sensor board includes an Osram IR light/proximity sensor (SFH7770). This sensor is interfaced via a TWI master bus mapped to pins on the J1 I/O expansion header on an Xplained development platform. When the EXT_BOARD value is set to SENSORS_XPLAINED_LIGHTPROX_1, the following are defined:
The following list summarizes available sensor service configuration constants that are specified by board configurations defined in this module. | |
#define | SENSORS_XPLAINED_BOARD |
#define | CONF_SENSOR_BUS_TWI |
#define | INCLUDE_SFH7770 |
Xplained Board J1 Connector Pin Mapping | |
These constants map AVR & AVR32 ports to pins on the Xplained board J1 connector where pins on the 10-pin header correspond to the following functions: 10-pin Header Function
-------------------------------------------
Pin 1 SDA
Pin 2 SCL
Pin 3 RXD
Pin 4 TXD
Pin 5 SS
Pin 6 MOSI
Pin 7 MISO
Pin 8 SCK
| |
#define | SENSOR_BOARD_PIN1 XPLD_HEADER_J1_PIN1 |
#define | SENSOR_BOARD_PIN2 XPLD_HEADER_J1_PIN2 |
#define | SENSOR_BOARD_PIN3 XPLD_HEADER_J1_PIN3 |
#define | SENSOR_BOARD_PIN4 XPLD_HEADER_J1_PIN4 |
#define | SENSOR_BOARD_PIN5 XPLD_HEADER_J1_PIN5 |
#define | SENSOR_BOARD_PIN6 XPLD_HEADER_J1_PIN6 |
#define | SENSOR_BOARD_PIN7 XPLD_HEADER_J1_PIN7 |
#define | SENSOR_BOARD_PIN8 XPLD_HEADER_J1_PIN8 |
#define | SENSOR_BOARD_PORT XPLD_HEADER_J1_PORT |
#define | SENSOR_BOARD_PORT_vect XPLD_HEADER_J1_INT0_vect |
Sensor Device Interrupt Routing | |
The following constants map I/O expansion header pins that are used as sensor event signal inputs to the MCU interrupt controller lines and IRQ numbers. These definitions are provided as a board-level description for the sensor drivers and are not used directly in sensor service client applications. | |
#define | INVALID_IRQ_NUMBER ((unsigned int) -1) |
#define | SENSOR_PIN1_IRQ (AVR32_GPIO_IRQ_0 + (SENSOR_BOARD_PIN1 / 8)) |
#define | SENSOR_PIN2_IRQ (AVR32_GPIO_IRQ_0 + (SENSOR_BOARD_PIN2 / 8)) |
#define | SENSOR_PIN3_IRQ (AVR32_GPIO_IRQ_0 + (SENSOR_BOARD_PIN3 / 8)) |
#define | SENSOR_PIN4_IRQ (AVR32_GPIO_IRQ_0 + (SENSOR_BOARD_PIN4 / 8)) |
#define | SENSOR_PIN5_IRQ (AVR32_GPIO_IRQ_0 + (SENSOR_BOARD_PIN5 / 8)) |
#define | SENSOR_PIN6_IRQ (AVR32_GPIO_IRQ_0 + (SENSOR_BOARD_PIN6 / 8)) |
#define | SENSOR_PIN7_IRQ (AVR32_GPIO_IRQ_0 + (SENSOR_BOARD_PIN7 / 8)) |
#define | SENSOR_PIN8_IRQ (AVR32_GPIO_IRQ_0 + (SENSOR_BOARD_PIN8 / 8)) |
Sensor Device I/O Pins | |
The following constants specify I/O expansion header pins that are used as sensor event signal inputs to the MCU and, in some cases, control signal outputs from the MCU to the sensor device. For example, the These definitions are provided as a board-level description for the sensor drivers and are not used directly in sensor service client applications. | |
#define | sfh7770_sigint (SENSOR_BOARD_PIN3) |
#define | sfh7770_sigout (INVALID_PIN_NUMBER) |
Sensor Physical Orientation | |
The following constants describe the physical orientation of multi-axis sensor devices, relative to the standardized axes of the sensors API. This allows for devices to be mounted in different configurations but provide consistent output to applications in terms of each axis. For each sensor device, the orientation description consists of a set of three values in X, Y, Z order, which specify which sensor axis and sign corresponds to the standard axis positive direction. These definitions are provided as a board-level description for the sensor drivers and are not used directly in sensor service client applications. | |
#define | NON_DIRECTIONAL_DEV {AXIS_NONE, AXIS_NONE, AXIS_NONE} |
#define | sfh7770_orientation NON_DIRECTIONAL_DEV |
Typedefs | |
typedef void(* | SENSOR_IRQ_HANDLER )(volatile void *) |
Sensor Pin Interrupt Handler Callback Type. More... | |
Functions | |
void | sensor_board_init (void) |
Initialize sensor board target resources. More... | |
bool | sensor_board_irq_connect (uint32_t gpio_pin, SENSOR_IRQ_HANDLER handler, void *arg) |
Install a sensor interrupt handler. More... | |