Cyclic Redundancy Check module driver.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | CRC_APP NVM_CMD_APP_CRC_gc |
Perform a CRC calculation on the boot loader section. More... | |
#define | CRC_BOOT NVM_CMD_BOOT_CRC_gc |
Perform a CRC calculation on the application section. More... | |
#define | CRC_FLASH_RANGE NVM_CMD_FLASH_RANGE_CRC_gc |
Perform a CRC calculation on an address range in flash. More... | |
Enumerations | |
enum | crc_16_32_t { CRC_16BIT, CRC_32BIT } |
Flag to indicate whether DMA is supported. More... | |
Functions | |
void | crc16_append_value (uint16_t value, void *ptr) |
Appends a CRC value to the given pointer. More... | |
void | crc32_append_value (uint32_t value, void *ptr) |
Get and append data to generate checksum zero with CRC32. More... | |
uint32_t | crc_flash_checksum (NVM_CMD_t crc_type, flash_addr_t flash_addr, uint32_t len) |
Perform a CRC-32 calculation on the entire flash memory, on only the application section, on only the boot section, or on a selectable range of the flash memory. More... | |
uint32_t | crc_io_checksum (void *data, uint16_t len, enum crc_16_32_t crc_16_32) |
Calculate the CRC checksum for data in a buffer. More... | |
void | crc_io_checksum_byte_add (uint8_t data) |
Add one byte of data to CRC performed on I/O interface. More... | |
void | crc_io_checksum_byte_start (enum crc_16_32_t crc_16_32) |
Reset CRC module and set source to I/O interface. More... | |
uint32_t | crc_io_checksum_byte_stop (void) |
Disable CRC module and return checksum. More... | |
void | crc_set_initial_value (uint32_t value) |
Set initial CRC value for next CRC calculation. More... | |