Functions | |
void | reader_txt_beg (void) |
This function goes at the beginning of file and read the text header. More... | |
void | reader_txt_close (void) |
Close text file. More... | |
uint16_t | reader_txt_get_line (bool b_unicode, FS_STRING string, uint16_t u16_str_size) |
This function fills an ASCII buffer with the current text line of opened file. More... | |
bool | reader_txt_jump_line (uint16_t nb_line) |
This function jumps text lines. More... | |
bool | reader_txt_new (const FS_STRING sz_name, uint8_t u8_txt_format) |
Create a new text file. More... | |
bool | reader_txt_open (bool b_readonly) |
Open a selected text file in the current navigator. More... | |
void | reader_txt_select_format (uint8_t u8_txt_format) |
This function allow to select the text format to decode. More... | |
void reader_txt_beg | ( | void | ) |
This function goes at the beginning of file and read the text header.
References file_read_buf(), file_seek(), fs_g_nav_entry, FS_SEEK_SET, Fs_management_entry::u8_txt_format, UNI_MAX_HEADER_SIZE, unicode_header_get(), and unicode_header_scan().
Referenced by pl_main_open(), pl_nav_readentry(), pl_nav_setpos(), and reader_txt_open().
void reader_txt_close | ( | void | ) |
Close text file.
References file_close().
This function fills an ASCII buffer with the current text line of opened file.
@param b_unicode true to return a unicode string (UTF16), ASCII otherwise over there @param string string used to store text line @param u16_str_size maximum size of string (unit character, 1B for ASCII, 2B for unicode) @return size of the line (may be < or > at u16_str_size) @return 0, in case of error
//! This routine remove the character '\n' '\r' //!
References file_eof(), file_getc(), file_read_buf(), file_seek(), FS_EOF, FS_ERR_EOF, fs_g_nav_entry, fs_g_status, FS_SEEK_CUR_RE, LSB, MSB, nav_checkdisk_disable(), nav_checkdisk_enable(), Fs_management_entry::u8_txt_format, UNI_MAX_UTF8_SIZE, UNI_TYPE_UTF16BE, UNI_TYPE_UTF16LE, UNI_TYPE_UTF8, and utf8_to_unicode().
Referenced by pl_main_readline(), reader_id3_read_string(), and reader_txt_jump_line().
bool reader_txt_jump_line | ( | uint16_t | nb_line | ) |
This function jumps text lines.
nb_line | number of lines to jump |
References file_eof(), and reader_txt_get_line().
Create a new text file.
sz_name | contains the file name (ASCII or UNICODE ) |
u8_txt_format | text format to use (UNI_TYPE_UTF8, UNI_TYPE_UTF16BE, UNI_TYPE_UTF16LE, UNI_TYPE_ASCII) |
References file_write_buf(), fs_g_nav_entry, nav_file_create(), Fs_management_entry::u8_txt_format, UNI_MAX_HEADER_SIZE, and unicode_header_get().
Open a selected text file in the current navigator.
b_readonly | true to open the text file in read only access |
References file_open(), FOPEN_MODE_R, FOPEN_MODE_R_PLUS, and reader_txt_beg().
Referenced by pl_main_open().
void reader_txt_select_format | ( | uint8_t | u8_txt_format | ) |
This function allow to select the text format to decode.
u8_txt_format | text format selected (UNI_TYPE_UTF8, UNI_TYPE_UTF16BE, UNI_TYPE_UTF16LE, UNI_TYPE_ASCII) |
References fs_g_nav_entry, and Fs_management_entry::u8_txt_format.
Referenced by reader_id3_read_string().