#include "conf_access.h"
#include <stdio.h>
#include "gpio.h"
#include "mci.h"
#include "conf_sd_mmc_mci.h"
#include "sd_mmc_mci.h"
#include "cycle_counter.h"
Macros | |
#define | SDMMC_SWITCH_FUNC_G1_KEEP (0xf << 0) |
#define | SDMMC_SWITCH_FUNC_G2_KEEP (0xf << 4) |
#define | SDMMC_SWITCH_FUNC_G3_KEEP (0xf << 8) |
#define | SDMMC_SWITCH_FUNC_G4_KEEP (0xf << 12) |
#define | SDMMC_SWITCH_FUNC_G5_KEEP (0xf << 16) |
#define | SDMMC_SWITCH_FUNC_G6_KEEP (0xf << 20) |
#define | SDMMC_SWITCH_FUNC_HIGH_SPEED (1 << 0) |
#define | SDMMC_SWITCH_FUNC_MODE_CHECK (0 << 31) |
#define | SDMMC_SWITCH_FUNC_MODE_SWITCH (1 << 31) |
Functions | |
bool | is_sd_mmc_mci_card_present (uint8_t slot) |
Performs a card check presence. More... | |
bool | is_sd_mmc_mci_card_protected (uint8_t slot) |
Performs a card check protection. More... | |
static bool | sd_mmc_get_ext_csd (uint8_t slot) |
bool | sd_mmc_mci_card_init (unsigned char slot) |
Initializes the SD/MMC card. More... | |
bool | sd_mmc_mci_cmd_send_status (uint8_t slot) |
ask mmc status register. More... | |
bool | sd_mmc_mci_dma_read_multiple_sector_2_ram (uint8_t slot, void *ram, uint32_t nb_sector) |
Reads nb_sector SD/MMC sector to a RAM buffer, using the DMA. More... | |
bool | sd_mmc_mci_dma_read_open (uint8_t slot, uint32_t pos, void *ram, uint16_t nb_sector) |
Opens a DF memory in read mode at a given sector. DMA will be used. More... | |
bool | sd_mmc_mci_dma_read_sector_2_ram (uint8_t slot, void *ram) |
Reads 1 SD/MMC sector to a RAM buffer, using the DMA. More... | |
bool | sd_mmc_mci_dma_write_multiple_sector_from_ram (uint8_t slot, const void *ram, uint32_t nb_sector) |
Writes nb_sector SD/MMC sector from a RAM buffer, using the DMA. More... | |
bool | sd_mmc_mci_dma_write_open (uint8_t slot, uint32_t pos, const void *ram, uint16_t nb_sector) |
This function opens a DF memory in write mode at a given sector. DMA will be used. More... | |
bool | sd_mmc_mci_dma_write_sector_from_ram (uint8_t slot, const void *ram) |
Writes 1 SD/MMC sector from a RAM buffer, using the DMA. More... | |
static bool | sd_mmc_mci_get_csd (uint8_t slot) |
bool | sd_mmc_mci_init (unsigned char card_slot, long pbb_hz, long cpu_hz) |
Initializes the MCI driver. More... | |
bool | sd_mmc_mci_mem_check (uint8_t slot) |
Performs a memory check. More... | |
bool | sd_mmc_mci_read_close (uint8_t slot) |
Unselects the current DF memory. More... | |
bool | sd_mmc_mci_read_multiple_sector_2_ram (uint8_t slot, void *ram, uint32_t nb_sector) |
Reads nb_sector SD/MMC sector to a RAM buffer. More... | |
bool | sd_mmc_mci_read_open (uint8_t slot, uint32_t pos, uint16_t nb_sector) |
Opens a DF memory in read mode at a given sector. More... | |
bool | sd_mmc_mci_read_sector_2_ram (uint8_t slot, void *ram) |
Reads 1 SD/MMC sector to a RAM buffer. More... | |
bool | sd_mmc_mci_write_close (uint8_t slot) |
Fills the end of the current logical sector and launches page programming. More... | |
bool | sd_mmc_mci_write_multiple_sector_from_ram (uint8_t slot, const void *ram, uint32_t nb_sector) |
Writes nb_sector SD/MMC sector from a RAM buffer. More... | |
bool | sd_mmc_mci_write_open (uint8_t slot, uint32_t pos, uint16_t nb_sector) |
This function opens a DF memory in write mode at a given sector. More... | |
bool | sd_mmc_mci_write_sector_from_ram (uint8_t slot, const void *ram) |
Writes 1 SD/MMC sector from a RAM buffer. More... | |
static bool | sd_mmc_set_block_len (uint8_t slot, uint16_t length) |
Variables | |
uint8_t | g_card_bus_width [MCI_NR_SLOTS] |
uint16_t | g_card_freq [MCI_NR_SLOTS] |
uint32_t | g_card_rca [MCI_NR_SLOTS] |
uint32_t | g_card_size [MCI_NR_SLOTS] |
SD/MMC Card Size per Slot. More... | |
uint8_t | g_card_type [MCI_NR_SLOTS] |
static uint32_t | g_cpu_hz = 0 |
static uint32_t | g_pbb_hz = 0 |
volatile uint32_t | gl_ptr_mem [MCI_NR_SLOTS] ={0, 0} |
volatile avr32_mci_t * | mci = &AVR32_MCI |
bool | sd_mmc_mci_init_done [MCI_NR_SLOTS] = {false, false} |
Initialization sequence status per Slot. More... | |
COMPILER_WORD_ALIGNED uint8_t | sector_buf_0 [SD_MMC_SECTOR_SIZE] |
COMPILER_WORD_ALIGNED uint8_t | sector_buf_1 [SD_MMC_SECTOR_SIZE] |
#define SDMMC_SWITCH_FUNC_G1_KEEP (0xf << 0) |
#define SDMMC_SWITCH_FUNC_G2_KEEP (0xf << 4) |
Referenced by sd_mmc_mci_card_init().
#define SDMMC_SWITCH_FUNC_G3_KEEP (0xf << 8) |
Referenced by sd_mmc_mci_card_init().
#define SDMMC_SWITCH_FUNC_G4_KEEP (0xf << 12) |
Referenced by sd_mmc_mci_card_init().
#define SDMMC_SWITCH_FUNC_G5_KEEP (0xf << 16) |
Referenced by sd_mmc_mci_card_init().
#define SDMMC_SWITCH_FUNC_G6_KEEP (0xf << 20) |
Referenced by sd_mmc_mci_card_init().
#define SDMMC_SWITCH_FUNC_HIGH_SPEED (1 << 0) |
Referenced by sd_mmc_mci_card_init().
#define SDMMC_SWITCH_FUNC_MODE_CHECK (0 << 31) |
Referenced by sd_mmc_mci_card_init().
#define SDMMC_SWITCH_FUNC_MODE_SWITCH (1 << 31) |
Referenced by sd_mmc_mci_card_init().
|
static |
References g_card_bus_width, g_card_freq, g_card_size, g_card_type, mci, MCI_LAST_SLOTS, mci_rd_data(), mci_rx_ready(), mci_select_card(), mci_send_cmd(), mci_set_block_count(), mci_set_block_size(), MCI_SUCCESS, MMC_CARD_HC, MSB0, SD_MMC_SECTOR_SIZE, SD_MMC_SEND_EXT_CSD_CMD, swap32, and val.
Referenced by sd_mmc_mci_card_init().
|
static |
References csd_t::csd, CSD_BLEN_512, CSD_MSK_SPEC_VER, CSD_SPEC_VER_4_0, csd_t::csd_v1, csd_t::csd_v2, csd_v1_t::cSizeMult, csd_v1_t::deviceSizeH, csd_v2_t::deviceSizeH, csd_v1_t::deviceSizeL, csd_v2_t::deviceSizeL, g_card_bus_width, g_card_freq, g_card_rca, g_card_size, g_card_type, mci, MCI_LAST_SLOTS, mci_read_response(), mci_select_card(), mci_send_cmd(), MCI_SUCCESS, MMC_CARD, MMC_CARD_V4, MSB0, csd_v1_t::readBlLen, SD_CARD, SD_CARD_HC, SD_MMC_SEND_CSD_CMD, csd_v1_t::tranSpeed, and csd_v1_t::writeBlLen.
Referenced by sd_mmc_mci_card_init().
|
static |
References g_card_bus_width, mci, MCI_LAST_SLOTS, mci_read_response(), mci_select_card(), mci_send_cmd(), mci_set_block_count(), mci_set_block_size(), MCI_SUCCESS, MMC_TRAN_STATE, MMC_TRAN_STATE_MSK, and SD_MMC_SET_BLOCKLEN_CMD.
Referenced by sd_mmc_mci_card_init().
uint8_t g_card_bus_width[MCI_NR_SLOTS] |
uint16_t g_card_freq[MCI_NR_SLOTS] |
Referenced by sd_mmc_get_ext_csd(), sd_mmc_mci_card_init(), and sd_mmc_mci_get_csd().
uint32_t g_card_rca[MCI_NR_SLOTS] |
uint32_t g_card_size[MCI_NR_SLOTS] |
SD/MMC Card Size per Slot.
Referenced by sd_mmc_get_ext_csd(), sd_mmc_mci_get_csd(), and sd_mmc_mci_read_capacity().
uint8_t g_card_type[MCI_NR_SLOTS] |
|
static |
|
static |
Referenced by sd_mmc_mci_card_init(), and sd_mmc_mci_init().
volatile uint32_t gl_ptr_mem[MCI_NR_SLOTS] ={0, 0} |
Referenced by sd_mmc_mci_dma_read_open(), sd_mmc_mci_dma_write_open(), sd_mmc_mci_read_open(), and sd_mmc_mci_write_open().
volatile avr32_mci_t* mci = &AVR32_MCI |
Referenced by sd_mmc_get_ext_csd(), sd_mmc_mci_card_init(), sd_mmc_mci_cmd_send_status(), sd_mmc_mci_dma_read_open(), sd_mmc_mci_dma_write_open(), sd_mmc_mci_get_csd(), sd_mmc_mci_init(), sd_mmc_mci_mem_check(), sd_mmc_mci_read_close(), sd_mmc_mci_read_multiple_sector_2_ram(), sd_mmc_mci_read_open(), sd_mmc_mci_read_sector_2_ram(), sd_mmc_mci_write_close(), sd_mmc_mci_write_multiple_sector_from_ram(), sd_mmc_mci_write_open(), sd_mmc_mci_write_sector_from_ram(), and sd_mmc_set_block_len().
bool sd_mmc_mci_init_done[MCI_NR_SLOTS] = {false, false} |
Initialization sequence status per Slot.
Referenced by sd_mmc_mci_card_init(), sd_mmc_mci_mem_check(), and sd_mmc_mci_test_unit_ready().
COMPILER_WORD_ALIGNED uint8_t sector_buf_0[SD_MMC_SECTOR_SIZE] |
COMPILER_WORD_ALIGNED uint8_t sector_buf_1[SD_MMC_SECTOR_SIZE] |