|
Ctrl_status | sd_mmc_spi_mem_2_ram (uint32_t addr, void *ram) |
| This function reads 1 sector from SD/MMC to internal ram buffer. More...
|
|
void | sd_mmc_spi_mem_init (void) |
| This function initializes the hw/sw resources required to drive the SD_MMC_SPI. More...
|
|
Ctrl_status | sd_mmc_spi_ram_2_mem (uint32_t addr, const void *ram) |
| This function initializes the memory for a write operation from ram buffer to SD/MMC (1 sector) More...
|
|
Ctrl_status | sd_mmc_spi_read_capacity (uint32_t *nb_sector) |
| This function gives the address of the last valid sector. More...
|
|
bool | sd_mmc_spi_removal (void) |
| This function tells if the memory has been removed or not. More...
|
|
Ctrl_status | sd_mmc_spi_test_unit_ready (void) |
| This function tests the state of the SD_MMC memory and sends it to the Host. More...
|
|
bool | sd_mmc_spi_wr_protect (void) |
| This function returns the write protected status of the memory. More...
|
|