Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Modules
Here is a list of all modules:
[detail level 123]
oFAT file systemFAT file system driver that provides an interface for accessing a FAT file system located on a memory device
oMemory Control AccessCommon abstraction layer for memory interfaces
oUSB task entry point module
|oUSB software Events ManagementMacros to manage USB events detected under interrupt
|\Standard requests defines
oUSBB low-level driver moduleUSBB low-level driver module
|oUSBB endpointsIdentifiers of USBB endpoints (USBB device operating mode)
|oUSBB pipesIdentifiers of USBB pipes (USBB host operating mode)
|oUSBB standard typesList of the standard types used in USBB
|oUSBB IP propertiesThese macros give access to IP properties
|oUSBB common management driversThese macros manage the USBB controller
|oUSBB device controller driversThese macros manage the USBB Device controller
|oUSBB endpoint driversThese macros manage the common features of the endpoints
|oUSBB endpoint DMA driversThese macros manage the common features of the endpoint DMA channels
|oUSBB host controller driversThese macros manage the USBB Host controller
|oUSBB pipe driversThese macros manage the common features of the pipes
|\USBB pipe DMA driversThese macros manage the common features of the pipe DMA channels
oCompiler abstraction layer and code utilitiesCompiler abstraction layer and code utilities for 32-bit AVR
|oPreprocessor - Macro Repeat
|oPreprocessor - Stringize
|oPreprocessor - Token Paste
|\Status Codes
oAtmel part identification macrosThis collection of macros identify which series and families that the various Atmel parts belong to
|oAVR UC3 parts
|oAVR XMEGA parts
|omegaAVR parts
|\SAM parts
oGlobal interrupt managementThis is a driver for global enabling and disabling of interrupts
|\Deprecated interrupt definitions
oINTC Software Driver API for AVR UC3This is a software module to register interrupt handlers at any specified interrupt level to any interrupt line managed by the INTC module in AVR UC3 devices
oCPU - PM - Power ManagerThe Power Manager (PM) controls the oscillators and PLLs, and generates the clocks and resets in the device
|\Power Clocks Library
oPower Manager (PM)This is a stub on the AVR UC3 Power Manager(PM) for the sleepmgr service
oMEMORY - FLASHC - Flash ControllerFLASHC interfaces a flash block with the 32-bit internal HSB bus
oCPU - Cycle CounterCPU Cycle Counter provides an interface to the COUNT and COMPARE registers
oWDT - Watchdog TimerDriver for the Watchdog Timer
oDLMALLOC - Dynamic memory allocationDlmalloc is a version of malloc/free/realloc, which offers memory administration functionallity
oFeatures
oCompilation
oMain Files
oGetting Started
oSupported Device List
oAUDIO - TLV320AIC23B Audio CodecSoftware Driver for the TLV320AIC23B Audio Codec
oGPIO - General-Purpose Input/OutputGPIO gives access to the MCU pins
oUC3 Peripheral DMA ControllerThe Peripheral DMA controller (PDCA) transfers data between on-chip peripheral modules such as USART, SPI, SSC and on- and off-chip memories
oSSC - Synchronous Serial Controller (I2S)Driver for the I2S protocol using the SSC (Synchronous Serial Controller)
oAUDIO - Mono Audio PWM DACMono Audio DAC implemented with a PWM hardware module
oAUDIO - TPA6130A2 Audio AmplifierSoftware Driver for the TPA6130A2 Audio Amplifier
oTWI - Two-Wire InterfaceDriver for the TWI (Two-Wire Interface)
oAUDIO - ABDAC - Audio Bitstream DACAudio Bitstream DAC (Digital to Analog Converter) provides functions to convert a 16-bit sample value to a digital bitstream
oTOUCH - QT1081 QTouch sensorThe QT1081 sensor is operated by GPIOs and this driver provides a wrapper for the GPIO accesses
oDISPLAY - LCD Display - ET024006DHUThe ET024006DHU is a RGB LCD display from EDT and it offers a resolution of 240x320 pixels
oMEMORY - EBI Static Memory ControllerEBI (External Bus Interface) SMC (Static Memory Controller) allows to connect a Static Memory to the microcontroller
oAT45DBX DataFlash (from ASF ver. 1)Driver for the AT45dbX series SPI DataFlash memories (from ASF V1)
oSPI - Serial Peripheral InterfaceSee Quick start guide for SPI driver on AVR32 devices
oMEMORY - SDRAM MT48LC16M16A2TG7EThis a configuration for the MT48LC16M16A2TG7E SDRAM from Mircon
oMEMORY - EBI SDRAM ControllerEBI (External Bus Interface) SDRAM Controller allows to connect a SDRAM to the microcontroller
oUSB host enumeration functions module
oUSB host task module
|\Host controller statesDefines for device state coding
oUSB application configuration
|oUSB host operating mode configuration
||oUSB host custom actions
||\USB device operating mode configuration
|\USB stream control parametersDefines the way the USB stream control will operate
oMEMORY - SD/MMC card access using SPIDriver for SD (Secure Digital) / MMC (MultiMedia Card) access using SPI (Serial Peripheral Interface)
|\SD/MMC SPI Memory
\Generic board supportThe generic board support module includes board-specific definitions and function prototypes, such as the board initialization function