These macros manage the USBB controller.
Macros | |
#define | Is_usb_bconnection_error_interrupt() (Tst_bits(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_BCERRI_MASK)) |
tests if a B-device connection error occurs More... | |
#define | Is_usb_bconnection_error_interrupt_enabled() (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_BCERRE_MASK)) |
#define | Is_usb_clock_frozen() (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_FRZCLK_MASK)) |
#define | Is_usb_data_srp_method_selected() (!Is_usb_vbus_srp_method_selected()) |
#define | Is_usb_device_mode_forced() (!Is_usb_id_pin_enabled() && Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_UIMOD_MASK)) |
Test if device mode is forced. More... | |
#define | Is_usb_device_srp() (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_SRPREQ_MASK)) |
tests if a SRP from device occurs More... | |
#define | Is_usb_enabled() (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_USBE_MASK)) |
#define | Is_usb_full_speed_mode() (Rd_bitfield(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_SPEED_MASK) == AVR32_USBB_USBSTA_SPEED_FULL) |
Test if controller is in full speed mode. More... | |
#define | Is_usb_full_speed_mode_used() (!Is_usb_low_speed_mode_forced()) |
Test if device full speed mode is used. More... | |
#define | Is_usb_hnp() (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_HNPREQ_MASK)) |
tests if a HNP occurs More... | |
#define | Is_usb_hnp_error_interrupt() (Tst_bits(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_HNPERRI_MASK)) |
tests if a HNP error occurs More... | |
#define | Is_usb_hnp_error_interrupt_enabled() (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_HNPERRE_MASK)) |
#define | Is_usb_host_mode_forced() (!Is_usb_id_pin_enabled() && !Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_UIMOD_MASK)) |
Test if host mode is forced. More... | |
#define | Is_usb_id_device() (Tst_bits(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_ID_MASK)) |
#define | Is_usb_id_interrupt_enabled() (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_IDTE_MASK)) |
#define | Is_usb_id_pin_enabled() (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_UIDE_MASK)) |
Test if external USB_ID pin enabled (listened to by USB) More... | |
#define | Is_usb_id_transition() (Tst_bits(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_IDTI_MASK)) |
#define | Is_usb_low_speed_mode() (Rd_bitfield(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_SPEED_MASK) == AVR32_USBB_USBSTA_SPEED_LOW) |
Test if controller is in low-speed mode. More... | |
#define | Is_usb_low_speed_mode_forced() (Tst_bits(AVR32_USBB_udcon, AVR32_USBB_UDCON_LS_MASK)) |
Test if device low-speed mode is forced. More... | |
#define | Is_usb_otg_pad_enabled() (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_OTGPADE_MASK)) |
#define | Is_usb_role_exchange_interrupt() (Tst_bits(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_ROLEEXI_MASK)) |
tests if a role exchange occurs More... | |
#define | Is_usb_role_exchange_interrupt_enabled() (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_ROLEEXE_MASK)) |
#define | Is_usb_srp_interrupt() (Tst_bits(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_SRPI_MASK)) |
tests if a SRP occurs More... | |
#define | Is_usb_srp_interrupt_enabled() (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_SRPE_MASK)) |
#define | Is_usb_suspend_time_out_interrupt() (Tst_bits(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_STOI_MASK)) |
tests if a suspend time out occurs More... | |
#define | Is_usb_suspend_time_out_interrupt_enabled() (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_STOE_MASK)) |
#define | Is_usb_vbof_active_high() (!Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_VBUSPO_MASK)) |
Get USB_VBOF output pin polarity. More... | |
#define | Is_usb_vbof_active_low() (!Is_usb_vbof_active_high()) |
#define | Is_usb_vbof_pin_output() |
Test if USB_VBOF is output onto its pin. More... | |
#define | Is_usb_vbus_enabled() (Tst_bits(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_VBUSRQ_MASK)) |
tests if VBus activation has been requested More... | |
#define | Is_usb_vbus_error_interrupt() (Tst_bits(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_VBERRI_MASK)) |
tests if a VBus error occurs More... | |
#define | Is_usb_vbus_error_interrupt_enabled() (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_VBERRE_MASK)) |
#define | Is_usb_vbus_high() (Tst_bits(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_VBUS_MASK)) |
#define | Is_usb_vbus_hw_control_enabled() (!Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_VBUSHWC_MASK)) |
#define | Is_usb_vbus_interrupt_enabled() (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_VBUSTE_MASK)) |
#define | Is_usb_vbus_low() (!Is_usb_vbus_high()) |
#define | Is_usb_vbus_srp_method_selected() (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_SRPSEL_MASK)) |
#define | Is_usb_vbus_transition() (Tst_bits(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_VBUSTI_MASK)) |
#define | Usb_ack_bconnection_error_interrupt() (AVR32_USBB_usbstaclr = AVR32_USBB_USBSTACLR_BCERRIC_MASK) |
acks B-device connection error interrupt More... | |
#define | Usb_ack_hnp_error_interrupt() (AVR32_USBB_usbstaclr = AVR32_USBB_USBSTACLR_HNPERRIC_MASK) |
acks HNP error interrupt More... | |
#define | Usb_ack_id_transition() (AVR32_USBB_usbstaclr = AVR32_USBB_USBSTACLR_IDTIC_MASK) |
#define | Usb_ack_role_exchange_interrupt() (AVR32_USBB_usbstaclr = AVR32_USBB_USBSTACLR_ROLEEXIC_MASK) |
acks role exchange interrupt More... | |
#define | Usb_ack_srp_interrupt() (AVR32_USBB_usbstaclr = AVR32_USBB_USBSTACLR_SRPIC_MASK) |
acks SRP interrupt More... | |
#define | Usb_ack_suspend_time_out_interrupt() (AVR32_USBB_usbstaclr = AVR32_USBB_USBSTACLR_STOIC_MASK) |
acks suspend time out interrupt More... | |
#define | Usb_ack_vbus_error_interrupt() (AVR32_USBB_usbstaclr = AVR32_USBB_USBSTACLR_VBERRIC_MASK) |
acks VBus error interrupt More... | |
#define | Usb_ack_vbus_transition() (AVR32_USBB_usbstaclr = AVR32_USBB_USBSTACLR_VBUSTIC_MASK) |
#define | Usb_configure_timeout(timer, timeout) |
Configure time-out of specified OTG timer. More... | |
#define | Usb_device_initiate_hnp() (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_HNPREQ_MASK)) |
initiates a Host negotiation Protocol More... | |
#define | Usb_device_initiate_srp() (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_SRPREQ_MASK)) |
initiates a Session Request Protocol More... | |
#define | Usb_disable() (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_USBE_MASK)) |
Disable USB macro. More... | |
#define | Usb_disable_bconnection_error_interrupt() (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_BCERRE_MASK)) |
disables B-device connection error interrupt More... | |
#define | Usb_disable_hnp_error_interrupt() (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_HNPERRE_MASK)) |
disables HNP error interrupt More... | |
#define | Usb_disable_id_interrupt() (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_IDTE_MASK)) |
#define | Usb_disable_id_pin() (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_UIDE_MASK)) |
Disable external USB_ID pin (ignored by USB) More... | |
#define | Usb_disable_otg_pad() (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_OTGPADE_MASK)) |
Disable OTG pad. More... | |
#define | Usb_disable_role_exchange_interrupt() (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_ROLEEXE_MASK)) |
disables role exchange interrupt More... | |
#define | Usb_disable_srp_interrupt() (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_SRPE_MASK)) |
disables SRP interrupt More... | |
#define | Usb_disable_suspend_time_out_interrupt() (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_STOE_MASK)) |
disables suspend time out interrupt More... | |
#define | Usb_disable_vbus() (AVR32_USBB_usbstaclr = AVR32_USBB_USBSTACLR_VBUSRQC_MASK) |
requests VBus deactivation More... | |
#define | Usb_disable_vbus_error_interrupt() (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_VBERRE_MASK)) |
disables VBus error interrupt More... | |
#define | Usb_disable_vbus_hw_control() (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_VBUSHWC_MASK)) |
disables hardware control over the USB_VBOF output pin More... | |
#define | Usb_disable_vbus_interrupt() (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_VBUSTE_MASK)) |
#define | Usb_enable() (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_USBE_MASK)) |
Enable USB macro. More... | |
#define | Usb_enable_bconnection_error_interrupt() (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_BCERRE_MASK)) |
enables B-device connection error interrupt More... | |
#define | Usb_enable_hnp_error_interrupt() (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_HNPERRE_MASK)) |
enables HNP error interrupt More... | |
#define | Usb_enable_id_interrupt() (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_IDTE_MASK)) |
#define | Usb_enable_id_pin() (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_UIDE_MASK)) |
Enable external USB_ID pin (listened to by USB) More... | |
#define | Usb_enable_otg_pad() (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_OTGPADE_MASK)) |
Enable OTG pad. More... | |
#define | Usb_enable_role_exchange_interrupt() (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_ROLEEXE_MASK)) |
enables role exchange interrupt More... | |
#define | Usb_enable_srp_interrupt() (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_SRPE_MASK)) |
enables SRP interrupt More... | |
#define | Usb_enable_suspend_time_out_interrupt() (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_STOE_MASK)) |
enables suspend time out interrupt More... | |
#define | Usb_enable_vbus() (AVR32_USBB_usbstaset = AVR32_USBB_USBSTASET_VBUSRQS_MASK) |
requests VBus activation More... | |
#define | Usb_enable_vbus_error_interrupt() (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_VBERRE_MASK)) |
enables VBus error interrupt More... | |
#define | Usb_enable_vbus_hw_control() (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_VBUSHWC_MASK)) |
enables hardware control over the USB_VBOF output pin More... | |
#define | Usb_enable_vbus_interrupt() (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_VBUSTE_MASK)) |
#define | Usb_force_device_mode() (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_UIMOD_MASK), Usb_disable_id_pin()) |
Disable external USB_ID pin and force device mode. More... | |
#define | Usb_force_full_speed_mode() do { } while (0) |
#define | Usb_force_host_mode() (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_UIMOD_MASK), Usb_disable_id_pin()) |
Disable external USB_ID pin and force host mode. More... | |
#define | Usb_force_low_speed_mode() (Set_bits(AVR32_USBB_udcon, AVR32_USBB_UDCON_LS_MASK)) |
Force device low-speed mode. More... | |
#define | Usb_freeze_clock() (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_FRZCLK_MASK)) |
Stop (freeze) internal USB clock. More... | |
#define | Usb_get_fsm_drd_state() (Rd_bitfield(AVR32_USBB_usbfsm, AVR32_USBB_USBFSM_DRDSTATE_MASK)) |
Get the dual-role device state of the internal USB finite state machine of the USBB controller. More... | |
#define | Usb_get_timeout(timer) |
Get configured time-out of specified OTG timer. More... | |
#define | Usb_host_accept_hnp() (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_HNPREQ_MASK)) |
accepts a Host negotiation Protocol More... | |
#define | Usb_host_reject_hnp() (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_HNPREQ_MASK)) |
rejects a Host negotiation Protocol More... | |
#define | Usb_output_vbof_pin() |
Output USB_VBOF onto its pin. More... | |
#define | Usb_raise_bconnection_error_interrupt() (AVR32_USBB_usbstaset = AVR32_USBB_USBSTASET_BCERRIS_MASK) |
raises B-device connection error interrupt More... | |
#define | Usb_raise_hnp_error_interrupt() (AVR32_USBB_usbstaset = AVR32_USBB_USBSTASET_HNPERRIS_MASK) |
raises HNP error interrupt More... | |
#define | Usb_raise_id_transition() (AVR32_USBB_usbstaset = AVR32_USBB_USBSTASET_IDTIS_MASK) |
#define | Usb_raise_role_exchange_interrupt() (AVR32_USBB_usbstaset = AVR32_USBB_USBSTASET_ROLEEXIS_MASK) |
raises role exchange interrupt More... | |
#define | Usb_raise_srp_interrupt() (AVR32_USBB_usbstaset = AVR32_USBB_USBSTASET_SRPIS_MASK) |
raises SRP interrupt More... | |
#define | Usb_raise_suspend_time_out_interrupt() (AVR32_USBB_usbstaset = AVR32_USBB_USBSTASET_STOIS_MASK) |
raises suspend time out interrupt More... | |
#define | Usb_raise_vbus_error_interrupt() (AVR32_USBB_usbstaset = AVR32_USBB_USBSTASET_VBERRIS_MASK) |
raises VBus error interrupt More... | |
#define | Usb_raise_vbus_transition() (AVR32_USBB_usbstaset = AVR32_USBB_USBSTASET_VBUSTIS_MASK) |
#define | Usb_select_data_srp_method() (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_SRPSEL_MASK)) |
selects data line as SRP method More... | |
#define | Usb_select_vbus_srp_method() (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_SRPSEL_MASK)) |
selects VBus as SRP method More... | |
#define | Usb_set_vbof_active_high() (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_VBUSPO_MASK)) |
Set USB_VBOF output pin polarity. More... | |
#define | Usb_set_vbof_active_low() (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_VBUSPO_MASK)) |
#define | Usb_unfreeze_clock() (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_FRZCLK_MASK)) |
#define | Usb_use_dual_speed_mode() do { } while (0) |
#define | Usb_use_full_speed_mode() (Clr_bits(AVR32_USBB_udcon, AVR32_USBB_UDCON_LS_MASK)) |
Use device full speed mode (default) More... | |
#define | USB_VBOF_FUNCTION ATPASTE2(USB_VBOF, _FUNCTION) |
#define | USB_VBOF_PIN ATPASTE2(USB_VBOF, _PIN) |
Check that multiplexed pin used for USB_VBOF is defined. More... | |
#define Is_usb_bconnection_error_interrupt | ( | ) | (Tst_bits(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_BCERRI_MASK)) |
tests if a B-device connection error occurs
Referenced by usb_host_task().
#define Is_usb_bconnection_error_interrupt_enabled | ( | ) | (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_BCERRE_MASK)) |
#define Is_usb_clock_frozen | ( | ) | (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_FRZCLK_MASK)) |
Referenced by usb_host_task(), and usb_host_task_init().
#define Is_usb_data_srp_method_selected | ( | ) | (!Is_usb_vbus_srp_method_selected()) |
#define Is_usb_device_mode_forced | ( | ) | (!Is_usb_id_pin_enabled() && Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_UIMOD_MASK)) |
Test if device mode is forced.
#define Is_usb_device_srp | ( | ) | (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_SRPREQ_MASK)) |
tests if a SRP from device occurs
#define Is_usb_enabled | ( | ) | (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_USBE_MASK)) |
Referenced by usb_host_task_init().
#define Is_usb_full_speed_mode | ( | ) | (Rd_bitfield(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_SPEED_MASK) == AVR32_USBB_USBSTA_SPEED_FULL) |
Test if controller is in full speed mode.
#define Is_usb_full_speed_mode_used | ( | ) | (!Is_usb_low_speed_mode_forced()) |
Test if device full speed mode is used.
#define Is_usb_hnp | ( | ) | (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_HNPREQ_MASK)) |
tests if a HNP occurs
#define Is_usb_hnp_error_interrupt | ( | ) | (Tst_bits(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_HNPERRI_MASK)) |
tests if a HNP error occurs
#define Is_usb_hnp_error_interrupt_enabled | ( | ) | (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_HNPERRE_MASK)) |
#define Is_usb_host_mode_forced | ( | ) | (!Is_usb_id_pin_enabled() && !Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_UIMOD_MASK)) |
Test if host mode is forced.
#define Is_usb_id_device | ( | ) | (Tst_bits(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_ID_MASK)) |
#define Is_usb_id_interrupt_enabled | ( | ) | (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_IDTE_MASK)) |
#define Is_usb_id_pin_enabled | ( | ) | (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_UIDE_MASK)) |
Test if external USB_ID pin enabled (listened to by USB)
#define Is_usb_id_transition | ( | ) | (Tst_bits(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_IDTI_MASK)) |
#define Is_usb_low_speed_mode | ( | ) | (Rd_bitfield(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_SPEED_MASK) == AVR32_USBB_USBSTA_SPEED_LOW) |
Test if controller is in low-speed mode.
Referenced by host_get_data(), and host_transfer_control().
#define Is_usb_low_speed_mode_forced | ( | ) | (Tst_bits(AVR32_USBB_udcon, AVR32_USBB_UDCON_LS_MASK)) |
Test if device low-speed mode is forced.
#define Is_usb_otg_pad_enabled | ( | ) | (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_OTGPADE_MASK)) |
#define Is_usb_role_exchange_interrupt | ( | ) | (Tst_bits(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_ROLEEXI_MASK)) |
tests if a role exchange occurs
#define Is_usb_role_exchange_interrupt_enabled | ( | ) | (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_ROLEEXE_MASK)) |
#define Is_usb_srp_interrupt | ( | ) | (Tst_bits(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_SRPI_MASK)) |
tests if a SRP occurs
#define Is_usb_srp_interrupt_enabled | ( | ) | (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_SRPE_MASK)) |
#define Is_usb_suspend_time_out_interrupt | ( | ) | (Tst_bits(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_STOI_MASK)) |
tests if a suspend time out occurs
#define Is_usb_suspend_time_out_interrupt_enabled | ( | ) | (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_STOE_MASK)) |
#define Is_usb_vbof_active_high | ( | ) | (!Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_VBUSPO_MASK)) |
Get USB_VBOF output pin polarity.
#define Is_usb_vbof_active_low | ( | ) | (!Is_usb_vbof_active_high()) |
#define Is_usb_vbof_pin_output | ( | ) |
Test if USB_VBOF is output onto its pin.
#define Is_usb_vbus_enabled | ( | ) | (Tst_bits(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_VBUSRQ_MASK)) |
tests if VBus activation has been requested
#define Is_usb_vbus_error_interrupt | ( | ) | (Tst_bits(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_VBERRI_MASK)) |
tests if a VBus error occurs
Referenced by usb_host_task().
#define Is_usb_vbus_error_interrupt_enabled | ( | ) | (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_VBERRE_MASK)) |
#define Is_usb_vbus_high | ( | ) | (Tst_bits(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_VBUS_MASK)) |
Referenced by usb_host_task().
#define Is_usb_vbus_hw_control_enabled | ( | ) | (!Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_VBUSHWC_MASK)) |
#define Is_usb_vbus_interrupt_enabled | ( | ) | (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_VBUSTE_MASK)) |
#define Is_usb_vbus_low | ( | ) | (!Is_usb_vbus_high()) |
Referenced by usb_host_task().
#define Is_usb_vbus_srp_method_selected | ( | ) | (Tst_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_SRPSEL_MASK)) |
#define Is_usb_vbus_transition | ( | ) | (Tst_bits(AVR32_USBB_usbsta, AVR32_USBB_USBSTA_VBUSTI_MASK)) |
#define Usb_ack_bconnection_error_interrupt | ( | ) | (AVR32_USBB_usbstaclr = AVR32_USBB_USBSTACLR_BCERRIC_MASK) |
acks B-device connection error interrupt
Referenced by usb_host_task().
#define Usb_ack_hnp_error_interrupt | ( | ) | (AVR32_USBB_usbstaclr = AVR32_USBB_USBSTACLR_HNPERRIC_MASK) |
acks HNP error interrupt
#define Usb_ack_id_transition | ( | ) | (AVR32_USBB_usbstaclr = AVR32_USBB_USBSTACLR_IDTIC_MASK) |
#define Usb_ack_role_exchange_interrupt | ( | ) | (AVR32_USBB_usbstaclr = AVR32_USBB_USBSTACLR_ROLEEXIC_MASK) |
acks role exchange interrupt
#define Usb_ack_srp_interrupt | ( | ) | (AVR32_USBB_usbstaclr = AVR32_USBB_USBSTACLR_SRPIC_MASK) |
acks SRP interrupt
#define Usb_ack_suspend_time_out_interrupt | ( | ) | (AVR32_USBB_usbstaclr = AVR32_USBB_USBSTACLR_STOIC_MASK) |
acks suspend time out interrupt
#define Usb_ack_vbus_error_interrupt | ( | ) | (AVR32_USBB_usbstaclr = AVR32_USBB_USBSTACLR_VBERRIC_MASK) |
acks VBus error interrupt
Referenced by usb_host_task().
#define Usb_ack_vbus_transition | ( | ) | (AVR32_USBB_usbstaclr = AVR32_USBB_USBSTACLR_VBUSTIC_MASK) |
#define Usb_configure_timeout | ( | timer, | |
timeout | |||
) |
Configure time-out of specified OTG timer.
#define Usb_device_initiate_hnp | ( | ) | (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_HNPREQ_MASK)) |
initiates a Host negotiation Protocol
#define Usb_device_initiate_srp | ( | ) | (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_SRPREQ_MASK)) |
initiates a Session Request Protocol
#define Usb_disable | ( | ) | (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_USBE_MASK)) |
Disable USB macro.
Referenced by usb_host_task_init().
#define Usb_disable_bconnection_error_interrupt | ( | ) | (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_BCERRE_MASK)) |
disables B-device connection error interrupt
#define Usb_disable_hnp_error_interrupt | ( | ) | (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_HNPERRE_MASK)) |
disables HNP error interrupt
#define Usb_disable_id_interrupt | ( | ) | (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_IDTE_MASK)) |
#define Usb_disable_id_pin | ( | ) | (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_UIDE_MASK)) |
Disable external USB_ID pin (ignored by USB)
#define Usb_disable_otg_pad | ( | ) | (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_OTGPADE_MASK)) |
Disable OTG pad.
Referenced by usb_host_task_init().
#define Usb_disable_role_exchange_interrupt | ( | ) | (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_ROLEEXE_MASK)) |
disables role exchange interrupt
#define Usb_disable_srp_interrupt | ( | ) | (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_SRPE_MASK)) |
disables SRP interrupt
#define Usb_disable_suspend_time_out_interrupt | ( | ) | (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_STOE_MASK)) |
disables suspend time out interrupt
#define Usb_disable_vbus | ( | ) | (AVR32_USBB_usbstaclr = AVR32_USBB_USBSTACLR_VBUSRQC_MASK) |
requests VBus deactivation
Referenced by usb_host_task().
#define Usb_disable_vbus_error_interrupt | ( | ) | (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_VBERRE_MASK)) |
disables VBus error interrupt
#define Usb_disable_vbus_hw_control | ( | ) | (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_VBUSHWC_MASK)) |
disables hardware control over the USB_VBOF output pin
Referenced by usb_host_task_init().
#define Usb_disable_vbus_interrupt | ( | ) | (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_VBUSTE_MASK)) |
#define Usb_enable | ( | ) | (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_USBE_MASK)) |
Enable USB macro.
Referenced by usb_host_task_init().
#define Usb_enable_bconnection_error_interrupt | ( | ) | (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_BCERRE_MASK)) |
enables B-device connection error interrupt
#define Usb_enable_hnp_error_interrupt | ( | ) | (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_HNPERRE_MASK)) |
enables HNP error interrupt
#define Usb_enable_id_interrupt | ( | ) | (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_IDTE_MASK)) |
#define Usb_enable_id_pin | ( | ) | (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_UIDE_MASK)) |
Enable external USB_ID pin (listened to by USB)
#define Usb_enable_otg_pad | ( | ) | (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_OTGPADE_MASK)) |
Enable OTG pad.
Referenced by usb_host_task_init().
#define Usb_enable_role_exchange_interrupt | ( | ) | (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_ROLEEXE_MASK)) |
enables role exchange interrupt
#define Usb_enable_srp_interrupt | ( | ) | (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_SRPE_MASK)) |
enables SRP interrupt
#define Usb_enable_suspend_time_out_interrupt | ( | ) | (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_STOE_MASK)) |
enables suspend time out interrupt
#define Usb_enable_vbus | ( | ) | (AVR32_USBB_usbstaset = AVR32_USBB_USBSTASET_VBUSRQS_MASK) |
requests VBus activation
Referenced by usb_host_task().
#define Usb_enable_vbus_error_interrupt | ( | ) | (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_VBERRE_MASK)) |
enables VBus error interrupt
#define Usb_enable_vbus_hw_control | ( | ) | (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_VBUSHWC_MASK)) |
enables hardware control over the USB_VBOF output pin
#define Usb_enable_vbus_interrupt | ( | ) | (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_VBUSTE_MASK)) |
#define Usb_force_device_mode | ( | ) | (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_UIMOD_MASK), Usb_disable_id_pin()) |
Disable external USB_ID pin and force device mode.
#define Usb_force_full_speed_mode | ( | ) | do { } while (0) |
#define Usb_force_host_mode | ( | ) | (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_UIMOD_MASK), Usb_disable_id_pin()) |
Disable external USB_ID pin and force host mode.
#define Usb_force_low_speed_mode | ( | ) | (Set_bits(AVR32_USBB_udcon, AVR32_USBB_UDCON_LS_MASK)) |
Force device low-speed mode.
#define Usb_freeze_clock | ( | ) | (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_FRZCLK_MASK)) |
Stop (freeze) internal USB clock.
Referenced by usb_host_task().
#define Usb_get_fsm_drd_state | ( | ) | (Rd_bitfield(AVR32_USBB_usbfsm, AVR32_USBB_USBFSM_DRDSTATE_MASK)) |
Get the dual-role device state of the internal USB finite state machine of the USBB controller.
#define Usb_get_timeout | ( | timer | ) |
Get configured time-out of specified OTG timer.
#define Usb_host_accept_hnp | ( | ) | (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_HNPREQ_MASK)) |
accepts a Host negotiation Protocol
#define Usb_host_reject_hnp | ( | ) | (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_HNPREQ_MASK)) |
rejects a Host negotiation Protocol
#define Usb_output_vbof_pin | ( | ) |
Output USB_VBOF onto its pin.
Referenced by usb_host_task_init().
#define Usb_raise_bconnection_error_interrupt | ( | ) | (AVR32_USBB_usbstaset = AVR32_USBB_USBSTASET_BCERRIS_MASK) |
raises B-device connection error interrupt
#define Usb_raise_hnp_error_interrupt | ( | ) | (AVR32_USBB_usbstaset = AVR32_USBB_USBSTASET_HNPERRIS_MASK) |
raises HNP error interrupt
#define Usb_raise_id_transition | ( | ) | (AVR32_USBB_usbstaset = AVR32_USBB_USBSTASET_IDTIS_MASK) |
#define Usb_raise_role_exchange_interrupt | ( | ) | (AVR32_USBB_usbstaset = AVR32_USBB_USBSTASET_ROLEEXIS_MASK) |
raises role exchange interrupt
#define Usb_raise_srp_interrupt | ( | ) | (AVR32_USBB_usbstaset = AVR32_USBB_USBSTASET_SRPIS_MASK) |
raises SRP interrupt
#define Usb_raise_suspend_time_out_interrupt | ( | ) | (AVR32_USBB_usbstaset = AVR32_USBB_USBSTASET_STOIS_MASK) |
raises suspend time out interrupt
#define Usb_raise_vbus_error_interrupt | ( | ) | (AVR32_USBB_usbstaset = AVR32_USBB_USBSTASET_VBERRIS_MASK) |
raises VBus error interrupt
#define Usb_raise_vbus_transition | ( | ) | (AVR32_USBB_usbstaset = AVR32_USBB_USBSTASET_VBUSTIS_MASK) |
#define Usb_select_data_srp_method | ( | ) | (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_SRPSEL_MASK)) |
selects data line as SRP method
#define Usb_select_vbus_srp_method | ( | ) | (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_SRPSEL_MASK)) |
selects VBus as SRP method
#define Usb_set_vbof_active_high | ( | ) | (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_VBUSPO_MASK)) |
Set USB_VBOF output pin polarity.
Referenced by usb_host_task_init().
#define Usb_set_vbof_active_low | ( | ) | (Set_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_VBUSPO_MASK)) |
Referenced by usb_host_task_init().
#define Usb_unfreeze_clock | ( | ) | (Clr_bits(AVR32_USBB_usbcon, AVR32_USBB_USBCON_FRZCLK_MASK)) |
Referenced by usb_host_task(), and usb_host_task_init().
#define Usb_use_dual_speed_mode | ( | ) | do { } while (0) |
#define Usb_use_full_speed_mode | ( | ) | (Clr_bits(AVR32_USBB_udcon, AVR32_USBB_UDCON_LS_MASK)) |
Use device full speed mode (default)