Microchip® Advanced Software Framework

tpa6130.h File Reference
#include <stddef.h>
#include "compiler.h"

Macros

#define TPA6130_MODE_MONO   1
 
#define TPA6130_MODE_STEREO   0
 
#define TPA6130_SIG_DIFF   0
 
#define TPA6130_SIG_POS   1
 
#define TPA6130_TWI_ADDRESS   0x60
 
Volume Control
#define TPA6130_VOL_MIN   ((int8_t)( 0))
 
#define TPA6130_VOL_MAX   ((int8_t)( 63))
 

Functions

void tpa6130_dac_decrease_volume (void)
 Decreases the output volume of the DACs. More...
 
void tpa6130_dac_flush (void)
 Flushes the sample buffer being output to the DACs. More...
 
uint8_t tpa6130_dac_get_volume (void)
 Returns the current volume of the DAC. More...
 
void tpa6130_dac_increase_volume (void)
 Increases the output volume of the DACs. More...
 
bool tpa6130_dac_is_volume_boosted (void)
 Returns the state of the boost mode of the DAC. More...
 
bool tpa6130_dac_is_volume_muted (void)
 Returns the state of the mute mode of the DAC. More...
 
void tpa6130_dac_mute (bool mute)
 No more audio if input is true. More...
 
bool tpa6130_dac_output (void *sample_buffer, size_t sample_length)
 Outputs a sample buffer to the DACs. More...
 
void tpa6130_dac_set_volume (uint8_t volume)
 Set the volume of the DAC. More...
 
void tpa6130_dac_setup (uint32_t sample_rate_hz, uint8_t num_channels, uint8_t bits_per_sample, bool swap_channels, void(*callback)(uint32_t arg), uint32_t callback_opt, uint32_t pba_hz)
 Sets the DACs up with new settings. More...
 
void tpa6130_dac_start (uint32_t sample_rate_hz, uint8_t num_channels, uint8_t bits_per_sample, bool swap_channels, void(*callback)(uint32_t arg), uint32_t callback_opt, uint32_t pba_hz)
 Starts the ABDAC. More...
 
void tpa6130_dac_stop (void)
 Stops the DACs. More...
 
int8_t tpa6130_get_volume (void)
 Gets the current volume settings. More...
 
int8_t tpa6130_init (void)
 Probes and initializes the amplifier. Probes the TWI bus for the amplifier by using the slave address specified in the configuration (TPA6130_TWI_ADDRESS). If the device responds with an ACK the version register is read out and compared to the valid versions (TPA6130_VERSION). Last step is to set volume to 0, unmute and set the configuration specified in the conf_tpa6130.h file (stereo, mono ..). More...
 
void tpa6130_powerup (void)
 Powers up the amplifier from low power mode. This is the software low power mode described in the datasheet. More...
 
void tpa6130_set_volume (int8_t volume)
 Sets the volume of the amplifier. Valid values are between 0 (min -59dB) and 63 (max 4dB) although the function takes care of any values higher than that by setting it to max. More...
 
void tpa6130_shutdown (void)
 Shuts down the amplifier and sets it into low power mode. This is the software low power mode described in the datasheet. More...