#include "compiler.h"
Macros | |
Identifiers of LEDs to Use with LED Functions | |
#define | LED0 0x01 |
#define | LED1 0x02 |
#define | LED2 0x04 |
#define | LED3 0x08 |
Functions | |
void | LED_Display (U32 leds) |
Sets the state of all LEDs. More... | |
void | LED_Display_Field (U32 field, U32 leds) |
Sets as a bit-field the state of the specified LEDs. More... | |
void | LED_Display_Mask (U32 mask, U32 leds) |
Sets the state of the specified LEDs. More... | |
U8 | LED_Get_Intensity (U32 led) |
Gets the intensity of the specified LED. More... | |
void | LED_Off (U32 leds) |
Turns off the specified LEDs. More... | |
void | LED_On (U32 leds) |
Turns on the specified LEDs. More... | |
U32 | LED_Read_Display (void) |
Gets the last state of all LEDs set through the LED API. More... | |
U32 | LED_Read_Display_Field (U32 field) |
Gets as a bit-field the last state of the specified LEDs set through the LED API. More... | |
U32 | LED_Read_Display_Mask (U32 mask) |
Gets the last state of the specified LEDs set through the LED API. More... | |
void | LED_Set_Intensity (U32 leds, U8 intensity) |
Sets the intensity of the specified LEDs. More... | |
bool | LED_Test (U32 leds) |
Tests the last state of the specified LEDs set through the LED API. More... | |
void | LED_Toggle (U32 leds) |
Toggles the specified LEDs. More... | |
#define LED0 0x01 |
#define LED1 0x02 |
#define LED2 0x04 |
#define LED3 0x08 |
void LED_Display | ( | U32 | leds | ) |
Sets the state of all LEDs.
leds | New state of all LEDs (1 bit per LED). |
References tLED_DESCRIPTOR::GPIO, LED_COUNT, LED_State, tLED_DESCRIPTOR::PIN_MASK, and tLED_DESCRIPTOR::PORT.
Sets as a bit-field the state of the specified LEDs.
field | LEDs of which to set the state (1 bit per LED). |
leds | New state of the specified LEDs (1 bit per LED, beginning with the first specified LED). |
References ctz, and LED_Display_Mask().
Sets the state of the specified LEDs.
mask | LEDs of which to set the state (1 bit per LED). |
leds | New state of the specified LEDs (1 bit per LED). |
References ctz, tLED_DESCRIPTOR::GPIO, LED_COUNT, LED_State, tLED_DESCRIPTOR::PIN_MASK, tLED_DESCRIPTOR::PORT, and Wr_bits.
Referenced by LED_Display_Field().
Gets the intensity of the specified LED.
led | LED of which to get the intensity (1 bit per LED; only the least significant set bit is used). |
void LED_Off | ( | U32 | leds | ) |
Turns off the specified LEDs.
leds | LEDs to turn off (1 bit per LED). |
References Clr_bits, ctz, tLED_DESCRIPTOR::GPIO, LED_COUNT, LED_State, tLED_DESCRIPTOR::PIN_MASK, and tLED_DESCRIPTOR::PORT.
Referenced by prompt_user().
void LED_On | ( | U32 | leds | ) |
Turns on the specified LEDs.
leds | LEDs to turn on (1 bit per LED). |
References ctz, tLED_DESCRIPTOR::GPIO, LED_COUNT, LED_State, tLED_DESCRIPTOR::PIN_MASK, tLED_DESCRIPTOR::PORT, and Set_bits.
Referenced by main().
U32 LED_Read_Display | ( | void | ) |
Gets the last state of all LEDs set through the LED API.
References LED_State.
Gets as a bit-field the last state of the specified LEDs set through the LED API.
field | LEDs of which to get the state (1 bit per LED). |
References LED_State, and Rd_bitfield.
Sets the intensity of the specified LEDs.
leds | LEDs of which to set the intensity (1 bit per LED). |
intensity | New intensity of the specified LEDs (0x00 to 0xFF). |
Tests the last state of the specified LEDs set through the LED API.
leds | LEDs of which to test the state (1 bit per LED). |
true
if at least one of the specified LEDs has a state on, else false
.void LED_Toggle | ( | U32 | leds | ) |
Toggles the specified LEDs.
leds | LEDs to toggle (1 bit per LED). |
References ctz, tLED_DESCRIPTOR::GPIO, LED_COUNT, LED_State, tLED_DESCRIPTOR::PIN_MASK, tLED_DESCRIPTOR::PORT, and Tgl_bits.
Referenced by main(), and prompt_user().