Osram SFH7770 light & proximity sensor driver.
This file contains functions for initializing and reading data from a Osram SFH7770 light & proximity sensor.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Data Structures | |
struct | current_level_t |
Proximity sensor LED current table (mA, register field value) More... | |
struct | sample_rate_t |
Sample rate table entry. More... | |
Macros | |
#define | NUM_CURRENT_LEVELS (sizeof(current_table) / sizeof(current_level_t)) |
#define | NUM_LIGHT_RATES (sizeof(light_rate_table) / sizeof(sample_rate_t)) |
#define | NUM_PROX_RATES (sizeof(prox_rate_table) / sizeof(sample_rate_t)) |
#define | SFH7770_NVRAM_OFFSET (0x18) |
Functions | |
static bool | sfh7770_calibrate (sensor_t *sensor, sensor_calibration_t calib_type, int step, void *info) |
Calibrate proximity sensor detection thresholds. More... | |
static bool | sfh7770_device_id (sensor_hal_t *hal, sensor_data_t *data) |
Read SFH7770 device ID and revision numbers. More... | |
static bool | sfh7770_event (sensor_t *sensor, sensor_event_t sensor_event, sensor_event_callback_t *callback, bool enable) |
Enable or disable SFH7770 sensor events. More... | |
static bool | sfh7770_get_light (sensor_hal_t *hal, sensor_data_t *data) |
Read SFH7770 light level data. More... | |
static bool | sfh7770_get_proximity (sensor_hal_t *hal, sensor_data_t *data) |
Read SFH7770 proximity data. More... | |
static bool | sfh7770_get_threshold (sensor_hal_t *hal, int16_t channel, sensor_threshold_desc_t *threshold) |
Get event threshold value. More... | |
bool | sfh7770_init (sensor_t *sensor, int resvd) |
Osram SFH7770 light & proximity sensor driver initialization. More... | |
static bool | sfh7770_ioctl (sensor_t *sensor, sensor_command_t cmd, void *arg) |
SFH7770 ioctl control entry point. More... | |
static void | sfh7770_isr (volatile void *arg) |
Osram SFH7770 driver interrupt service routine. More... | |
static bool | sfh7770_read (sensor_t *sensor, sensor_read_t type, sensor_data_t *data) |
Read sensor data. More... | |
static bool | sfh7770_set_current (sensor_hal_t *hal, int16_t channel, uint16_t *level_mA) |
Set proximity LED current level. More... | |
static bool | sfh7770_set_rate (sensor_hal_t *hal, sensor_type_t type, uint16_t rate_hz) |
Set sensor sample rate. More... | |
static bool | sfh7770_set_state (sensor_hal_t *hal, sensor_type_t type, sensor_state_t state) |
Set the SFH7770 execution mode. More... | |
static bool | sfh7770_set_threshold (sensor_hal_t *hal, int16_t channel, sensor_threshold_desc_t *threshold) |
Set event threshold value. More... | |
Variables | |
static const current_level_t | current_table [] |
static sensor_event_callback_t | event_cb [3] |
Sensor Event Callback table (proximity=0, low light=1, high light=2) More... | |
static uint16_t | high_light_threshold |
Event threshold value for hight light. More... | |
static const sample_rate_t | light_rate_table [] |
Light sensor sample rate table (Hz, reg field value) More... | |
static uint16_t | low_light_threshold |
Event threshold value for low light. More... | |
static const sample_rate_t | prox_rate_table [] |
Proximity sensor sample rate table (Hz, reg field value) More... | |
static bool | sfh7770_initialized = false |
Driver initialization flag. More... | |
#define NUM_CURRENT_LEVELS (sizeof(current_table) / sizeof(current_level_t)) |
Referenced by sfh7770_set_current().
#define NUM_LIGHT_RATES (sizeof(light_rate_table) / sizeof(sample_rate_t)) |
Referenced by sfh7770_set_rate().
#define NUM_PROX_RATES (sizeof(prox_rate_table) / sizeof(sample_rate_t)) |
Referenced by sfh7770_set_rate().
#define SFH7770_NVRAM_OFFSET (0x18) |
Referenced by sfh7770_calibrate(), sfh7770_init(), and sfh7770_set_threshold().
|
static |
Calibrate proximity sensor detection thresholds.
This function measures the proximity sensor output in 3 different steps, one for each channel in the device. This function should be called when a sample object has been placed at the desired distance from the device to define the threshold for near-proximity detection. The measured proximity sensor value for each channel is stored in non-volatile memory. These thresholds will later be used to set the threshold during the device initialization sequence.
This routine must be called 3 times total, with the "step" parameter indicating what stage of the calibration is being performed (i.e. which channel of the proximity sensor). This multi-step mechanism allows the application to prompt for physical placement of the object to be detected before this routine is called.
sensor | Address of an initialized sensor device descriptor. |
calib_type | The address of a vector storing sensor axis data. |
step | The calibration stage number [1,3]. |
info | Unimplemented (ignored) parameter. |
References sensor_desc::err, sensor_desc::hal, MANUAL_CALIBRATE, nvram_read(), nvram_write(), sensor_bus_get, sensor_bus_write, SENSOR_ERR_IO, SENSOR_ERR_PARAMS, SFH7770_NVRAM_OFFSET, SFH7770_PS_DATA_LED1, SFH7770_PS_DATA_LED2, SFH7770_PS_DATA_LED3, and SFH7770_PS_THR_LED1.
Referenced by sfh7770_init().
|
static |
Read SFH7770 device ID and revision numbers.
This function reads the sensor hardware identification registers and returns these values in the specified data structure.
hal | Address of an initialized sensor hardware descriptor. |
data | Address of sensor_data_t structure to return values. |
References sensor_data_t::device, PART_ID_MASK, PART_ID_SHIFT, PART_REV_MASK, sensor_bus_get, and SFH7770_PART_ID.
Referenced by sfh7770_read().
|
static |
Enable or disable SFH7770 sensor events.
sensor | Address of an initialized sensor device descriptor |
callback | Application-defined event callback handler descriptor |
enable | Enable flag: true = enable event, false = disable event |
References sensor_desc::hal, INT_MODE_ALS, INT_MODE_PS, sensor_bus_get, sensor_bus_put, SENSOR_EVENT_HIGH_LIGHT, SENSOR_EVENT_LOW_LIGHT, SENSOR_EVENT_NEAR_PROXIMITY, and SFH7770_INT_SET.
Referenced by sfh7770_init(), and sfh7770_ioctl().
|
static |
Read SFH7770 light level data.
This function reads the ambient light level data from the sensor and places it in the user-provided sensor_data_t structure.
sensor | Address of an initialized sensor device descriptor. |
data | The address of a vector storing sensor measurement data. |
References sensor_data_t::light, sensor_bus_read, and SFH7770_ALS_DATA_LSB.
Referenced by sfh7770_read().
|
static |
Read SFH7770 proximity data.
This function reads the proximity data from the three channels of the sensor and places it in the user-provided sensor_data_t structure. The proximity value is not in standard units, so for "scaled" output the values are encoded based on whether or not the proximity reading exceeds the programmed threshold level for each channel (LED).
The sensor has only a single threshold level, so only two possible values are reported: PROXIMITY_NEAR (if threshold is exceeded) or PROXIMITY_NONE.
sensor | Address of an initialized sensor device descriptor. |
data | The address of a vector storing sensor measurement data. |
References sensor_data_t::proximity, PROXIMITY_NEAR, PROXIMITY_NONE, PS_LED1_THRESH, PS_LED2_THRESH, PS_LED3_THRESH, sensor_data_t::scaled, sensor_bus_read, and SFH7770_ALS_PS_STATUS.
Referenced by sfh7770_read().
|
static |
Get event threshold value.
hal | Address of an initialized sensor hardware descriptor. |
channel | Channel (LED) number to set threshold |
threshold | Address of threshold descriptor. |
References high_light_threshold, low_light_threshold, sensor_bus_get, SENSOR_CHANNEL_ALL, SENSOR_THRESHOLD_HIGH_LIGHT, SENSOR_THRESHOLD_LOW_LIGHT, SENSOR_THRESHOLD_NEAR_PROXIMITY, SFH7770_PS_THR_LED1, sensor_threshold_desc_t::type, and sensor_threshold_desc_t::value.
Referenced by sfh7770_ioctl().
Osram SFH7770 light & proximity sensor driver initialization.
This is the main initialization function for the SFH7770 device.
sensor | Address of a sensor device descriptor. |
resvd | Reserved value. |
References ALS_CONTROL_SW_RESET, ALS_INTERVAL_500MS, ALS_MODE_FREE_RUNNING, sensor_hal::burst_addr, sensor_hal::bus, sensor_desc::drv, sensor_device_t::func, sensor_desc::hal, I_LED2_SHIFT, I_LED_50MA, LED_ACTIVE_ALL, sensor_hal::mcu_sigint, nvram_read(), PS_INTERVAL_100MS, PS_MODE_FREE_RUNNING, sensor_funcs_t::read, sensor_hal::resolution, sensor_bus_get, sensor_bus_put, sensor_bus_write, sensor_irq_connect(), SENSOR_SCALE_one, SENSOR_TYPE_LIGHT, SENSOR_TYPE_PROXIMITY, SENSOR_UNITS_lux, SENSOR_VENDOR_OSRAM, SFH7770_ALS_CONTROL, SFH7770_ALS_DATA_LSB, SFH7770_ALS_INTERVAL, sfh7770_calibrate(), SFH7770_DATA_RESOLUTION, sfh7770_event(), SFH7770_I_LED_1_2, SFH7770_I_LED_3, sfh7770_initialized, SFH7770_INT_SET, sfh7770_ioctl(), sfh7770_isr(), SFH7770_NVRAM_OFFSET, SFH7770_PART_ID, SFH7770_PART_ID_VAL, SFH7770_PART_REV_VAL, SFH7770_PS_CONTROL, SFH7770_PS_INTERVAL, SFH7770_PS_THR_LED1, sfh7770_read(), bus_desc_t::status, STATUS_OK, and sensor_desc::type.
|
static |
SFH7770 ioctl control entry point.
hal | Address of an initialized sensor hardware descriptor. |
cmd | Command to execute |
arg | Argument for command (varies) |
References sensor_desc::channel, sensor_desc::err, sensor_desc::hal, SENSOR_DISABLE_EVENT, SENSOR_ENABLE_EVENT, SENSOR_ERR_UNSUPPORTED, SENSOR_GET_THRESHOLD, SENSOR_SET_CURRENT, SENSOR_SET_SAMPLE_RATE, SENSOR_SET_STATE, SENSOR_SET_THRESHOLD, sfh7770_event(), sfh7770_get_threshold(), sfh7770_set_current(), sfh7770_set_rate(), sfh7770_set_state(), sfh7770_set_threshold(), and sensor_desc::type.
Referenced by sfh7770_init().
|
static |
Osram SFH7770 driver interrupt service routine.
This is the common interrupt service routine for all enabled SFH7770 interrupt events. Three different types of interrupts can be programmed: high light level, low light level, and near proximity. All share the same interrupt pin and therefore the same ISR entry.
arg | The address of the driver sensor_hal_t descriptor. |
References sensor_hal::burst_addr, sensor_hal::bus, sensor_event_data_t::channel, sensor_event_data_t::data, sensor_event_data_t::event, sensor_event_callback_t::handler, high_light_threshold, INT_SOURCE_ALS, INT_SOURCE_LED1, INT_SOURCE_LED2, INT_SOURCE_LED3, INT_SOURCE_MASK, sensor_data_t::light, low_light_threshold, bus_desc_t::no_wait, sensor_data_t::proximity, PROXIMITY_NEAR, PROXIMITY_NONE, PS_LED1_THRESH, PS_LED2_THRESH, PS_LED3_THRESH, sensor_data_t::scaled, sensor_bus_read, SENSOR_EVENT_HIGH_LIGHT, SENSOR_EVENT_LOW_LIGHT, SENSOR_EVENT_NEAR_PROXIMITY, SENSOR_EVENT_UNKNOWN, sensor_timestamp(), bus_desc_t::status, STATUS_OK, and sensor_data_t::timestamp.
Referenced by sfh7770_init().
|
static |
Read sensor data.
This routine calls the appropriate internal data function to obtain the specified type of data from the sensor device.
sensor | Address of an initialized sensor device descriptor. |
type | Type of sensor data to read. |
data | The address where data values are returned. |
References sensor_desc::err, sensor_desc::hal, SENSOR_ERR_FUNCTION, SENSOR_READ_ID, SENSOR_READ_LIGHT, SENSOR_READ_PROXIMITY, sfh7770_device_id(), sfh7770_get_light(), and sfh7770_get_proximity().
Referenced by sfh7770_init().
|
static |
Set proximity LED current level.
hal | Address of an initialized sensor hardware descriptor. |
channel | Channel (LED) number to set current |
curr_levels | Address of an array of current levels (1 per LED) |
References current_level_t::field_val, I_LED1_MASK, I_LED2_MASK, I_LED2_SHIFT, NUM_CURRENT_LEVELS, sensor_bus_get, sensor_bus_put, SENSOR_CHANNEL_ALL, SFH7770_I_LED_1_2, and SFH7770_I_LED_3.
Referenced by sfh7770_ioctl().
|
static |
Set sensor sample rate.
hal | Address of an initialized sensor hardware descriptor. |
type | Active mode of the sensor (i.e. light or proximity) |
rate_hz | Sample rate in Hz |
References NUM_LIGHT_RATES, NUM_PROX_RATES, sensor_bus_put, SENSOR_TYPE_LIGHT, SENSOR_TYPE_PROXIMITY, SFH7770_ALS_INTERVAL, and SFH7770_PS_INTERVAL.
Referenced by sfh7770_ioctl().
|
static |
Set the SFH7770 execution mode.
This routine sets a specified SFH7770 execution state to one of the following:
SENSOR_STATE_SLEEP: Setting the sleep mode puts the specific sensor unit (light or proximity) in standby mode, in which no measurements are made.
SENSOR_STATE_NORMAL: Setting the sleep mode puts the specific sensor unit (light or proximity) in continuous measurement mode.
hal | Address of an initialized sensor hardware descriptor. |
type | The operational type of the sensor (light or proximity) |
state | A specified sensor operational state. |
References ALS_MODE_FREE_RUNNING, ALS_MODE_STANDBY, PS_MODE_FREE_RUNNING, PS_MODE_STANDBY, sensor_bus_put, SENSOR_STATE_NORMAL, SENSOR_STATE_SLEEP, SENSOR_TYPE_LIGHT, SFH7770_ALS_CONTROL, and SFH7770_PS_CONTROL.
Referenced by sfh7770_ioctl().
|
static |
Set event threshold value.
hal | Address of an initialized sensor hardware descriptor. |
channel | Channel (LED) number to set threshold |
threshold | Address of threshold descriptor. |
References high_light_threshold, if(), low_light_threshold, nvram_write(), sensor_bus_put, sensor_bus_write, SENSOR_CHANNEL_ALL, SENSOR_THRESHOLD_HIGH_LIGHT, SENSOR_THRESHOLD_LOW_LIGHT, SENSOR_THRESHOLD_NEAR_PROXIMITY, SFH7770_ALS_LO_THR_LSB, SFH7770_ALS_UP_THR_LSB, SFH7770_NVRAM_OFFSET, SFH7770_PS_THR_LED1, sensor_threshold_desc_t::type, and sensor_threshold_desc_t::value.
Referenced by sfh7770_ioctl().
|
static |
|
static |
Sensor Event Callback table (proximity=0, low light=1, high light=2)
|
static |
Event threshold value for hight light.
Referenced by sfh7770_get_threshold(), sfh7770_isr(), and sfh7770_set_threshold().
|
static |
Light sensor sample rate table (Hz, reg field value)
|
static |
Event threshold value for low light.
Referenced by sfh7770_get_threshold(), sfh7770_isr(), and sfh7770_set_threshold().
|
static |
Proximity sensor sample rate table (Hz, reg field value)
Driver initialization flag.
Referenced by sfh7770_init().