Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Bluetooth (SPP Profile) with Cybercom Stack Application for evk1105 Documentation

Introduction

This is the documentation for the Cybercom Bluetooth demo. The setup of the demo is explained in the getting started of the bluetooth extension board (ATEXTBT). Operating mode:

Main Files

Compilation Information

This software is written for GNU GCC for AVR32 and for IAR Embedded Workbench for Atmel AVR32. Other compilers may or may not work.

Device Information

All UC3 devices can be used.

Configuration Information

This example has been tested with the following configuration:

  • UC3C_EK, EVK1104 and EVK1105 evaluation kit;

Information

To connect EXTBT to UC3C_EK, EVK1104, EVK1105, please refer to : http://ww1.microchip.com/downloads/en/AppNotes/doc32153.pdf.

Issues

The connection Bluetooth may be failed if the connection is initiated from the board. The state changes to "connected" too early even if the connection is not completed on the PC. If the connection is initiated by the PC, the connection will succeed in all cases. Please refer to http://ww1.microchip.com/downloads/en/AppNotes/doc32153.pdf.

Contact Information

For further information, visit Atmel AVR.