Microchip® Advanced Software Framework

qt1081.h File Reference
#include "compiler.h"
#include "board.h"
#include "gpio.h"

Functions

static __always_inline int is_touch_sensor_0 (void)
 This function tests if touch sensor 0 was touched. More...
 
static __always_inline int is_touch_sensor_1 (void)
 This function tests if touch sensor 1 was touched. More...
 
static __always_inline int is_touch_sensor_2 (void)
 This function tests if touch sensor 2 was touched. More...
 
static __always_inline int is_touch_sensor_3 (void)
 This function tests if touch sensor 3 was touched. More...
 
static __always_inline int is_touch_sensor_4 (void)
 This function tests if touch sensor 4 was touched. More...
 
static __always_inline void qt1081_power_down (void)
 Puts the QT1081 into low power mode. More...
 
static __always_inline void qt1081_power_up (void)
 Puts the QT1081 into low power mode. More...