Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
UC3-L0 Xplained with Xplained Light/Proximity Board #1 Documentation

Introduction

This application performs a multi-step manual calibration on a 3-channel proximity sensor device. An object (e.g. a hand) is placed in front of the proximity sensor at the desired distance for proximity detection. The user presses the button on the processor board to advance to the next channel. After each channel's threshold has been set, the program will continuously display an indication of the current proximity status for each channel.

Contact Information

For further information, visit Atmel AVR.
Support and FAQ: https://www.microchip.com/support/