Common Sensor Service Pressure Sensor Example.
Copyright (c) 2011-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | ACTIVITY_LED (LED1) |
#define | PRINT_BANNER (true) |
Functions | |
int | main (void) |
Pressure sensor demonstration application entry. More... | |
int main | ( | void | ) |
Pressure sensor demonstration application entry.
After initializing the development platform and sensors, this application attaches a descriptor to the sensor on an Xplained pressure sensor board. The sensor pressure and temperature data, which is formatted and printed via printf() after being read, can be viewed with a terminal application on a machine attached to the serial interface on the development board.
References ACTIVITY_LED, sensor_device_t::caps, delay_ms, sensor_desc::drv, sensor_desc::err, sensor_desc::hal, LED_Toggle(), sensor_caps_t::name, sensor_data_t::pressure, PRINT_BANNER, sensor_hal::resolution, sensor_data_t::scaled, sensor_attach(), sensor_device_id(), sensor_get_pressure(), sensor_get_temperature(), sensor_platform_init(), sensor_set_state(), SENSOR_STATE_HIGHEST_POWER, SENSOR_TYPE_BAROMETER, and sensor_data_t::temperature.