This is the documentation for FPU demo application running on the UC3C_EK development kit. Operating mode:
This software is written for IAR Embedded Workbench for Atmel AVR32. Other compilers may or may not work.
All AVR32 AT32UC3 devices with FPU can be used.
This example has been tested with the following configuration:
For further information, visit Atmel AVR32.