Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
Display DIP204 Example for evk1100 Documentation

Introduction

This documents data structures, functions, variables, defines, enums, and typedefs in the software.
It also gives an example of the usage of the DIP204 LCD on EVK1100.

Example's operating mode:

  • A default message is displayed on the 4 lines of the LCD
  • Press PB0 to see the full set of available chars on the LCD
  • Press PB1 to decrease the backlight power of the LCD
  • Press PB2 to increase the backlight power of the LCD
  • Use the joystick to see arrows displayed on the LCD
  • Press the joystick to see a circle displayed on the LCD and to return to the idle screen (displaying the default message)

Compilation Info

This software was written for the GNU GCC for AVR32 and IAR Systems compiler for AVR32. Other compilers may or may not work.

Device Info

All AVR32UC devices with an SPI module can be used. This example has been tested with the following setup:

  • EVK1100 evaluation kit

Setup Information

CPU speed: 12 MHz

Contact Information

For further information, visit Atmel AVR32.