This is the documentation for the AT42QT1060 driver.
This example demonstrates how to use the AT42QT1060 interface.
This software is written for GNU GCC for AVR32 and for IAR Embedded Workbench for Atmel AVR32. Other compilers may or may not work.
All AVR32 devices with a TWI or TWIM can be used.
This example has been tested with the following configuration:
For further information, visit Atmel AVR32.