The QT1081 sensor is operated by GPIOs and this driver provides a wrapper for the GPIO accesses.
Functions | |
static __always_inline int | is_touch_sensor_0 (void) |
This function tests if touch sensor 0 was touched. More... | |
static __always_inline int | is_touch_sensor_1 (void) |
This function tests if touch sensor 1 was touched. More... | |
static __always_inline int | is_touch_sensor_2 (void) |
This function tests if touch sensor 2 was touched. More... | |
static __always_inline int | is_touch_sensor_3 (void) |
This function tests if touch sensor 3 was touched. More... | |
static __always_inline int | is_touch_sensor_4 (void) |
This function tests if touch sensor 4 was touched. More... | |
static __always_inline void | qt1081_power_down (void) |
Puts the QT1081 into low power mode. More... | |
static __always_inline void | qt1081_power_up (void) |
Puts the QT1081 into low power mode. More... | |
|
static |
This function tests if touch sensor 0 was touched.
true
if the sensor is touched, otherwise 0
. References gpio_get_pin_value(), QT1081_TOUCH_SENSOR_0, and QT1081_TOUCH_SENSOR_0_PRESSED.
|
static |
This function tests if touch sensor 1 was touched.
true
if the sensor is touched, otherwise 0
. References gpio_get_pin_value(), QT1081_TOUCH_SENSOR_1, and QT1081_TOUCH_SENSOR_1_PRESSED.
|
static |
This function tests if touch sensor 2 was touched.
true
if the sensor is touched, otherwise 0
. References gpio_get_pin_value(), QT1081_TOUCH_SENSOR_2, and QT1081_TOUCH_SENSOR_2_PRESSED.
|
static |
This function tests if touch sensor 3 was touched.
true
if the sensor is touched, otherwise 0
. References gpio_get_pin_value(), QT1081_TOUCH_SENSOR_3, and QT1081_TOUCH_SENSOR_3_PRESSED.
|
static |
This function tests if touch sensor 4 was touched.
true
if the sensor is touched, otherwise 0
. References gpio_get_pin_value(), QT1081_TOUCH_SENSOR_4, and QT1081_TOUCH_SENSOR_4_PRESSED.
|
static |
Puts the QT1081 into low power mode.
References gpio_set_gpio_pin(), and QT1081_LP_MODE.
|
static |
Puts the QT1081 into low power mode.
References gpio_clr_gpio_pin(), and QT1081_LP_MODE.