This is the documentation for the resistive touch driver example.
This example demonstrates how to use a resistive touch panel with the UC3.
This software is written for GNU GCC for AVR32 and for IAR Embedded Workbench for Atmel AVR32. Other compilers may or may not work.
This example has been tested with the following configuration:
For further information, visit Atmel AVR32.