Data Structures | |
struct | adcifa_opt_t |
Parameters for the ADCIFA peripheral. More... | |
struct | adcifa_sequencer_conversion_opt_t |
Parameters for an conversion in the Sequencer. More... | |
struct | adcifa_sequencer_opt_t |
Parameters for the configuration of the Sequencer. More... | |
struct | adcifa_window_monitor_opt_t |
Parameters for the windows monitor mode. More... | |
Macros | |
#define | ADCIFA_clear_eoc_sequencer_0() ((AVR32_ADCIFA.scr) |= (1 << AVR32_ADCIFA_SCR_SEOC0)) |
Sequencer 0 : Ack end of Conversion. More... | |
#define | ADCIFA_clear_eoc_sequencer_1() ((AVR32_ADCIFA.scr) |= (1 << AVR32_ADCIFA_SCR_SEOC1) |
Sequencer 1 : Ack end of Conversion. More... | |
#define | ADCIFA_clear_eos_sequencer_0() ((AVR32_ADCIFA.scr) |= (1 << AVR32_ADCIFA_SCR_SEOS0)) |
Sequencer 0 : Ack end of Sequence. More... | |
#define | ADCIFA_clear_eos_sequencer_1() ((AVR32_ADCIFA.scr) |= (1 << AVR32_ADCIFA_SCR_SEOS1)) |
Sequencer 1 : Ack end of Sequence. More... | |
#define | ADCIFA_clear_window_0() ((AVR32_ADCIFA.scr) |= (1 << AVR32_ADCIFA_SCR_WM0)) |
Window Monitor 0 : Ack the Window Monitor 0 Status Bit. More... | |
#define | ADCIFA_clear_window_1() ((AVR32_ADCIFA.scr) |= (1 << AVR32_ADCIFA_SCR_WM1)) |
Window Monitor 1 : Ack the Window Monitor 1 Status Bit. More... | |
#define | ADCIFA_CONFIGURATION_ACCEPTED 0x1 |
This constant is used as return value for adcifa_configure and adcifa_configure_sequencer functions. More... | |
#define | ADCIFA_CONFIGURATION_REFUSED 0x0 |
This constant is used as return value for adcifa_configure and adcifa_configure_sequencer functions. More... | |
#define | ADCIFA_configure_muxsel0n(m7, m6, m5, m4, m3, m2, m1, m0) |
Configuration of Mux Negative for Sequencer 0. More... | |
#define | ADCIFA_configure_muxsel0p(m7, m6, m5, m4, m3, m2, m1, m0) |
Configuration of Mux Positive for Sequencer 0. More... | |
#define | ADCIFA_configure_muxsel1n(m7, m6, m5, m4, m3, m2, m1, m0) |
Configuration of Mux Negative for Sequencer 1. More... | |
#define | ADCIFA_configure_muxsel1p(m7, m6, m5, m4, m3, m2, m1, m0) |
Configuration of Mux Positive for Sequencer 1. More... | |
#define | ADCIFA_configure_sequencer_0(cnvnb, sres, trgsel, socb, sh_mode, hwla, sa) |
Configuration of Sequencer 0. More... | |
#define | ADCIFA_configure_sequencer_1(cnvnb, sres, trgsel, socb, csws, hwla, sa) |
Configuration of Sequencer 1. More... | |
#define | ADCIFA_configure_sh0gain(g7, g6, g5, g4, g3, g2, g1, g0) |
Configuration of Gain for Sequencer 0. More... | |
#define | ADCIFA_configure_sh1gain(g7, g6, g5, g4, g3, g2, g1, g0) |
Configuration of Gain for Sequencer 1. More... | |
#define | ADCIFA_disable() |
Enable the ADCIFA. More... | |
#define | ADCIFA_enable() |
Enable the ADCIFA. More... | |
#define | ADCIFA_is_eoc_sequencer_0() |
Sequencer 0 : Check end of Conversion. More... | |
#define | ADCIFA_is_eoc_sequencer_1() |
Sequencer 1 : Check end of Conversion. More... | |
#define | ADCIFA_is_eos_sequencer_0() |
Sequencer 0 : Check end of Sequence. More... | |
#define | ADCIFA_is_eos_sequencer_1() |
Sequencer 1 : Check end of Sequence. More... | |
#define | ADCIFA_is_startup_time() |
Check Startup Time flag. More... | |
#define | ADCIFA_is_window_0_set() |
Window Monitor 0 : Check the Window Monitor 0 Status Bit. More... | |
#define | ADCIFA_is_window_1_set() |
Window Monitor 1 : Check the Window Monitor 1 Status Bit. More... | |
#define | ADCIFA_NONE 0xFF |
Parameter. More... | |
#define | ADCIFA_read_resx_sequencer_0(ind) ((int32_t)AVR32_ADCIFA.resx[(ind)]) |
Return result for conversion for Sequencer 0. More... | |
#define | ADCIFA_read_resx_sequencer_1(ind) ((int)AVR32_ADCIFA.resx[(ind) + 8]) |
Return result for conversion for Sequencer 1. More... | |
#define | ADCIFA_set_gain_calibration(gcal) |
Set Gain Calibration. More... | |
#define | ADCIFA_set_offset_calibration(ocal) |
Set Offset Calibration. More... | |
#define | ADCIFA_set_sh0_gain_calibration(scal) |
Set Sample & Hold Gain Calibration for Seq 0. More... | |
#define | ADCIFA_set_sh1_gain_calibration(scal) |
Set Sample & Hold Gain Calibration for Seq 0. More... | |
#define | ADCIFA_softsoc_sequencer(seq) |
#define | ADCIFA_softsoc_sequencer_0() { AVR32_ADCIFA.cr = AVR32_ADCIFA_CR_SOC0_MASK; } |
Sequencer 0 : Software Start of Conversion. More... | |
#define | ADCIFA_softsoc_sequencer_1() { AVR32_ADCIFA.cr = AVR32_ADCIFA_CR_SOC1_MASK; } |
Sequencer 1 : Software Start of Conversion. More... | |
#define | ADCIFA_START_UP_TIME 1000 |
ADCIFA Start-Up time (us) More... | |
#define | ADCIFA_STATUS_COMPLETED 0x2 |
This constant is used as return value for the adcifa_get_values_from_sequencer function. More... | |
#define | ADCIFA_STATUS_NOT_COMPLETED 0x3 |
This constant is used as return value for the adcifa_get_values_from_sequencer function. More... | |
#define | AVR32_FLASHC_FACTORY_PAGE_ADDRESS 0x80800200 |
#define | AVR32_FLASHC_FROW_GAIN0_MASK 0x000003FF |
#define | AVR32_FLASHC_FROW_GAIN0_OFFSET 0 |
#define | AVR32_FLASHC_FROW_GAIN0_WORD 8 |
#define | AVR32_FLASHC_FROW_GAIN1_MASK 0x03FF0000 |
#define | AVR32_FLASHC_FROW_GAIN1_OFFSET 16 |
#define | AVR32_FLASHC_FROW_GAIN1_WORD 8 |
#define | AVR32_FLASHC_FROW_GCAL_MASK 0x00007FFF |
#define | AVR32_FLASHC_FROW_GCAL_OFFSET 0 |
#define | AVR32_FLASHC_FROW_GCAL_WORD 4 |
#define | AVR32_FLASHC_FROW_OCAL_MASK 0x3F000000 |
#define | AVR32_FLASHC_FROW_OCAL_OFFSET 24 |
#define | AVR32_FLASHC_FROW_OCAL_WORD 4 |
Positive Inputs used by the ADC | |
#define | AVR32_ADCIFA_INP_ADCIN0 0 |
#define | AVR32_ADCIFA_INP_ADCIN1 1 |
#define | AVR32_ADCIFA_INP_ADCIN2 2 |
#define | AVR32_ADCIFA_INP_ADCIN3 3 |
#define | AVR32_ADCIFA_INP_ADCIN4 4 |
#define | AVR32_ADCIFA_INP_ADCIN5 5 |
#define | AVR32_ADCIFA_INP_ADCIN6 6 |
#define | AVR32_ADCIFA_INP_ADCIN7 7 |
#define | AVR32_ADCIFA_INP_DAC0_INT 8 |
#define | AVR32_ADCIFA_INP_TSENSE 9 |
#define | AVR32_ADCIFA_INP_GNDANA 10 |
Negative Inputs used by the ADC | |
#define | AVR32_ADCIFA_INN_ADCIN8 0 |
#define | AVR32_ADCIFA_INN_ADCIN9 1 |
#define | AVR32_ADCIFA_INN_ADCIN10 2 |
#define | AVR32_ADCIFA_INN_ADCIN11 3 |
#define | AVR32_ADCIFA_INN_ADCIN12 4 |
#define | AVR32_ADCIFA_INN_ADCIN13 5 |
#define | AVR32_ADCIFA_INN_ADCIN14 6 |
#define | AVR32_ADCIFA_INN_ADCIN15 7 |
#define | AVR32_ADCIFA_INN_DAC1_INT 8 |
#define | AVR32_ADCIFA_INN_GNDANA 9 |
References used by the ADC | |
#define | ADCIFA_REF1V 0x0 /** Internal 1V reference */ |
#define | ADCIFA_REF06VDD 0x1 /** Internal 0.6 x VDDANA reference */ |
#define | ADCIFA_ADCREF0 0x2 /** External 0 reference ADCREF0 */ |
#define | ADCIFA_ADCREF1 0x3 /** External 1 reference ADCREF1 */ |
#define | ADCIFA_ADCREF 0x10 /** External reference ADCREFP/ADCREFN */ |
Triggering Source used by the ADC | |
#define | ADCIFA_TRGSEL_SOFT 0x0 /** Trigger Source Software */ |
#define | ADCIFA_TRGSEL_ITIMER 0x1 /** Trigger Source Timer */ |
#define | ADCIFA_TRGSEL_EVT 0x2 /** Trigger Source Event */ |
#define | ADCIFA_TRGSEL_CONTINUOUS 0x3 /** Trigger Source Continuous */ |
Resolution selected by the ADC | |
#define | ADCIFA_SRES_8B 0x2 /** Resolution 8-Bits */ |
#define | ADCIFA_SRES_10B 0x1 /** Resolution 10-Bits */ |
#define | ADCIFA_SRES_12B 0x0 /** Resolution 12-Bits */ |
Gain selected on a Conversion by the ADC | |
#define | ADCIFA_SHG_1 0x0 /** Gain Conversion = 1 */ |
#define | ADCIFA_SHG_2 0x1 /** Gain Conversion = 2 */ |
#define | ADCIFA_SHG_4 0x2 /** Gain Conversion = 4 */ |
#define | ADCIFA_SHG_8 0x3 /** Gain Conversion = 8 */ |
#define | ADCIFA_SHG_16 0x4 /** Gain Conversion = 16 */ |
#define | ADCIFA_SHG_32 0x5 /** Gain Conversion = 32 */ |
#define | ADCIFA_SHG_64 0x6 /** Gain Conversion = 64 */ |
Conversion Management of the Sequence | |
#define | ADCIFA_SOCB_ALLSEQ |
#define | ADCIFA_SOCB_SINGLECONV |
Sampling Mode (OVSX2 & SHDYN) | |
#define | ADCIFA_SH_MODE_STANDARD 0x0 /** No dynamic over sampling */ |
#define | ADCIFA_SH_MODE_OVERSAMP 0x1 /** Over sampling: OVSX2 = 1 */ |
#define | ADCIFA_SH_MODE_DYNAMIC 0x2 /** Dynamic: SHDYN = 1 */ |
Half Word Left Adjustment (HWLA) | |
#define | ADCIFA_HWLA_NOADJ 0x0 /** Disable the HWLA mode */ |
#define | ADCIFA_HWLA_LEFTADJ 0x1 /** Enable the HWLA mode */ |
Software Acknowledge (SA) | |
#define | ADCIFA_SA_EOS_SOFTACK 0x0 /** Disable the SA mode */ |
#define | ADCIFA_SA_NO_EOS_SOFTACK 0x1 /** Enable the SA mode */ |
Sequence numbers | |
#define | ADCIFA_SEQ0 0x0 |
#define | ADCIFA_SEQ1 0x1 |
#define | ADCIFA_SEQ0_SEQ1 0x3 |
Window monitor | |
#define | ADCIFA_WINDOW_MODE_NONE 0 /** No Window Mode : Default */ |
#define | ADCIFA_WINDOW_MODE_BELOW 1 /** Active : Result < High Threshold */ |
#define | ADCIFA_WINDOW_MODE_ABOVE 2 /** Active : Result > Low Threshold */ |
#define | ADCIFA_WINDOW_MODE_INSIDE 3 /** Active : Low Threshold < Result < High Threshold */ |
#define | ADCIFA_WINDOW_MODE_OUTSIDE 4 /** Active : Result >= Low Threshold or Result >= High Threshold */ |
Functions | |
void | adcifa_calibrate_offset (volatile avr32_adcifa_t *adcifa, adcifa_opt_t *p_adcifa_opt, uint32_t pb_hz) |
bool | adcifa_check_eoc (volatile avr32_adcifa_t *adcifa, uint8_t sequencer) |
Get End of Conversion status bit. More... | |
bool | adcifa_check_eos (volatile avr32_adcifa_t *adcifa, uint8_t sequencer) |
Get End of Conversion status bit. More... | |
void | adcifa_clear_interrupt (volatile avr32_adcifa_t *adcifa, uint32_t interrupt_flags) |
Clear any ADCIFA interrupt. More... | |
uint8_t | adcifa_configure (volatile avr32_adcifa_t *adcifa, adcifa_opt_t *p_adcifa_opt, uint32_t pb_hz) |
Configure ADCIFA. More... | |
uint8_t | adcifa_configure_sequencer (volatile avr32_adcifa_t *adcifa, uint8_t sequencer, adcifa_sequencer_opt_t *p_adcifa_sequencer_opt, adcifa_sequencer_conversion_opt_t *p_adcifa_sequencer_conversion_opt) |
Configure ADCIFA specific sequencer. More... | |
void | adcifa_configure_window_monitor (volatile avr32_adcifa_t *adcifa, uint8_t sequencer, adcifa_window_monitor_opt_t *adc_window_monitor_opt) |
Configure ADCIFA specific window monitor. More... | |
void | adcifa_disable_interrupt (volatile avr32_adcifa_t *adcifa, uint32_t interrupt_flags) |
Disable any ADCIFA interrupt. More... | |
void | adcifa_enable_interrupt (volatile avr32_adcifa_t *adcifa, uint32_t interrupt_flags) |
Enable any ADCIFA interrupt. More... | |
void | adcifa_get_calibration_data (volatile avr32_adcifa_t *adcifa, adcifa_opt_t *p_adcifa_opt) |
Get ADCIFA Calibration Data. More... | |
uint8_t | adcifa_get_values_from_sequencer (volatile avr32_adcifa_t *adcifa, uint8_t sequencer, adcifa_sequencer_opt_t *p_adcifa_sequencer_opt, int16_t *adcifa_values) |
Get channel values for a specific sequence. More... | |
void | adcifa_start_itimer (volatile avr32_adcifa_t *adcifa, uint32_t timer_count) |
Start the ADCIFA timer. More... | |
void | adcifa_start_sequencer (volatile avr32_adcifa_t *adcifa, uint8_t sequencer) |
Start analog to digital conversion for a specific sequencer. More... | |
void | adcifa_stop_itimer (volatile avr32_adcifa_t *adcifa) |
Stop the ADCIFA timer. More... | |