Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
ADCIFB Example 1 for UC3_L0_XPLAINED Documentation

Introduction

This is the documentation for the data structures, functions, variables, defines, enums, and typedefs for the ADCIFB software driver.

It also gives an example of usage of the ADCIFB module, eg:

  • On the AT32UC3L-EK: Display on a serial terminal the battery voltage converted value.
  • On the UC3-L0-Xplained: Display on a serial terminal the voltage from NTC temperature sensor.

Main Files

Compilation Info

This software was written for the GNU GCC for AVR32 and IAR Systems compiler for AVR32. Other compilers may or may not work.

Device Info

All AVR32 devices with an ADCIFB module can be used. This example has been tested with the following setup:

  • AT32UC3L-EK evaluation kit
  • UC3-L0-Xplained kit

Setup Information for the UC3-L0 Xplained kit

CPU speed: 48 MHz

  • Insert a V450HR battery into the socket of the AT32UC3L-EK
  • Connect a PC USB cable to the USB VCP plug of the AT32UC3L-EK
  • PC terminal settings:
    • 57600 bps,
    • 8 data bits,
    • no parity bit,
    • 1 stop bit,
    • no flow control.

Setup Information for the UC3-L0 Xplained kit

CPU speed: 48 MHz

  • Connect a PC USB cable to the USB VCP plug of the UC3-L0 Xplained
  • PC terminal settings:
    • 57600 bps,
    • 8 data bits,
    • no parity bit,
    • 1 stop bit,
    • no flow control.

Contact Information

For further information, visit Atmel AVR32.
Support and FAQ: https://www.microchip.com/support/