Microchip® Advanced Software Framework

stk600_rcuc3l0.h File Reference
#include "compiler.h"
#include "led.h"

Macros

#define LED_COUNT   4
 Number of LEDs. More...
 
Oscillator Definitions
#define FOSC32   32768
 Osc32 frequency: Hz. More...
 
#define OSC32_STARTUP   AVR32_SCIF_OSCCTRL32_STARTUP_8192_RCOSC
 Osc32 startup time: RCOsc periods. More...
 
#define FOSC0   12000000
 Osc0 frequency: Hz. More...
 
#define OSC0_STARTUP   AVR32_SCIF_OSCCTRL0_STARTUP_2048_RCOSC
 Osc0 startup time: RCOsc periods. More...
 
GPIO Connections of LEDs. To use these defines, connect the STK600 PORTA

PA4-to-PA7 connectors to respectively the LEDs LED0-to-LED3 connectors. Note that when the JTAG is active, it uses pins PA00-to-PA03 of the UC3L. This is why we didn't use pins PA00-to-PA03 for the LEDs LED0-to-LED3.

#define LED0_GPIO   AVR32_PIN_PA04
 
#define LED1_GPIO   AVR32_PIN_PA05
 
#define LED2_GPIO   AVR32_PIN_PA06
 
#define LED3_GPIO   AVR32_PIN_PA07
 
#define LED4_GPIO   AVR32_PIN_PA10
 
#define LED5_GPIO   AVR32_PIN_PA11
 
#define LED6_GPIO   AVR32_PIN_PA12
 
#define LED7_GPIO   AVR32_PIN_PA13
 
GPIO Connections of Push Buttons. To use these defines, connect the

STK600 PORTD connector to the SWITCHES connector.

#define GPIO_PUSH_BUTTON_SW0   AVR32_PIN_PB00
 
#define GPIO_PUSH_BUTTON_SW0_PRESSED   0
 
#define GPIO_PUSH_BUTTON_SW1   AVR32_PIN_PB01
 
#define GPIO_PUSH_BUTTON_SW1_PRESSED   0
 
#define GPIO_PUSH_BUTTON_SW2   AVR32_PIN_PB02
 
#define GPIO_PUSH_BUTTON_SW2_PRESSED   0
 
#define GPIO_PUSH_BUTTON_SW3   AVR32_PIN_PB03
 
#define GPIO_PUSH_BUTTON_SW3_PRESSED   0
 
#define GPIO_PUSH_BUTTON_SW4   AVR32_PIN_PB04
 
#define GPIO_PUSH_BUTTON_SW4_PRESSED   0
 
#define GPIO_PUSH_BUTTON_SW5   AVR32_PIN_PB05
 
#define GPIO_PUSH_BUTTON_SW5_PRESSED   0
 
#define GPIO_PUSH_BUTTON_SW6   AVR32_PIN_PB06
 
#define GPIO_PUSH_BUTTON_SW6_PRESSED   0
 
#define GPIO_PUSH_BUTTON_SW7   AVR32_PIN_PB07
 
#define GPIO_PUSH_BUTTON_SW7_PRESSED   0
 
SPI Connections of the AT45DBX Data Flash Memory
#define AT45DBX_SPI   (&AVR32_SPI)
 
#define AT45DBX_SPI_NPCS   0
 
#define AT45DBX_SPI_SCK_PIN   AVR32_SPI_SCK_0_0_PIN
 
#define AT45DBX_SPI_SCK_FUNCTION   AVR32_SPI_SCK_0_0_FUNCTION
 
#define AT45DBX_SPI_MISO_PIN   AVR32_SPI_MISO_0_0_PIN
 
#define AT45DBX_SPI_MISO_FUNCTION   AVR32_SPI_MISO_0_0_FUNCTION
 
#define AT45DBX_SPI_MOSI_PIN   AVR32_SPI_MOSI_0_0_PIN
 
#define AT45DBX_SPI_MOSI_FUNCTION   AVR32_SPI_MOSI_0_0_FUNCTION
 
#define AT45DBX_SPI_NPCS0_PIN   AVR32_SPI_NPCS_0_0_PIN
 
#define AT45DBX_SPI_NPCS0_FUNCTION   AVR32_SPI_NPCS_0_0_FUNCTION
 

#define AT45DBX_SPI   (&AVR32_SPI)
#define AT45DBX_SPI_MISO_FUNCTION   AVR32_SPI_MISO_0_0_FUNCTION
#define AT45DBX_SPI_MISO_PIN   AVR32_SPI_MISO_0_0_PIN
#define AT45DBX_SPI_MOSI_FUNCTION   AVR32_SPI_MOSI_0_0_FUNCTION
#define AT45DBX_SPI_MOSI_PIN   AVR32_SPI_MOSI_0_0_PIN
#define AT45DBX_SPI_NPCS   0
#define AT45DBX_SPI_NPCS0_FUNCTION   AVR32_SPI_NPCS_0_0_FUNCTION
#define AT45DBX_SPI_NPCS0_PIN   AVR32_SPI_NPCS_0_0_PIN
#define AT45DBX_SPI_SCK_FUNCTION   AVR32_SPI_SCK_0_0_FUNCTION
#define AT45DBX_SPI_SCK_PIN   AVR32_SPI_SCK_0_0_PIN
#define FOSC0   12000000

Osc0 frequency: Hz.

Referenced by clockfrequencies_configure().

#define FOSC32   32768

Osc32 frequency: Hz.

#define GPIO_PUSH_BUTTON_SW0   AVR32_PIN_PB00
#define GPIO_PUSH_BUTTON_SW0_PRESSED   0
#define GPIO_PUSH_BUTTON_SW1   AVR32_PIN_PB01
#define GPIO_PUSH_BUTTON_SW1_PRESSED   0
#define GPIO_PUSH_BUTTON_SW2   AVR32_PIN_PB02
#define GPIO_PUSH_BUTTON_SW2_PRESSED   0
#define GPIO_PUSH_BUTTON_SW3   AVR32_PIN_PB03
#define GPIO_PUSH_BUTTON_SW3_PRESSED   0
#define GPIO_PUSH_BUTTON_SW4   AVR32_PIN_PB04
#define GPIO_PUSH_BUTTON_SW4_PRESSED   0
#define GPIO_PUSH_BUTTON_SW5   AVR32_PIN_PB05
#define GPIO_PUSH_BUTTON_SW5_PRESSED   0
#define GPIO_PUSH_BUTTON_SW6   AVR32_PIN_PB06
#define GPIO_PUSH_BUTTON_SW6_PRESSED   0
#define GPIO_PUSH_BUTTON_SW7   AVR32_PIN_PB07
#define GPIO_PUSH_BUTTON_SW7_PRESSED   0
#define LED0_GPIO   AVR32_PIN_PA04
#define LED1_GPIO   AVR32_PIN_PA05
#define LED2_GPIO   AVR32_PIN_PA06
#define LED3_GPIO   AVR32_PIN_PA07
#define LED4_GPIO   AVR32_PIN_PA10
#define LED5_GPIO   AVR32_PIN_PA11
#define LED6_GPIO   AVR32_PIN_PA12
#define LED7_GPIO   AVR32_PIN_PA13
#define LED_COUNT   4

Number of LEDs.

Referenced by LED_Display(), LED_Display_Mask(), LED_Off(), LED_On(), and LED_Toggle().

#define OSC0_STARTUP   AVR32_SCIF_OSCCTRL0_STARTUP_2048_RCOSC

Osc0 startup time: RCOsc periods.

Referenced by clockfrequencies_configure().

#define OSC32_STARTUP   AVR32_SCIF_OSCCTRL32_STARTUP_8192_RCOSC

Osc32 startup time: RCOsc periods.