Functions | |
int | main (void) |
Main function to alter the state of the pin GPIO_PIN_EXAMPLE . More... | |
int main | ( | void | ) |
Main function to alter the state of the pin GPIO_PIN_EXAMPLE
.
References gpio_clr_gpio_pin(), gpio_get_pin_value(), GPIO_PIN_EXAMPLE_1, GPIO_PIN_EXAMPLE_2, GPIO_PIN_EXAMPLE_3, gpio_set_gpio_pin(), and gpio_tgl_gpio_pin().