Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
MEMORY - MDMA - Memory DMA Controller

This driver interfaces the MDMA (Memory Direct Memory Access Controller) which performs memory-to-memory transfers with as little CPU intervention as possible.

Data Structures

struct  mdma_descriptor_t
 MDMA Descriptor Structure Definition. More...
 
struct  mdma_interrupt_t
 MDMA interrupts. More...
 
struct  mdma_opt_t
 MDMA Option Settings. More...
 

Macros

#define MDMA_DEFAULT_TIMEOUT   10000
 Default time-out value (number of attempts). More...
 
#define MDMA_INVALID_ARGUMENT   (-1)
 MDMA driver functions return value in case of invalid argument(s). More...
 

Functions

int mdma_channels_is_enable (volatile avr32_mdma_t *mdma, U32 channels)
 Check if a DMA Transfer for a Channel is enable. More...
 
void mdma_configure_interrupts (volatile avr32_mdma_t *mdma, const mdma_interrupt_t *bitfield)
 Enables various MDMA interrupts. More...
 
void mdma_descriptor_mode_xfert_init (volatile avr32_mdma_t *mdma, U32 channel, U32 *start_adress)
 Init a Descriptor Mode Transfer for a Channel. More...
 
unsigned long mdma_get_interrupt_settings (volatile avr32_mdma_t *mdma)
 MDMA interrupt settings. More...
 
void mdma_single_mode_xfert_init (volatile avr32_mdma_t *mdma, U32 channel, const mdma_opt_t *opt, U32 *src, U32 *dest)
 Init a Single Mode Transfer for a Channel. More...
 
void mdma_start_descriptor_xfert (volatile avr32_mdma_t *mdma, U32 channels, U8 arbitration)
 Start a Descriptor DMA Transfer for a Channel. More...
 
void mdma_start_single_xfert (volatile avr32_mdma_t *mdma, U32 channels, U8 arbitration)
 Start a Single DMA Transfer for a Channel. More...
 
int mdma_stop_channels (volatile avr32_mdma_t *mdma, U32 channels)
 Stop a DMA Transfer for a Channel. More...
 

Return Values

#define MDMA_SUCCESS   0
 Successful completion. More...
 
#define MDMA_FAILURE   -1
 Failure because of some unspecified reason. More...
 

MDMA Transfer Size

#define MDMA_TRANSFERT_SIZE_BYTE   (0)
 
#define MDMA_TRANSFERT_SIZE_HLFW   (1)
 
#define MDMA_TRANSFERT_SIZE_WORD   (2)
 

MDMA Channel Mode

#define MDMA_SINGLE_TRANSFERT_MODE   (0)
 
#define MDMA_DESCRIPTOR_MODE   (1)
 

MDMA Arbitration Mode

#define MDMA_FIXED_PRIORITY_MODE   (0)
 
#define MDMA_ROUND_ROBIN_MODE   (1)
 

MDMA Burst Transfer Size

#define MDMA_SINGLE_TRANSFER_BURST   (0)
 
#define MDMA_4_BEAT_BURST   (1)
 
#define MDMA_8_BEAT_BURST   (2)
 
#define MDMA_16_BEAT_BURST   (3)
 

#define MDMA_16_BEAT_BURST   (3)
#define MDMA_4_BEAT_BURST   (1)
#define MDMA_8_BEAT_BURST   (2)
#define MDMA_DEFAULT_TIMEOUT   10000

Default time-out value (number of attempts).

Referenced by mdma_stop_channels().

#define MDMA_DESCRIPTOR_MODE   (1)
#define MDMA_FAILURE   -1

Failure because of some unspecified reason.

Referenced by mdma_channels_is_enable(), and mdma_stop_channels().

#define MDMA_FIXED_PRIORITY_MODE   (0)

Referenced by main().

#define MDMA_INVALID_ARGUMENT   (-1)

MDMA driver functions return value in case of invalid argument(s).

#define MDMA_ROUND_ROBIN_MODE   (1)
#define MDMA_SINGLE_TRANSFER_BURST   (0)
#define MDMA_SINGLE_TRANSFERT_MODE   (0)
#define MDMA_SUCCESS   0

Successful completion.

Referenced by mdma_channels_is_enable(), and mdma_stop_channels().

#define MDMA_TRANSFERT_SIZE_BYTE   (0)
#define MDMA_TRANSFERT_SIZE_HLFW   (1)
#define MDMA_TRANSFERT_SIZE_WORD   (2)

int mdma_channels_is_enable ( volatile avr32_mdma_t *  mdma,
U32  channels 
)

Check if a DMA Transfer for a Channel is enable.

Parameters
mdmaPointer to the MDMA instance to access.
channelsMDMA Channel to check
Return values
MDMA_SUCCESSif channel is enable.
MDMA_FAILUREif channel is disable.

References MDMA_FAILURE, and MDMA_SUCCESS.

void mdma_configure_interrupts ( volatile avr32_mdma_t *  mdma,
const mdma_interrupt_t bitfield 
)

Enables various MDMA interrupts.

Parameters
mdmaPointer to the MDMA instance to access.
bitfieldThe interrupt enable configuration.

References mdma_interrupt_t::berr0, mdma_interrupt_t::berr1, mdma_interrupt_t::berr2, mdma_interrupt_t::berr3, mdma_interrupt_t::ch0c, mdma_interrupt_t::ch1c, mdma_interrupt_t::ch2c, mdma_interrupt_t::ch3c, Disable_global_interrupt, Enable_global_interrupt, and Is_global_interrupt_enabled.

Referenced by main().

void mdma_descriptor_mode_xfert_init ( volatile avr32_mdma_t *  mdma,
U32  channel,
U32 start_adress 
)

Init a Descriptor Mode Transfer for a Channel.

Parameters
mdmaPointer to the MDMA instance to access.
channelMDMA Channel To configure
start_adressStart address of the buffer

Referenced by main().

unsigned long mdma_get_interrupt_settings ( volatile avr32_mdma_t *  mdma)

MDMA interrupt settings.

Parameters
mdmaPointer to the MDMA instance to access.
Return values
>=0The interrupt enable configuration organized according to mdma_interrupt_t.
InterruptSettings.
void mdma_single_mode_xfert_init ( volatile avr32_mdma_t *  mdma,
U32  channel,
const mdma_opt_t opt,
U32 src,
U32 dest 
)

Init a Single Mode Transfer for a Channel.

Parameters
mdmaPointer to the MDMA instance to access.
channelMDMA Channel To configure
optPointer to the MDMA option.
srcPointer to the source buffer.
destPointer to the destination buffer.

References mdma_opt_t::burst_size, mdma_opt_t::count, MDMA_SINGLE_TRANSFERT_MODE, mdma_opt_t::size, and mdma_opt_t::tc_ienable.

void mdma_start_descriptor_xfert ( volatile avr32_mdma_t *  mdma,
U32  channels,
U8  arbitration 
)

Start a Descriptor DMA Transfer for a Channel.

Parameters
mdmaPointer to the MDMA instance to access.
channelsMDMA Channel To configure
arbitrationPointer to the MDMA option.

References MDMA_DESCRIPTOR_MODE.

Referenced by main().

void mdma_start_single_xfert ( volatile avr32_mdma_t *  mdma,
U32  channels,
U8  arbitration 
)

Start a Single DMA Transfer for a Channel.

Parameters
mdmaPointer to the MDMA instance to access.
channelsMDMA Channel To configure
arbitrationPointer to the MDMA option.
int mdma_stop_channels ( volatile avr32_mdma_t *  mdma,
U32  channels 
)

Stop a DMA Transfer for a Channel.

Parameters
mdmaPointer to the MDMA instance to access.
channelsMDMA Channel To configure
Return values
MDMA_FAILURETimeout has expired/ MDMA_SUCCESS success.

References MDMA_DEFAULT_TIMEOUT, MDMA_FAILURE, and MDMA_SUCCESS.