Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
TWI - Two-Wire Master Interface

Driver for the TWIM (Two-Wire Master Interface).

This driver provides access to the main features of the TWIM controller. The TWIM interconnects components on a unique two-wire bus. The TWIM is programmable as a master with sequential or single-byte access. Multiple master capability is supported.

Data Structures

struct  twim_options_t
 Input parameters when initializing the twim module mode. More...
 
struct  twim_package_t
 Information concerning the data transmission. More...
 
struct  twim_transfer_t
 Information concerning the data transmission. More...
 

Macros

#define AVR32_TWIM_IER_NAK_MASK
 Interrupt Enable Register Mask for No Acknowledgements. More...
 
#define AVR32_TWIM_IER_STD_MASK
 Frequently used Interrupt Enable Register Mask. More...
 
#define AVR32_TWIM_SCR_NAK_MASK
 Status Clear Register Mask for No Acknowledgements. More...
 
#define AVR32_TWIM_SR_NAK_MASK
 Status Register Mask for No Acknowledgements. More...
 
#define AVR32_TWIM_SR_STD_MASK
 Frequently used Status Clear Register Mask. More...
 
#define TWI_FAST_MODE_SPEED   (400000 /* kbit/s */)
 TWI Fast Mode. More...
 
#define TWI_STD_MODE_SPEED   (100000 /* kbit/s */)
 

Functions

static status_code_t twi_master_read (volatile avr32_twi_t *twim, const twi_package_t *package)
 Compatibility with TWI Module driver for read operation. More...
 
static status_code_t twi_master_write (volatile avr32_twi_t *twim, const twi_package_t *package)
 Compatibility with TWI Module drivers for write operation. More...
 
status_code_t twim_chained_transfer (volatile avr32_twim_t *twim, volatile twim_transfer_t *first, volatile twim_transfer_t *second, bool tenbit)
 Perform Chained transfers to a TWI compatible slave device. More...
 
void twim_disable_interrupt (volatile avr32_twim_t *twim)
 Disable the TWI interrupts and clear its status register. More...
 
static void twim_master_disable (volatile avr32_twim_t *twim)
 Disable Master Mode of the TWI. More...
 
static void twim_master_enable (volatile avr32_twim_t *twim)
 Enable Master Mode of the TWI. More...
 
status_code_t twim_master_init (volatile avr32_twim_t *twim, const twim_options_t *opt)
 Initialize the twi master module. More...
 
status_code_t twim_probe (volatile avr32_twim_t *twim, uint32_t chip_addr)
 Test if a chip answers for a given twi address. More...
 
status_code_t twim_read (volatile avr32_twim_t *twim, uint8_t *buffer, uint32_t nbytes, uint32_t saddr, bool tenbit)
 Read multiple bytes from a TWI compatible slave device. More...
 
status_code_t twim_read_packet (volatile avr32_twim_t *twim, const twim_package_t *package)
 Read multiple bytes from a TWI compatible slave device. More...
 
status_code_t twim_set_speed (volatile avr32_twim_t *twim, uint32_t speed, uint32_t pba_hz)
 Set the twim bus speed in conjunction with the clock frequency. More...
 
uint8_t twim_status (void)
 Information about the current status of the TWI Bus. More...
 
status_code_t twim_write (volatile avr32_twim_t *twim, const uint8_t *buffer, uint32_t nbytes, uint32_t saddr, bool tenbit)
 Write multiple bytes to a TWI compatible slave device. More...
 
status_code_t twim_write_packet (volatile avr32_twim_t *twim, const twim_package_t *package)
 Write multiple bytes to a TWI compatible slave device. More...
 

TWI Driver Compatibility

Codes for UC3 devices using TWI modules can easily be ported to UC3 devices with TWIM module

#define avr32_twi_t   avr32_twim_t
 
#define twi_options_t   twim_options_t
 
#define twi_package_t   twim_package_t
 
#define twi_master_init   twim_master_init
 
#define twi_probe   twim_probe
 
enum  twim_transfer_status {
  TWI_SUCCESS = 0,
  TWI_INVALID_ARGUMENT = -1,
  TWI_ARBITRATION_LOST = -2,
  TWI_NO_CHIP_FOUND = -3,
  TWI_RECEIVE_NACK = -4,
  TWI_SEND_NACK = -5,
  TWI_INVALID_CLOCK_DIV = -6
}
 Status Codes for TWI Transfer. More...
 
typedef enum twim_transfer_status twim_transfer_status_t
 

#define avr32_twi_t   avr32_twim_t
#define AVR32_TWIM_IER_NAK_MASK
Value:
(AVR32_TWIM_IER_ANAK_MASK \
| AVR32_TWIM_IER_DNAK_MASK)

Interrupt Enable Register Mask for No Acknowledgements.

Referenced by ISR(), and twim_write().

#define AVR32_TWIM_IER_STD_MASK
Value:
| AVR32_TWIM_IER_ARBLST_MASK)
#define AVR32_TWIM_IER_NAK_MASK
Interrupt Enable Register Mask for No Acknowledgements.
Definition: twim.h:79

Frequently used Interrupt Enable Register Mask.

Referenced by twim_read(), twim_read_packet(), and twim_write_packet().

#define AVR32_TWIM_SCR_NAK_MASK
Value:
(AVR32_TWIM_SCR_ANAK_MASK \
| AVR32_TWIM_SCR_DNAK_MASK)

Status Clear Register Mask for No Acknowledgements.

Referenced by twim_chained_transfer().

#define AVR32_TWIM_SR_NAK_MASK
Value:
(AVR32_TWIM_SR_ANAK_MASK \
| AVR32_TWIM_SR_DNAK_MASK)

Status Register Mask for No Acknowledgements.

Referenced by twim_chained_transfer().

#define AVR32_TWIM_SR_STD_MASK
Value:
| AVR32_TWIM_SR_ARBLST_MASK)
#define AVR32_TWIM_SR_NAK_MASK
Status Register Mask for No Acknowledgements.
Definition: twim.h:76

Frequently used Status Clear Register Mask.

Referenced by ISR().

#define TWI_FAST_MODE_SPEED   (400000 /* kbit/s */)

TWI Fast Mode.

#define twi_master_init   twim_master_init

Referenced by twi_init().

#define twi_options_t   twim_options_t

Referenced by twi_init().

#define twi_probe   twim_probe
#define TWI_STD_MODE_SPEED   (100000 /* kbit/s */)

TWI Standard Mode

Status Codes for TWI Transfer.

Enumerator
TWI_SUCCESS 

TWI Transaction Success.

TWI_INVALID_ARGUMENT 

Invalid Argument Passed.

TWI_ARBITRATION_LOST 

Bus Arbitration Lost.

TWI_NO_CHIP_FOUND 

Slave Not Found.

TWI_RECEIVE_NACK 

Data No Acknowledgement Received.

TWI_SEND_NACK 

Data No Acknowledgement Send.

TWI_INVALID_CLOCK_DIV 

Invalid Clock Divider Value.

static status_code_t twi_master_read ( volatile avr32_twi_t twim,
const twi_package_t package 
)
inlinestatic

Compatibility with TWI Module driver for read operation.

Parameters
twimBase address of the TWIM (i.e. &AVR32_TWIM).
packagePackage information and data (see twim_package_t)
Returns
STATUS_OK If all bytes were read, error code otherwise

References twim_read_packet().

Referenced by at42qt1060_get_status(), and at42qt1060_read_reg().

static status_code_t twi_master_write ( volatile avr32_twi_t twim,
const twi_package_t package 
)
inlinestatic

Compatibility with TWI Module drivers for write operation.

Parameters
twimBase address of the TWIM (i.e. &AVR32_TWI).
*packagePackage information and data (see twim_package_t)
Returns
STATUS_OK if all bytes were written, error code otherwise

References twim_write_packet().

Referenced by at42qt1060_read_reg(), and at42qt1060_write_reg().

status_code_t twim_chained_transfer ( volatile avr32_twim_t *  twim,
volatile twim_transfer_t first,
volatile twim_transfer_t second,
bool  tenbit 
)

Perform Chained transfers to a TWI compatible slave device.

Parameters
twimBase address of the TWIM (i.e. &AVR32_TWIM)
*firstInformation regarding first transfer
*secondInformation regarding second transfer (see twim_transfer_t)
tenbitTo enable tenbit addressing
Return values
STATUS_OKChain transfer successful
ERR_IO_ERRORNACK received or Bus Arbitration lost

References AVR32_TWIM_SCR_NAK_MASK, AVR32_TWIM_SR_NAK_MASK, twim_transfer_t::buffer, twim_transfer_t::chip, cpu_relax, ERR_IO_ERROR, twim_transfer_t::length, twim_transfer_t::read, STATUS_OK, transfer_status, TWI_SUCCESS, twim_disable_interrupt(), twim_inst, twim_next, twim_rx_data, twim_tx_data, and twim_tx_nb_bytes.

void twim_disable_interrupt ( volatile avr32_twim_t *  twim)

Disable the TWI interrupts and clear its status register.

Parameters
twimBase address of the TWIM (i.e. &AVR32_TWI).

References cpu_irq_disable, cpu_irq_is_enabled, and UL.

Referenced by twim_chained_transfer(), twim_read(), twim_read_packet(), twim_write(), and twim_write_packet().

static void twim_master_disable ( volatile avr32_twim_t *  twim)
inlinestatic

Disable Master Mode of the TWI.

Parameters
twimBase address of the TWI instance.
static void twim_master_enable ( volatile avr32_twim_t *  twim)
inlinestatic

Enable Master Mode of the TWI.

Parameters
twimBase address of the TWI instance.
status_code_t twim_master_init ( volatile avr32_twim_t *  twim,
const twim_options_t opt 
)

Initialize the twi master module.

Parameters
twimBase address of the TWIM (i.e. &AVR32_TWIM)
*optOptions for initializing the twim module (see twim_options_t)
Return values
STATUS_OKTransaction is successful
ERR_INVALID_ARGInvalid arg resulting in wrong CWGR Exponential
ERR_IO_ERRORNACK is received or Bus Arbitration lost

References twim_options_t::chip, CONF_TWIM_IRQ_LEVEL, CONF_TWIM_IRQ_LINE, cpu_irq_disable, cpu_irq_enable, cpu_irq_is_enabled, cpu_irq_restore(), cpu_irq_save(), ERR_INVALID_ARG, ERR_IO_ERROR, irq_register_handler, twim_options_t::pba_hz, twim_options_t::smbus, twim_options_t::speed, STATUS_OK, transfer_status, TWI_ARBITRATION_LOST, TWI_RECEIVE_NACK, TWI_SUCCESS, twim_probe(), twim_set_speed(), and UL.

status_code_t twim_probe ( volatile avr32_twim_t *  twim,
uint32_t  chip_addr 
)

Test if a chip answers for a given twi address.

Parameters
twimBase address of the TWIM (i.e. &AVR32_TWIM)
chip_addrAddress of the chip which is searched for
Return values
STATUS_OKSlave Found
ERR_IO_ERRORANAK received or Bus Arbitration lost

References twim_write().

Referenced by twim_master_init().

status_code_t twim_read ( volatile avr32_twim_t *  twim,
uint8_t *  buffer,
uint32_t  nbytes,
uint32_t  saddr,
bool  tenbit 
)

Read multiple bytes from a TWI compatible slave device.

Parameters
twimBase address of the TWIM (i.e. &AVR32_TWIM)
*bufferReceived data
nbytesNumber of bytes to be transmitted
saddrSlave address
tenbitTen bit addressing
Return values
STATUS_OKIf all bytes were read successfully
ERR_IO_ERRORNACK received or Bus Arbitration lost

References AVR32_TWIM_IER_STD_MASK, cpu_irq_enable, cpu_relax, ERR_IO_ERROR, STATUS_OK, transfer_status, TWI_ARBITRATION_LOST, TWI_RECEIVE_NACK, TWI_SUCCESS, twim_disable_interrupt(), twim_inst, twim_it_mask, twim_next, twim_rx_data, twim_rx_nb_bytes, and twim_status().

status_code_t twim_read_packet ( volatile avr32_twim_t *  twim,
const twim_package_t package 
)

Read multiple bytes from a TWI compatible slave device.

Parameters
twimBase address of the TWIM (i.e. &AVR32_TWIM)
packagePackage information and data (see twim_package_t)
Return values
STATUS_OKIf all bytes were read successfully
ERR_IO_ERRORNACK received or Bus Arbitration lost

References twim_package_t::addr, twim_package_t::addr_length, AVR32_TWIM_IER_STD_MASK, twim_package_t::buffer, twim_package_t::chip, cpu_irq_enable, cpu_relax, ERR_IO_ERROR, twim_package_t::length, STATUS_OK, transfer_status, TWI_ARBITRATION_LOST, TWI_RECEIVE_NACK, TWI_SUCCESS, twim_disable_interrupt(), twim_inst, twim_it_mask, twim_next, twim_rx_data, twim_rx_nb_bytes, twim_status(), twim_tx_data, and twim_tx_nb_bytes.

Referenced by twi_master_read().

status_code_t twim_set_speed ( volatile avr32_twim_t *  twim,
uint32_t  speed,
uint32_t  pba_hz 
)

Set the twim bus speed in conjunction with the clock frequency.

Parameters
twimBase address of the TWIM (i.e. &AVR32_TWIM).
speedThe desired twim bus speed
pba_hzThe current running PBA clock frequency
Return values
STATUS_OKTransaction is successful
ERR_INVALID_ARGInvalid arg resulting in wrong CWGR Exponential

References ERR_INVALID_ARG, and STATUS_OK.

Referenced by twim_master_init().

uint8_t twim_status ( void  )

Information about the current status of the TWI Bus.

References twim_inst.

Referenced by twim_read(), twim_read_packet(), twim_write(), and twim_write_packet().

status_code_t twim_write ( volatile avr32_twim_t *  twim,
uint8_t const *  buffer,
uint32_t  nbytes,
uint32_t  saddr,
bool  tenbit 
)

Write multiple bytes to a TWI compatible slave device.

Parameters
twimBase address of the TWIM (i.e. &AVR32_TWIM).
*bufferData to be transmitted
nbytesNumber of bytes to be transmitted
saddrSlave address
tenbitTen bit addressing
Return values
STATUS_OKIf all bytes were send successfully
ERR_IO_ERRORNACK received or Bus Arbitration lost

References AVR32_TWIM_IER_NAK_MASK, cpu_irq_enable, cpu_relax, ERR_IO_ERROR, STATUS_OK, transfer_status, TWI_ARBITRATION_LOST, TWI_RECEIVE_NACK, TWI_SUCCESS, twim_disable_interrupt(), twim_inst, twim_it_mask, twim_next, twim_status(), twim_tx_data, and twim_tx_nb_bytes.

Referenced by twim_probe().

status_code_t twim_write_packet ( volatile avr32_twim_t *  twim,
const twim_package_t package 
)

Write multiple bytes to a TWI compatible slave device.

Parameters
twimBase address of the TWIM (i.e. &AVR32_TWIM)
*packagePackage information and data (see twim_package_t)
Return values
STATUS_OKIf all bytes were send successfully
ERR_IO_ERRORNACK received or Bus Arbitration lost

References twim_package_t::addr, twim_package_t::addr_length, AVR32_TWIM_IER_STD_MASK, twim_package_t::buffer, twim_package_t::chip, cpu_irq_enable, cpu_relax, ERR_IO_ERROR, twim_package_t::length, STATUS_OK, transfer_status, TWI_ARBITRATION_LOST, TWI_RECEIVE_NACK, TWI_SUCCESS, twim_disable_interrupt(), twim_inst, twim_it_mask, twim_next, twim_status(), twim_tx_data, and twim_tx_nb_bytes.

Referenced by twi_master_write().