Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
QDEC - Quadrature Decoder

Driver for the QDEC (Quadrature Decoder).

The QDEC handles three input channels: two phase signals (QEPA, QEPB) and one index pulse (QEPI). It has a 16-bit position counter and a 16-bit revolution counter and supports 32-bit timer/counter mode.

Data Structures

struct  qdec_interrupt_t
 QDEC interrupts. More...
 
struct  qdec_quadrature_decoder_opt_t
 Parameters when initializing a QDEC in Quadrature Decoder mode. More...
 
struct  qdec_timer_opt_t
 Parameters when initializing a QDEC in Counter mode. More...
 

Macros

#define QDEC_INVALID_ARGUMENT   (-1)
 QDEC driver functions return value in case of invalid argument(s). More...
 
#define QDEC_QDEC_MODE   1
 QDEC Mode Selection. More...
 
#define QDEC_TIMER_MODE   0
 TIMER Mode Selection. More...
 
#define QDEC_TSIR_DOWN   1
 Direction Down In TIMER Mode. More...
 
#define QDEC_TSIR_UP   0
 Direction Up In TIMER Mode. More...
 
#define QDEC_UPD_EVNT   1
 EVENT Changes Input In TIMER Mode. More...
 
#define QDEC_UPD_TSDIR   0
 TSDIR Changes Input In TIMER Mode. More...
 

Functions

int qdec_configure_interrupts (volatile avr32_qdec_t *qdec, const qdec_interrupt_t *bitfield)
 Enables various QDEC interrupts. More...
 
int qdec_get_interrupt_settings (volatile avr32_qdec_t *qdec)
 Get the QDEC current interrupt settings. More...
 
int qdec_init_quadrature_decoder_mode (volatile avr32_qdec_t *qdec, const qdec_quadrature_decoder_opt_t *opt)
 Sets options for QDEC quadrature decoder initialization. More...
 
int qdec_init_timer_mode (volatile avr32_qdec_t *qdec, const qdec_timer_opt_t *opt)
 Sets options for QDEC Timer mode initialization. More...
 
unsigned short int qdec_read_pc (volatile avr32_qdec_t *qdec)
 Read value of the channel's QDEC Position Current Counter register. More...
 
unsigned short int qdec_read_pc_cap (volatile avr32_qdec_t *qdec)
 Read value of the channel's QDEC Position Capture Counter register. More...
 
unsigned short int qdec_read_rc (volatile avr32_qdec_t *qdec)
 Read value of the channel's QDEC Revolution Current Counter register. More...
 
unsigned short int qdec_read_rc_cap (volatile avr32_qdec_t *qdec)
 Read value of the channel's QDEC Revolution Capture register. More...
 
int qdec_software_trigger (volatile avr32_qdec_t *qdec)
 Software Trigger Condition to start QDEC service. More...
 
int qdec_stop (volatile avr32_qdec_t *qdec)
 Stops a QDEC. More...
 
unsigned short int qdec_write_pc_cmp (volatile avr32_qdec_t *qdec, unsigned short int value)
 Writes a value to the channel's QDEC Position Counter Compare register. More...
 
unsigned short int qdec_write_pc_cnt (volatile avr32_qdec_t *qdec, unsigned short int value)
 Write value of the channel's QDEC Position Current Counter register. More...
 
unsigned short int qdec_write_pc_top (volatile avr32_qdec_t *qdec, unsigned short int value)
 Writes a value to the channel's QDEC Position Counter Top register. More...
 
unsigned short int qdec_write_rc_cmp (volatile avr32_qdec_t *qdec, unsigned short int value)
 Writes a value to the channel's QDEC Revolution Counter Compare register. More...
 
unsigned short int qdec_write_rc_cnt (volatile avr32_qdec_t *qdec, unsigned short int value)
 Write value of the channel's QDEC Revolution Current Counter register. More...
 
unsigned short int qdec_write_rc_top (volatile avr32_qdec_t *qdec, unsigned short int value)
 Writes a value to the channel's QDEC Revolution Counter Top register. More...
 

QDEC Index Phase Detection

#define QDEC_IDXPHS_QEPB_0_QEPA_0
 
#define QDEC_IDXPHS_QEPB_0_QEPA_1
 
#define QDEC_IDXPHS_QEPB_1_QEPA_0
 
#define QDEC_IDXPHS_QEPB_1_QEPA_1
 

#define QDEC_IDXPHS_QEPB_0_QEPA_0
#define QDEC_IDXPHS_QEPB_0_QEPA_1
#define QDEC_IDXPHS_QEPB_1_QEPA_0
#define QDEC_IDXPHS_QEPB_1_QEPA_1
#define QDEC_INVALID_ARGUMENT   (-1)

QDEC driver functions return value in case of invalid argument(s).

#define QDEC_QDEC_MODE   1

QDEC Mode Selection.

#define QDEC_TIMER_MODE   0

TIMER Mode Selection.

#define QDEC_TSIR_DOWN   1

Direction Down In TIMER Mode.

Referenced by main().

#define QDEC_TSIR_UP   0

Direction Up In TIMER Mode.

#define QDEC_UPD_EVNT   1

EVENT Changes Input In TIMER Mode.

#define QDEC_UPD_TSDIR   0

TSDIR Changes Input In TIMER Mode.

int qdec_configure_interrupts ( volatile avr32_qdec_t *  qdec,
const qdec_interrupt_t bitfield 
)

Enables various QDEC interrupts.

Parameters
qdecPointer to the QDEC instance to access.
bitfieldThe interrupt enable configuration.
Return values
0Success.

References AVR32_ENTER_CRITICAL_REGION, AVR32_LEAVE_CRITICAL_REGION, qdec_interrupt_t::cap, qdec_interrupt_t::cmp, qdec_interrupt_t::dirinv, qdec_interrupt_t::idexerr, qdec_interrupt_t::ovr, qdec_interrupt_t::pcro, qdec_interrupt_t::qepi, and qdec_interrupt_t::rcro.

Referenced by main().

int qdec_get_interrupt_settings ( volatile avr32_qdec_t *  qdec)

Get the QDEC current interrupt settings.

Parameters
qdecPointer to the QDEC instance to access.
Return values
>=0The interrupt enable configuration organized according to qdec_interrupt_t.
InterruptSettings Value.
int qdec_init_quadrature_decoder_mode ( volatile avr32_qdec_t *  qdec,
const qdec_quadrature_decoder_opt_t opt 
)
int qdec_init_timer_mode ( volatile avr32_qdec_t *  qdec,
const qdec_timer_opt_t opt 
)

Sets options for QDEC Timer mode initialization.

Parameters
qdecPointer to the QDEC instance to access.
optOptions for quadrature decoder mode.
Return values
0Success.

References qdec_timer_opt_t::evtrge, qdec_timer_opt_t::filten, qdec_timer_opt_t::pcce, qdec_timer_opt_t::rcce, qdec_timer_opt_t::tsdir, and qdec_timer_opt_t::upd.

Referenced by main().

unsigned short int qdec_read_pc ( volatile avr32_qdec_t *  qdec)

Read value of the channel's QDEC Position Current Counter register.

Parameters
qdecPointer to the QDEC instance to access.
Return values
>=0Status register value.
unsigned short int qdec_read_pc_cap ( volatile avr32_qdec_t *  qdec)

Read value of the channel's QDEC Position Capture Counter register.

Parameters
qdecPointer to the QDEC instance to access.
Return values
>=0Status register value.
QDEC_INVALID_ARGUMENTInvalid argument(s).
unsigned short int qdec_read_rc ( volatile avr32_qdec_t *  qdec)

Read value of the channel's QDEC Revolution Current Counter register.

Parameters
qdecPointer to the QDEC instance to access.
Return values
>=0Status register value.
unsigned short int qdec_read_rc_cap ( volatile avr32_qdec_t *  qdec)

Read value of the channel's QDEC Revolution Capture register.

Parameters
qdecPointer to the QDEC instance to access.
Return values
>=0Status register value.
QDEC_INVALID_ARGUMENTInvalid argument(s).
int qdec_software_trigger ( volatile avr32_qdec_t *  qdec)

Software Trigger Condition to start QDEC service.

Parameters
qdecPointer to the QDEC instance to access.
Return values
0Success.

Referenced by main().

int qdec_stop ( volatile avr32_qdec_t *  qdec)

Stops a QDEC.

Parameters
qdecPointer to the QDEC instance to access.
Return values
0Success.
unsigned short int qdec_write_pc_cmp ( volatile avr32_qdec_t *  qdec,
unsigned short int  value 
)

Writes a value to the channel's QDEC Position Counter Compare register.

Parameters
qdecPointer to the QDEC instance to access.
valueValue to write to the RC register.
Return values
>=0Written value.
QDEC_INVALID_ARGUMENTInvalid argument(s).

Referenced by main().

unsigned short int qdec_write_pc_cnt ( volatile avr32_qdec_t *  qdec,
unsigned short int  value 
)

Write value of the channel's QDEC Position Current Counter register.

Parameters
qdecPointer to the QDEC instance to access.
valueValue to write to the PC register.
Return values
>=0Status register value.

Referenced by main(), and qdec_int_handler().

unsigned short int qdec_write_pc_top ( volatile avr32_qdec_t *  qdec,
unsigned short int  value 
)

Writes a value to the channel's QDEC Position Counter Top register.

Parameters
qdecPointer to the QDEC instance to access.
valueValue to write to the RC register.
Return values
>=0Written value.
QDEC_INVALID_ARGUMENTInvalid argument(s).
unsigned short int qdec_write_rc_cmp ( volatile avr32_qdec_t *  qdec,
unsigned short int  value 
)

Writes a value to the channel's QDEC Revolution Counter Compare register.

Parameters
qdecPointer to the QDEC instance to access.
valueValue to write to the RC register.
Return values
>=0Written value.
QDEC_INVALID_ARGUMENTInvalid argument(s).

Referenced by main().

unsigned short int qdec_write_rc_cnt ( volatile avr32_qdec_t *  qdec,
unsigned short int  value 
)

Write value of the channel's QDEC Revolution Current Counter register.

Parameters
qdecPointer to the QDEC instance to access.
valueValue to write to the RC register.
Return values
>=0Status register value.

Referenced by main(), and qdec_int_handler().

unsigned short int qdec_write_rc_top ( volatile avr32_qdec_t *  qdec,
unsigned short int  value 
)

Writes a value to the channel's QDEC Revolution Counter Top register.

Parameters
qdecPointer to the QDEC instance to access.
valueValue to write to the RC register.
Return values
>=0Written value.