This is the documentation for the data structures, functions, variables, defines, enums, and typedefs for the SCIF driver.
It also gives an example of usage of the SCIF & PM module on UC3 products. This example shows how to configure the System Control Interface(SCIF) to:
This software was written for the GNU GCC for AVR32 and IAR Systems compiler for AVR32. Other compilers may or may not work.
All AVR32 devices with a PM module and a SCIF module can be used. This example has been tested with the following setup:
CPU speed: 115 kHz
On the STK600 + RCUC3L0 setup and also on the AT32UC3L-EK setup, the generic clock is output to the GCLK_1_0 pin. This is the GPIO pin 6/pin pa06/pin#10 on a UC3L QFP48 package. For the RCUC3L0 routing card, this pin is mapped on STK600.PORTA.PA6.
For more info about Atmel AVR32 visit Atmel AVR32
Support and FAQ: https://www.microchip.com/support/