This documents data structures, functions, variables, defines, enums, and typedefs in the software for application note AVR32x. It also gives an example of the usage of the SSC driver generating I2S output.
This software was written for the GNU GCC for AVR32 and IAR Systems compiler for AVR32. Other compilers may or may not work.
All AVR32 devices with an SSC module can be used. This example has been tested with the following setup:
CPU speed: 12 MHz
The SSC bus located on the EVK1100/EVK1101 board must be connected to an Audio Codec.
For further information, visit Atmel AVR32.