Clocks Management | |
enum | pcl_osc_t { PCL_OSC0 = 0, PCL_OSC1 = 1 } |
The different oscillators. More... | |
enum | pcl_dfll_t { PCL_DFLL0 = 0, PCL_DFLL1 = 1 } |
The different DFLLs. More... | |
enum | pcl_mainclk_t { PCL_MC_RCSYS, PCL_MC_OSC0, PCL_MC_OSC1, PCL_MC_OSC0_PLL0, PCL_MC_OSC1_PLL0, PCL_MC_OSC0_PLL1, PCL_MC_OSC1_PLL1, PCL_MC_DFLL0, PCL_MC_DFLL1, PCL_MC_RC120M, PCL_MC_RC8M, PCL_MC_CRIPOSC } |
Possible Main Clock Sources. More... | |
long int | pcl_configure_clocks (pcl_freq_param_t *param) |
Automatically configure the CPU, PBA, PBB, and HSB clocks. More... | |
long int | pcl_configure_clocks_rcsys (pcl_freq_param_t *param) |
Automatically configure the CPU, PBA, PBB, and HSB clocks using the RCSYS osc as main source clock. More... | |
long int | pcl_configure_clocks_rc120m (pcl_freq_param_t *param) |
Automatically configure the CPU, PBA, PBB, and HSB clocks using the RC120M osc as main source clock. More... | |
long int | pcl_configure_clocks_osc0 (pcl_freq_param_t *param) |
Automatically configure the CPU, PBA, PBB, and HSB clocks using the OSC0 osc as main source clock. More... | |
long int | pcl_configure_clocks_dfll0 (pcl_freq_param_t *param) |
Automatically configure the CPU, PBA, PBB, and HSB clocks using the DFLL0 as main source clock. More... | |
long int | pcl_switch_to_osc (pcl_osc_t osc, unsigned int fcrystal, unsigned int startup) |
Switch the main clock source to Osc0 configured in crystal mode. More... | |
long int | pcl_configure_usb_clock (void) |
Configure the USB Clock. More... | |
#define | pcl_freq_param_t pm_freq_param_t |
Input and output parameters to configure clocks with pcl_configure_clocks(). More... | |
#define | PCL_NOT_SUPPORTED (-10000) |
Define "not supported" for the lib. More... | |
#define | pcl_enable_module(module) pm_enable_module(&AVR32_PM, module) |
Enable the clock of a module. More... | |
#define | pcl_disable_module(module) pm_disable_module(&AVR32_PM, module) |
Disable the clock of a module. More... | |
Power Management | |
unsigned long | pcl_read_gplp (unsigned long gplp) |
Read the content of the GPLP registers. More... | |
void | pcl_write_gplp (unsigned long gplp, unsigned long value) |
Write into the GPLP registers. More... | |
#define pcl_disable_module | ( | module | ) | pm_disable_module(&AVR32_PM, module) |
Disable the clock of a module.
module | The module to shut down (use one of the defines in the part-specific header file under "toolchain folder"/avr32/inc(lude)/avr32/; depending on the clock domain, look for the sections "CPU clocks", "HSB clocks", "PBx clocks" or look in the module section). |
0 | Success. |
<0 | An error occurred. |
#define pcl_enable_module | ( | module | ) | pm_enable_module(&AVR32_PM, module) |
Enable the clock of a module.
module | The module to clock (use one of the defines in the part-specific header file under "toolchain folder"/avr32/inc(lude)/avr32/; depending on the clock domain, look for the sections "CPU clocks", "HSB clocks", "PBx clocks" or look in the module section). |
0 | Success. |
<0 | An error occurred. |
#define pcl_freq_param_t pm_freq_param_t |
Input and output parameters to configure clocks with pcl_configure_clocks().
#define PCL_NOT_SUPPORTED (-10000) |
Define "not supported" for the lib.
Referenced by pcl_configure_usb_clock(), and pcl_switch_to_osc().
enum pcl_dfll_t |
enum pcl_mainclk_t |
enum pcl_osc_t |
long int pcl_configure_clocks | ( | pcl_freq_param_t * | param | ) |
Automatically configure the CPU, PBA, PBB, and HSB clocks.
This function needs some parameters stored in a pcl_freq_param_t structure:
The CPU, HSB and PBA frequencies programmed after configuration are stored back into cpu_f and pba_f.
param | pointer on the configuration structure. |
0 | Success. |
<0 | The configuration cannot be performed. |
Automatically configure the CPU, PBA, PBB, and HSB clocks.
References pcl_configure_clocks_uc3l(), and pm_configure_clocks().
Referenced by main().
long int pcl_configure_clocks_dfll0 | ( | pcl_freq_param_t * | param | ) |
Automatically configure the CPU, PBA, PBB, and HSB clocks using the DFLL0 as main source clock.
This function needs some parameters stored in a pcl_freq_param_t structure:
Supported main clock sources: PCL_MC_DFLL0
Supported synchronous clocks frequencies: (these obviously depend on the DFLL target frequency; we'll take 100MHz as an example) 50MHz, 25MHz, 12.5MHz, 6.25MHz, 3.125MHz, 1562.5kHz, 781.25kHz, 390.625kHz.
param | pointer on the configuration structure. |
0 | Success. |
<0 | The configuration cannot be performed. |
References pcl_configure_synchronous_clocks().
Referenced by pcl_configure_clocks_uc3l().
long int pcl_configure_clocks_osc0 | ( | pcl_freq_param_t * | param | ) |
Automatically configure the CPU, PBA, PBB, and HSB clocks using the OSC0 osc as main source clock.
This function needs some parameters stored in a pcl_freq_param_t structure:
Supported main clock sources: PCL_MC_OSC0
Supported synchronous clocks frequencies: (these obviously depend on the OSC0 frequency; we'll take 16MHz as an example) 16MHz, 8MHz, 4MHz, 2MHz, 1MHz, 500kHz, 250kHz, 125kHz, 62.5kHz.
param | pointer on the configuration structure. |
0 | Success. |
<0 | The configuration cannot be performed. |
References pcl_configure_synchronous_clocks().
Referenced by pcl_configure_clocks_uc3l().
long int pcl_configure_clocks_rc120m | ( | pcl_freq_param_t * | param | ) |
Automatically configure the CPU, PBA, PBB, and HSB clocks using the RC120M osc as main source clock.
This function needs some parameters stored in a pcl_freq_param_t structure:
Supported main clock sources: PCL_MC_RC120M
Supported synchronous clocks frequencies: 30MHz, 15MHz, 7.5MHz, 3.75MHz, 1.875MHz, 937.5kHz, 468.75kHz.
param | pointer on the configuration structure. |
0 | Success. |
<0 | The configuration cannot be performed. |
References pcl_configure_synchronous_clocks().
Referenced by pcl_configure_clocks_uc3l().
long int pcl_configure_clocks_rcsys | ( | pcl_freq_param_t * | param | ) |
Automatically configure the CPU, PBA, PBB, and HSB clocks using the RCSYS osc as main source clock.
This function needs some parameters stored in a pcl_freq_param_t structure:
Supported main clock sources: PCL_MC_RCSYS
Supported synchronous clocks frequencies: 115200Hz, 57600Hz, 28800Hz, 14400Hz, 7200Hz, 3600Hz, 1800Hz, 900Hz, 450Hz.
param | pointer on the configuration structure. |
0 | Success. |
<0 | The configuration cannot be performed. |
References pcl_configure_synchronous_clocks().
Referenced by pcl_configure_clocks_uc3l().
long int pcl_configure_usb_clock | ( | void | ) |
Configure the USB Clock.
0 | Success. |
<0 | An error occurred. |
References AVR32_SCIF_GC_NO_DIV_CLOCK, AVR32_SCIF_GCLK_USBC, PASS, PCL_NOT_SUPPORTED, and pm_configure_usb_clock().
unsigned long pcl_read_gplp | ( | unsigned long | gplp | ) |
Read the content of the GPLP registers.
gplp | GPLP register index (0,1,... depending on the number of GPLP registers for a given part) |
long int pcl_switch_to_osc | ( | pcl_osc_t | osc, |
unsigned int | fcrystal, | ||
unsigned int | startup | ||
) |
Switch the main clock source to Osc0 configured in crystal mode.
osc | The oscillator to enable and switch to. |
fcrystal | Oscillator external crystal frequency (Hz) |
startup | Oscillator startup time. |
0 | Success. |
<0 | An error occurred. |
Switch the main clock source to Osc0 configured in crystal mode.
References flashc_set_flash_waitstate_and_readmode(), PASS, PCL_NOT_SUPPORTED, PCL_OSC0, and pm_switch_to_osc0().
Referenced by main().
void pcl_write_gplp | ( | unsigned long | gplp, |
unsigned long | value | ||
) |
Write into the GPLP registers.
gplp | GPLP register index (0,1,... depending on the number of GPLP registers for a given part) |
value | Value to write |