FLASHCDW interfaces a flash block with the 32-bit internal HSB bus.
Macros | |
#define | AVR32_FLASHCDW_REGIONS |
Number of flash regions defined by the FLASHCDW. More... | |
FLASHC Status | |
static unsigned int | flashcdw_error_status = 0 |
Sticky error status of the FLASHCDW. More... | |
static unsigned int | flashcdw_get_error_status (void) |
Gets the error status of the FLASHCDW. More... | |
Flash Properties | |
unsigned int | flashcdw_get_flash_size (void) |
Gets the size of the whole flash array. More... | |
unsigned int | flashcdw_get_page_count (void) |
Gets the total number of pages in the flash array. More... | |
unsigned int | flashcdw_get_page_count_per_region (void) |
Gets the number of pages in each flash region. More... | |
unsigned int | flashcdw_get_page_region (int page_number) |
Gets the region number of a page. More... | |
unsigned int | flashcdw_get_region_first_page_number (unsigned int region) |
Gets the number of the first page of a region. More... | |
FLASHCDW Control | |
unsigned int | flashcdw_get_wait_state (void) |
Gets the number of wait states of flash read accesses. More... | |
void | flashcdw_set_wait_state (unsigned int wait_state) |
Sets the number of wait states of flash read accesses. More... | |
void | flashcdw_set_flash_waitstate_and_readmode (unsigned long cpu_f_hz) |
Depending on the CPU frequency, set the wait states of flash read accesses and enable or disable the High speed read mode. More... | |
bool | flashcdw_is_ready_int_enabled (void) |
Tells whether the Flash Ready interrupt is enabled. More... | |
void | flashcdw_enable_ready_int (bool enable) |
Enables or disables the Flash Ready interrupt. More... | |
bool | flashcdw_is_lock_error_int_enabled (void) |
Tells whether the Lock Error interrupt is enabled. More... | |
void | flashcdw_enable_lock_error_int (bool enable) |
Enables or disables the Lock Error interrupt. More... | |
bool | flashcdw_is_prog_error_int_enabled (void) |
Tells whether the Programming Error interrupt is enabled. More... | |
void | flashcdw_enable_prog_error_int (bool enable) |
Enables or disables the Programming Error interrupt. More... | |
#define | flash_set_bus_freq(cpu_f_hz) flashcdw_set_flash_waitstate_and_readmode(cpu_f_hz) |
Alias on the flashcdw_set_flash_waitstate_and_readmode() function. More... | |
FLASHCDW Status | |
void(*volatile | flashcdw_wait_until_ready )(void) |
Pointer to the function used by the driver when it needs to wait until the FLASHCDW is ready to run a new command. More... | |
bool | flashcdw_is_ready (void) |
Tells whether the FLASHCDW is ready to run a new command. More... | |
void | flashcdw_default_wait_until_ready (void) |
Waits actively until the FLASHCDW is ready to run a new command. More... | |
bool | flashcdw_is_lock_error (void) |
Tells whether a Lock Error has occurred during the last function called that issued one or more FLASHCDW commands. More... | |
bool | flashcdw_is_programming_error (void) |
Tells whether a Programming Error has occurred during the last function called that issued one or more FLASHCDW commands. More... | |
bool | flashcdw_is_high_speed_enabled (void) |
Tells whether the High-speed read mode is enabled. More... | |
FLASHCDW Command Control | |
unsigned int | flashcdw_get_command (void) |
Gets the last issued FLASHCDW command. More... | |
unsigned int | flashcdw_get_page_number (void) |
Gets the current FLASHCDW page number. More... | |
void | flashcdw_issue_command (unsigned int command, int page_number) |
Issues a FLASHCDW command. More... | |
FLASHCDW Global Commands | |
void | flashcdw_no_operation (void) |
Issues a No Operation command to the FLASHCDW. More... | |
void | flashcdw_erase_all (void) |
Issues an Erase All command to the FLASHCDW. More... | |
FLASHCDW Protection Mechanisms | |
bool | flashcdw_is_security_bit_active (void) |
Tells whether the Security bit is active. More... | |
void | flashcdw_activate_security_bit (void) |
Activates the Security bit. More... | |
unsigned int | flashcdw_get_bootloader_protected_size (void) |
Gets the bootloader protected size. More... | |
unsigned int | flashcdw_set_bootloader_protected_size (unsigned int bootprot_size) |
Sets the bootloader protected size. More... | |
bool | flashcdw_is_external_privileged_fetch_locked (void) |
Tells whether external privileged fetch is locked. More... | |
void | flashcdw_lock_external_privileged_fetch (bool lock) |
Locks or unlocks external privileged fetch. More... | |
bool | flashcdw_is_jtag_user_protection_enabled (void) |
Tells whether the jtag user protection is enabled. More... | |
void | flashcdw_enable_jtag_user_protection (void) |
Enable the jtag user protection feature (i.e. program (set to "0") the UPROT bit) More... | |
void | flashcdw_disable_jtag_user_protection (void) |
Disable the jtag user protection feature (i.e. erase (set to "1") the UPROT bit) More... | |
bool | flashcdw_is_secure_state_enabled (void) |
Tells whether the Secure State is enabled. More... | |
bool | flashcdw_is_secure_state_debug_enabled (void) |
Tells whether the Secure State debug is enabled. More... | |
void | flashcdw_enable_secure_state_no_debug (void) |
Enable the Secure State with the Secure State debug disabled. More... | |
void | flashcdw_enable_secure_state_with_debug (void) |
Enable the Secure State with the Secure State debug enabled. More... | |
bool | flashcdw_is_page_region_locked (int page_number) |
Tells whether the region of a page is locked. More... | |
bool | flashcdw_is_region_locked (unsigned int region) |
Tells whether a region is locked. More... | |
void | flashcdw_lock_page_region (int page_number, bool lock) |
Locks or unlocks the region of a page. More... | |
void | flashcdw_lock_region (unsigned int region, bool lock) |
Locks or unlocks a region. More... | |
void | flashcdw_lock_all_regions (bool lock) |
Locks or unlocks all regions. More... | |
Access to General-Purpose Fuses | |
bool | flashcdw_read_gp_fuse_bit (unsigned int gp_fuse_bit) |
Reads a general-purpose fuse bit. More... | |
uint64_t | flashcdw_read_gp_fuse_bitfield (unsigned int pos, unsigned int width) |
Reads a general-purpose fuse bit-field. More... | |
uint8_t | flashcdw_read_gp_fuse_byte (unsigned int gp_fuse_byte) |
Reads a general-purpose fuse byte. More... | |
uint64_t | flashcdw_read_all_gp_fuses (void) |
Reads all general-purpose fuses. More... | |
bool | flashcdw_erase_gp_fuse_bit (unsigned int gp_fuse_bit, bool check) |
Erases a general-purpose fuse bit. More... | |
bool | flashcdw_erase_gp_fuse_bitfield (unsigned int pos, unsigned int width, bool check) |
Erases a general-purpose fuse bit-field. More... | |
bool | flashcdw_erase_gp_fuse_byte (unsigned int gp_fuse_byte, bool check) |
Erases a general-purpose fuse byte. More... | |
bool | flashcdw_erase_all_gp_fuses (bool check) |
Erases all general-purpose fuses. More... | |
void | flashcdw_write_gp_fuse_bit (unsigned int gp_fuse_bit, bool value) |
Writes a general-purpose fuse bit. More... | |
void | flashcdw_write_gp_fuse_bitfield (unsigned int pos, unsigned int width, uint64_t value) |
Writes a general-purpose fuse bit-field. More... | |
void | flashcdw_write_gp_fuse_byte (unsigned int gp_fuse_byte, uint8_t value) |
Writes a general-purpose fuse byte. More... | |
void | flashcdw_write_all_gp_fuses (uint64_t value) |
Writes all general-purpose fuses. More... | |
void | flashcdw_set_gp_fuse_bit (unsigned int gp_fuse_bit, bool value) |
Sets a general-purpose fuse bit with the appropriate erase and write operations. More... | |
void | flashcdw_set_gp_fuse_bitfield (unsigned int pos, unsigned int width, uint64_t value) |
Sets a general-purpose fuse bit-field with the appropriate erase and write operations. More... | |
void | flashcdw_set_gp_fuse_byte (unsigned int gp_fuse_byte, uint8_t value) |
Sets a general-purpose fuse byte with the appropriate erase and write operations. More... | |
void | flashcdw_set_all_gp_fuses (uint64_t value) |
Sets all general-purpose fuses with the appropriate erase and write operations. More... | |
Access to Flash Pages | |
void | flashcdw_clear_page_buffer (void) |
Clears the page buffer. More... | |
bool | flashcdw_is_page_erased (void) |
Tells whether the page to which the last Quick Page Read or Quick Page Read User Page command was applied was erased. More... | |
bool | flashcdw_quick_page_read (int page_number) |
Applies the Quick Page Read command to a page. More... | |
bool | flashcdw_erase_page (int page_number, bool check) |
Erases a page. More... | |
bool | flashcdw_erase_all_pages (bool check) |
Erases all pages within the flash array. More... | |
void | flashcdw_write_page (int page_number) |
Writes a page from the page buffer. More... | |
bool | flashcdw_quick_user_page_read (void) |
Issues a Quick Page Read User Page command to the FLASHCDW. More... | |
bool | flashcdw_erase_user_page (bool check) |
Erases the User page. More... | |
void | flashcdw_write_user_page (void) |
Writes the User page from the page buffer. More... | |
volatile void * | flashcdw_memset8 (volatile void *dst, uint8_t src, size_t nbytes, bool erase) |
Copies nbytes bytes to the flash destination pointed to by dst from the repeated src source byte. More... | |
volatile void * | flashcdw_memset16 (volatile void *dst, uint16_t src, size_t nbytes, bool erase) |
Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source half-word. More... | |
volatile void * | flashcdw_memset32 (volatile void *dst, uint32_t src, size_t nbytes, bool erase) |
Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source word. More... | |
volatile void * | flashcdw_memset64 (volatile void *dst, uint64_t src, size_t nbytes, bool erase) |
Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source double-word. More... | |
volatile void * | flashcdw_memcpy (volatile void *dst, const void *src, size_t nbytes, bool erase) |
Copies nbytes bytes to the flash destination pointed to by dst from the source pointed to by src. More... | |
#define | flashcdw_memset(dst, src, src_width, nbytes, erase) TPASTE2(flashcdw_memset, src_width)((dst), (src), (nbytes), (erase)) |
Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source pattern. More... | |
#define AVR32_FLASHCDW_REGIONS |
Number of flash regions defined by the FLASHCDW.
Referenced by flashcdw_get_page_count_per_region(), flashcdw_is_region_locked(), and flashcdw_lock_all_regions().
#define flash_set_bus_freq | ( | cpu_f_hz | ) | flashcdw_set_flash_waitstate_and_readmode(cpu_f_hz) |
Alias on the flashcdw_set_flash_waitstate_and_readmode() function.
cpu_f_hz | The CPU frequency |
#define flashcdw_memset | ( | dst, | |
src, | |||
src_width, | |||
nbytes, | |||
erase | |||
) | TPASTE2(flashcdw_memset, src_width)((dst), (src), (nbytes), (erase)) |
Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source pattern.
All pointer and size alignments are supported.
dst | Pointer to flash destination. |
src | Source double-word. |
src_width | src width in bits: 8, 16, 32 or 64. |
nbytes | Number of bytes to set. |
erase | Whether to erase before writing: true or false . |
false
only if the destination consists only of erased words, i.e. this function can not be used to write only one bit of a previously written word. E.g., if 0x00000001
then 0xFFFFFFFE
are written to a word, the resulting value in flash may be different from 0x00000000
.void flashcdw_activate_security_bit | ( | void | ) |
Activates the Security bit.
References flashcdw_issue_command().
void flashcdw_clear_page_buffer | ( | void | ) |
Clears the page buffer.
This command resets all bits in the page buffer to one. Write accesses to the page buffer can only change page buffer bits from one to zero.
References flashcdw_issue_command().
Referenced by flashcdw_memcpy(), and flashcdw_memset64().
void flashcdw_default_wait_until_ready | ( | void | ) |
Waits actively until the FLASHCDW is ready to run a new command.
This is the default function assigned to flashcdw_wait_until_ready.
References flashcdw_is_ready().
void flashcdw_disable_jtag_user_protection | ( | void | ) |
Disable the jtag user protection feature (i.e. erase (set to "1") the UPROT bit)
References flashcdw_set_gp_fuse_bit().
void flashcdw_enable_jtag_user_protection | ( | void | ) |
Enable the jtag user protection feature (i.e. program (set to "0") the UPROT bit)
References flashcdw_set_gp_fuse_bit().
void flashcdw_enable_lock_error_int | ( | bool | enable | ) |
Enables or disables the Lock Error interrupt.
enable | Whether to enable the Lock Error interrupt: true or false . |
References u_avr32_flashcdw_fcr_t::fcr, and u_avr32_flashcdw_fcr_t::FCR.
void flashcdw_enable_prog_error_int | ( | bool | enable | ) |
Enables or disables the Programming Error interrupt.
enable | Whether to enable the Programming Error interrupt: true or false . |
References u_avr32_flashcdw_fcr_t::fcr, and u_avr32_flashcdw_fcr_t::FCR.
void flashcdw_enable_ready_int | ( | bool | enable | ) |
Enables or disables the Flash Ready interrupt.
enable | Whether to enable the Flash Ready interrupt: true or false . |
References u_avr32_flashcdw_fcr_t::fcr, and u_avr32_flashcdw_fcr_t::FCR.
void flashcdw_enable_secure_state_no_debug | ( | void | ) |
Enable the Secure State with the Secure State debug disabled.
References flashcdw_write_gp_fuse_bitfield().
void flashcdw_enable_secure_state_with_debug | ( | void | ) |
Enable the Secure State with the Secure State debug enabled.
References flashcdw_write_gp_fuse_bitfield().
void flashcdw_erase_all | ( | void | ) |
Issues an Erase All command to the FLASHCDW.
This command erases all bits in the flash array, the general-purpose fuse bits and the Security bit. The User page is not erased.
This command also ensures that all volatile memories, such as register file and RAMs, are erased before the Security bit is erased, i.e. deactivated.
References flashcdw_issue_command().
Erases all general-purpose fuses.
check | Whether to check erase: true or false . |
true
if erase check was not requested.AVR32_FLASHCDW_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcdw_issue_command(), and flashcdw_read_all_gp_fuses().
Referenced by flashcdw_erase_gp_fuse_byte(), and flashcdw_set_all_gp_fuses().
Erases all pages within the flash array.
check | Whether to check erase: true or false . |
true
if erase check was not requested.References flashcdw_erase_page(), flashcdw_error_status, and flashcdw_get_page_count().
Erases a general-purpose fuse bit.
gp_fuse_bit | The general-purpose fuse bit: 0 to 63 . |
check | Whether to check erase: true or false . |
true
if erase check was not requested.AVR32_FLASHCDW_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcdw_issue_command(), and flashcdw_read_gp_fuse_bit().
Referenced by flashcdw_erase_gp_fuse_bitfield(), and flashcdw_set_gp_fuse_bit().
Erases a general-purpose fuse bit-field.
pos | The bit-position of the general-purpose fuse bit-field: 0 to 63 . |
width | The bit-width of the general-purpose fuse bit-field: 0 to 64 . |
check | Whether to check erase: true or false . |
true
if erase check was not requested.AVR32_FLASHCDW_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcdw_erase_gp_fuse_bit(), flashcdw_error_status, flashcdw_read_gp_fuse_bitfield(), and min.
Erases a general-purpose fuse byte.
gp_fuse_byte | The general-purpose fuse byte: 0 to 7 . |
check | Whether to check erase: true or false . |
true
if erase check was not requested.AVR32_FLASHCDW_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcdw_erase_all_gp_fuses(), flashcdw_error_status, flashcdw_read_all_gp_fuses(), flashcdw_read_gp_fuse_byte(), and flashcdw_write_gp_fuse_byte().
Referenced by flashcdw_set_gp_fuse_byte().
Erases a page.
page_number | The page number:
|
check | Whether to check erase: true or false . |
true
if erase check was not requested.References flashcdw_error_status, flashcdw_issue_command(), and flashcdw_quick_page_read().
Referenced by flashcdw_erase_all_pages(), flashcdw_memcpy(), and flashcdw_memset64().
Erases the User page.
check | Whether to check erase: true or false . |
true
if erase check was not requested.References flashcdw_issue_command(), and flashcdw_quick_user_page_read().
Referenced by flashcdw_memcpy(), and flashcdw_memset64().
unsigned int flashcdw_get_bootloader_protected_size | ( | void | ) |
Gets the bootloader protected size.
References flashcdw_read_gp_fuse_bitfield().
Referenced by flashcdw_set_bootloader_protected_size().
unsigned int flashcdw_get_command | ( | void | ) |
Gets the last issued FLASHCDW command.
|
static |
Gets the error status of the FLASHCDW.
AVR32_FLASHCDW_FSR_LOCKE_MASK
and AVR32_FLASHCDW_FSR_PROGE_MASK
.Referenced by flashcdw_issue_command().
unsigned int flashcdw_get_flash_size | ( | void | ) |
Gets the size of the whole flash array.
Referenced by flashcdw_get_page_count(), flashcdw_memcpy(), and flashcdw_memset64().
unsigned int flashcdw_get_page_count | ( | void | ) |
Gets the total number of pages in the flash array.
References flashcdw_get_flash_size().
Referenced by flashcdw_erase_all_pages(), and flashcdw_get_page_count_per_region().
unsigned int flashcdw_get_page_count_per_region | ( | void | ) |
Gets the number of pages in each flash region.
References AVR32_FLASHCDW_REGIONS, and flashcdw_get_page_count().
Referenced by flashcdw_get_page_region(), and flashcdw_get_region_first_page_number().
unsigned int flashcdw_get_page_number | ( | void | ) |
Gets the current FLASHCDW page number.
Referenced by flashcdw_get_page_region().
unsigned int flashcdw_get_page_region | ( | int | page_number | ) |
Gets the region number of a page.
page_number | The page number:
|
References flashcdw_get_page_count_per_region(), and flashcdw_get_page_number().
Referenced by flashcdw_is_page_region_locked().
unsigned int flashcdw_get_region_first_page_number | ( | unsigned int | region | ) |
Gets the number of the first page of a region.
region | The region number: 0 to (AVR32_FLASHCDW_REGIONS - 1) . |
References flashcdw_get_page_count_per_region().
Referenced by flashcdw_lock_region().
unsigned int flashcdw_get_wait_state | ( | void | ) |
Gets the number of wait states of flash read accesses.
bool flashcdw_is_external_privileged_fetch_locked | ( | void | ) |
Tells whether external privileged fetch is locked.
References flashcdw_read_gp_fuse_bit().
bool flashcdw_is_high_speed_enabled | ( | void | ) |
Tells whether the High-speed read mode is enabled.
bool flashcdw_is_jtag_user_protection_enabled | ( | void | ) |
Tells whether the jtag user protection is enabled.
References flashcdw_read_gp_fuse_bit().
bool flashcdw_is_lock_error | ( | void | ) |
Tells whether a Lock Error has occurred during the last function called that issued one or more FLASHCDW commands.
References flashcdw_error_status.
bool flashcdw_is_lock_error_int_enabled | ( | void | ) |
Tells whether the Lock Error interrupt is enabled.
bool flashcdw_is_page_erased | ( | void | ) |
Tells whether the page to which the last Quick Page Read or Quick Page Read User Page command was applied was erased.
Referenced by flashcdw_quick_page_read(), and flashcdw_quick_user_page_read().
bool flashcdw_is_page_region_locked | ( | int | page_number | ) |
Tells whether the region of a page is locked.
page_number | The page number:
|
References flashcdw_get_page_region(), and flashcdw_is_region_locked().
bool flashcdw_is_prog_error_int_enabled | ( | void | ) |
Tells whether the Programming Error interrupt is enabled.
bool flashcdw_is_programming_error | ( | void | ) |
Tells whether a Programming Error has occurred during the last function called that issued one or more FLASHCDW commands.
References flashcdw_error_status.
bool flashcdw_is_ready | ( | void | ) |
Tells whether the FLASHCDW is ready to run a new command.
Referenced by flashcdw_default_wait_until_ready().
bool flashcdw_is_ready_int_enabled | ( | void | ) |
Tells whether the Flash Ready interrupt is enabled.
bool flashcdw_is_region_locked | ( | unsigned int | region | ) |
Tells whether a region is locked.
region | The region number: 0 to (AVR32_FLASHCDW_REGIONS - 1) . |
References AVR32_FLASHCDW_REGIONS.
Referenced by flashcdw_is_page_region_locked().
bool flashcdw_is_secure_state_debug_enabled | ( | void | ) |
Tells whether the Secure State debug is enabled.
References flashcdw_read_gp_fuse_bitfield().
bool flashcdw_is_secure_state_enabled | ( | void | ) |
Tells whether the Secure State is enabled.
References flashcdw_read_gp_fuse_bitfield().
bool flashcdw_is_security_bit_active | ( | void | ) |
Tells whether the Security bit is active.
void flashcdw_issue_command | ( | unsigned int | command, |
int | page_number | ||
) |
Issues a FLASHCDW command.
command | The command: AVR32_FLASHCDW_FCMD_CMD_x . |
page_number | The page number to apply the command to:
|
References u_avr32_flashcdw_fcmd_t::fcmd, u_avr32_flashcdw_fcmd_t::FCMD, flashcdw_error_status, flashcdw_get_error_status(), and flashcdw_wait_until_ready.
Referenced by flashcdw_activate_security_bit(), flashcdw_clear_page_buffer(), flashcdw_erase_all(), flashcdw_erase_all_gp_fuses(), flashcdw_erase_gp_fuse_bit(), flashcdw_erase_page(), flashcdw_erase_user_page(), flashcdw_lock_page_region(), flashcdw_no_operation(), flashcdw_quick_page_read(), flashcdw_quick_user_page_read(), flashcdw_set_flash_waitstate_and_readmode(), flashcdw_write_gp_fuse_bit(), flashcdw_write_gp_fuse_byte(), flashcdw_write_page(), and flashcdw_write_user_page().
void flashcdw_lock_all_regions | ( | bool | lock | ) |
Locks or unlocks all regions.
lock | Whether to lock the regions: true or false . |
References AVR32_FLASHCDW_REGIONS, flashcdw_error_status, and flashcdw_lock_region().
void flashcdw_lock_external_privileged_fetch | ( | bool | lock | ) |
Locks or unlocks external privileged fetch.
lock | Whether to lock external privileged fetch: true or false . |
References flashcdw_set_gp_fuse_bit().
void flashcdw_lock_page_region | ( | int | page_number, |
bool | lock | ||
) |
Locks or unlocks the region of a page.
page_number | The page number:
|
lock | Whether to lock the region of the specified page: true or false . |
References flashcdw_issue_command().
Referenced by flashcdw_lock_region().
void flashcdw_lock_region | ( | unsigned int | region, |
bool | lock | ||
) |
Locks or unlocks a region.
region | The region number: 0 to (AVR32_FLASHCDW_REGIONS - 1) . |
lock | Whether to lock the specified region: true or false . |
References flashcdw_get_region_first_page_number(), and flashcdw_lock_page_region().
Referenced by flashcdw_lock_all_regions().
volatile void* flashcdw_memcpy | ( | volatile void * | dst, |
const void * | src, | ||
size_t | nbytes, | ||
bool | erase | ||
) |
Copies nbytes bytes to the flash destination pointed to by dst from the source pointed to by src.
The destination areas that are not within the flash array or the User page are caught by an Assert() operation.
All pointer and size alignments are supported.
dst | Pointer to flash destination. |
src | Pointer to source data. |
nbytes | Number of bytes to copy. |
erase | Whether to erase before writing: true or false . |
false
only if the destination consists only of erased words, i.e. this function can not be used to write only one bit of a previously written word. E.g., if 0x00000001
then 0xFFFFFFFE
are written to a word, the resulting value in flash may be different from 0x00000000
.References Assert, flashcdw_clear_page_buffer(), flashcdw_erase_page(), flashcdw_erase_user_page(), flashcdw_error_status, flashcdw_get_flash_size(), flashcdw_write_page(), flashcdw_write_user_page(), Union64::u64, and Union64::u8.
volatile void* flashcdw_memset16 | ( | volatile void * | dst, |
uint16_t | src, | ||
size_t | nbytes, | ||
bool | erase | ||
) |
Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source half-word.
All pointer and size alignments are supported.
dst | Pointer to flash destination. |
src | Source half-word. |
nbytes | Number of bytes to set. |
erase | Whether to erase before writing: true or false . |
false
only if the destination consists only of erased words, i.e. this function can not be used to write only one bit of a previously written word. E.g., if 0x00000001
then 0xFFFFFFFE
are written to a word, the resulting value in flash may be different from 0x00000000
.References flashcdw_memset32().
Referenced by flashcdw_memset8().
volatile void* flashcdw_memset32 | ( | volatile void * | dst, |
uint32_t | src, | ||
size_t | nbytes, | ||
bool | erase | ||
) |
Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source word.
All pointer and size alignments are supported.
dst | Pointer to flash destination. |
src | Source word. |
nbytes | Number of bytes to set. |
erase | Whether to erase before writing: true or false . |
false
only if the destination consists only of erased words, i.e. this function can not be used to write only one bit of a previously written word. E.g., if 0x00000001
then 0xFFFFFFFE
are written to a word, the resulting value in flash may be different from 0x00000000
.References flashcdw_memset64().
Referenced by flashcdw_memset16().
volatile void* flashcdw_memset64 | ( | volatile void * | dst, |
uint64_t | src, | ||
size_t | nbytes, | ||
bool | erase | ||
) |
Copies nbytes bytes to the flash destination pointed to by dst from the repeated src big-endian source double-word.
All pointer and size alignments are supported.
dst | Pointer to flash destination. |
src | Source double-word. |
nbytes | Number of bytes to set. |
erase | Whether to erase before writing: true or false . |
false
only if the destination consists only of erased words, i.e. this function can not be used to write only one bit of a previously written word. E.g., if 0x00000001
then 0xFFFFFFFE
are written to a word, the resulting value in flash may be different from 0x00000000
.References Align_down, flashcdw_clear_page_buffer(), flashcdw_erase_page(), flashcdw_erase_user_page(), flashcdw_error_status, flashcdw_get_flash_size(), flashcdw_write_page(), flashcdw_write_user_page(), Get_align, min, Test_align, StructCVPtr::u16ptr, Union64::u32, UnionVPtr::u32ptr, StructCVPtr::u32ptr, Union64::u64, UnionVPtr::u64ptr, UnionCVPtr::u64ptr, StructCVPtr::u64ptr, Union64::u8, UnionVPtr::u8ptr, UnionCVPtr::u8ptr, and StructCVPtr::u8ptr.
Referenced by flashcdw_memset32().
volatile void* flashcdw_memset8 | ( | volatile void * | dst, |
uint8_t | src, | ||
size_t | nbytes, | ||
bool | erase | ||
) |
Copies nbytes bytes to the flash destination pointed to by dst from the repeated src source byte.
All pointer and size alignments are supported.
dst | Pointer to flash destination. |
src | Source byte. |
nbytes | Number of bytes to set. |
erase | Whether to erase before writing: true or false . |
false
only if the destination consists only of erased words, i.e. this function cannot be used to write only one bit of a previously written word. E.g., if 0x00000001
then 0xFFFFFFFE
are written to a word, the resulting value in flash may be different from 0x00000000
.References flashcdw_memset16().
void flashcdw_no_operation | ( | void | ) |
Issues a No Operation command to the FLASHCDW.
References flashcdw_issue_command().
bool flashcdw_quick_page_read | ( | int | page_number | ) |
Applies the Quick Page Read command to a page.
page_number | The page number:
|
References flashcdw_is_page_erased(), and flashcdw_issue_command().
Referenced by flashcdw_erase_page().
bool flashcdw_quick_user_page_read | ( | void | ) |
Issues a Quick Page Read User Page command to the FLASHCDW.
References flashcdw_is_page_erased(), and flashcdw_issue_command().
Referenced by flashcdw_erase_user_page().
uint64_t flashcdw_read_all_gp_fuses | ( | void | ) |
Reads all general-purpose fuses.
AVR32_FLASHCDW_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. Referenced by flashcdw_erase_all_gp_fuses(), flashcdw_erase_gp_fuse_byte(), flashcdw_read_gp_fuse_bit(), flashcdw_read_gp_fuse_bitfield(), and flashcdw_read_gp_fuse_byte().
bool flashcdw_read_gp_fuse_bit | ( | unsigned int | gp_fuse_bit | ) |
Reads a general-purpose fuse bit.
gp_fuse_bit | The general-purpose fuse bit: 0 to 63 . |
AVR32_FLASHCDW_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcdw_read_all_gp_fuses().
Referenced by flashcdw_erase_gp_fuse_bit(), flashcdw_is_external_privileged_fetch_locked(), and flashcdw_is_jtag_user_protection_enabled().
uint64_t flashcdw_read_gp_fuse_bitfield | ( | unsigned int | pos, |
unsigned int | width | ||
) |
Reads a general-purpose fuse bit-field.
pos | The bit-position of the general-purpose fuse bit-field: 0 to 63 . |
width | The bit-width of the general-purpose fuse bit-field: 0 to 64 . |
AVR32_FLASHCDW_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcdw_read_all_gp_fuses(), and min.
Referenced by flashcdw_erase_gp_fuse_bitfield(), flashcdw_get_bootloader_protected_size(), flashcdw_is_secure_state_debug_enabled(), and flashcdw_is_secure_state_enabled().
uint8_t flashcdw_read_gp_fuse_byte | ( | unsigned int | gp_fuse_byte | ) |
Reads a general-purpose fuse byte.
gp_fuse_byte | The general-purpose fuse byte: 0 to 7 . |
AVR32_FLASHCDW_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcdw_read_all_gp_fuses().
Referenced by flashcdw_erase_gp_fuse_byte().
void flashcdw_set_all_gp_fuses | ( | uint64_t | value | ) |
Sets all general-purpose fuses with the appropriate erase and write operations.
value | The value of all general-purpose fuses as a word. |
AVR32_FLASHCDW_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcdw_erase_all_gp_fuses(), flashcdw_error_status, and flashcdw_write_all_gp_fuses().
unsigned int flashcdw_set_bootloader_protected_size | ( | unsigned int | bootprot_size | ) |
Sets the bootloader protected size.
bootprot_size | The wanted bootloader protected size in bytes. If this size is not supported, the actual size will be the nearest greater available size or the maximal possible size if the requested size is too large. |
References clz, flashcdw_get_bootloader_protected_size(), flashcdw_set_gp_fuse_bitfield(), max, and min.
void flashcdw_set_flash_waitstate_and_readmode | ( | unsigned long | cpu_f_hz | ) |
Depending on the CPU frequency, set the wait states of flash read accesses and enable or disable the High speed read mode.
cpu_f_hz | The CPU frequency |
References flashcdw_issue_command(), and flashcdw_set_wait_state().
Referenced by pcl_configure_synchronous_clocks(), and pcl_switch_to_osc().
void flashcdw_set_gp_fuse_bit | ( | unsigned int | gp_fuse_bit, |
bool | value | ||
) |
Sets a general-purpose fuse bit with the appropriate erase and write operations.
gp_fuse_bit | The general-purpose fuse bit: 0 to 63 . |
value | The value of the specified general-purpose fuse bit. |
AVR32_FLASHCDW_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcdw_erase_gp_fuse_bit(), and flashcdw_write_gp_fuse_bit().
Referenced by flashcdw_disable_jtag_user_protection(), flashcdw_enable_jtag_user_protection(), flashcdw_lock_external_privileged_fetch(), and flashcdw_set_gp_fuse_bitfield().
void flashcdw_set_gp_fuse_bitfield | ( | unsigned int | pos, |
unsigned int | width, | ||
uint64_t | value | ||
) |
Sets a general-purpose fuse bit-field with the appropriate erase and write operations.
pos | The bit-position of the general-purpose fuse bit-field: 0 to 63 . |
width | The bit-width of the general-purpose fuse bit-field: 0 to 64 . |
value | The value of the specified general-purpose fuse bit-field. |
AVR32_FLASHCDW_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcdw_error_status, flashcdw_set_gp_fuse_bit(), and min.
Referenced by flashcdw_set_bootloader_protected_size().
void flashcdw_set_gp_fuse_byte | ( | unsigned int | gp_fuse_byte, |
uint8_t | value | ||
) |
Sets a general-purpose fuse byte with the appropriate erase and write operations.
gp_fuse_byte | The general-purpose fuse byte: 0 to 7 . |
value | The value of the specified general-purpose fuse byte. |
AVR32_FLASHCDW_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcdw_erase_gp_fuse_byte(), flashcdw_error_status, and flashcdw_write_gp_fuse_byte().
void flashcdw_set_wait_state | ( | unsigned int | wait_state | ) |
Sets the number of wait states of flash read accesses.
wait_state | The number of wait states of flash read accesses: 0 to 1 . |
References u_avr32_flashcdw_fcr_t::fcr, and u_avr32_flashcdw_fcr_t::FCR.
Referenced by flashcdw_set_flash_waitstate_and_readmode().
void flashcdw_write_all_gp_fuses | ( | uint64_t | value | ) |
Writes all general-purpose fuses.
value | The value of all general-purpose fuses as a word. |
AVR32_FLASHCDW_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcdw_error_status, and flashcdw_write_gp_fuse_byte().
Referenced by flashcdw_set_all_gp_fuses().
void flashcdw_write_gp_fuse_bit | ( | unsigned int | gp_fuse_bit, |
bool | value | ||
) |
Writes a general-purpose fuse bit.
gp_fuse_bit | The general-purpose fuse bit: 0 to 63 . |
value | The value of the specified general-purpose fuse bit. |
AVR32_FLASHCDW_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcdw_issue_command().
Referenced by flashcdw_set_gp_fuse_bit(), and flashcdw_write_gp_fuse_bitfield().
void flashcdw_write_gp_fuse_bitfield | ( | unsigned int | pos, |
unsigned int | width, | ||
uint64_t | value | ||
) |
Writes a general-purpose fuse bit-field.
pos | The bit-position of the general-purpose fuse bit-field: 0 to 63 . |
width | The bit-width of the general-purpose fuse bit-field: 0 to 64 . |
value | The value of the specified general-purpose fuse bit-field. |
AVR32_FLASHCDW_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcdw_error_status, flashcdw_write_gp_fuse_bit(), and min.
Referenced by flashcdw_enable_secure_state_no_debug(), and flashcdw_enable_secure_state_with_debug().
void flashcdw_write_gp_fuse_byte | ( | unsigned int | gp_fuse_byte, |
uint8_t | value | ||
) |
Writes a general-purpose fuse byte.
gp_fuse_byte | The general-purpose fuse byte: 0 to 7 . |
value | The value of the specified general-purpose fuse byte. |
AVR32_FLASHCDW_GPF_NUM
. The other bits among the 64 are fixed at 1 by hardware. References flashcdw_issue_command().
Referenced by flashcdw_erase_gp_fuse_byte(), flashcdw_set_gp_fuse_byte(), and flashcdw_write_all_gp_fuses().
void flashcdw_write_page | ( | int | page_number | ) |
Writes a page from the page buffer.
page_number | The page number:
|
References flashcdw_issue_command().
Referenced by flashcdw_memcpy(), and flashcdw_memset64().
void flashcdw_write_user_page | ( | void | ) |
Writes the User page from the page buffer.
References flashcdw_issue_command().
Referenced by flashcdw_memcpy(), and flashcdw_memset64().
|
static |
Sticky error status of the FLASHCDW.
This variable is updated by functions that issue FLASHCDW commands. It contains the cumulated FLASHCDW error status of all the FLASHCDW commands issued by a function.
Referenced by flashcdw_erase_all_pages(), flashcdw_erase_gp_fuse_bitfield(), flashcdw_erase_gp_fuse_byte(), flashcdw_erase_page(), flashcdw_is_lock_error(), flashcdw_is_programming_error(), flashcdw_issue_command(), flashcdw_lock_all_regions(), flashcdw_memcpy(), flashcdw_memset64(), flashcdw_set_all_gp_fuses(), flashcdw_set_gp_fuse_bitfield(), flashcdw_set_gp_fuse_byte(), flashcdw_write_all_gp_fuses(), and flashcdw_write_gp_fuse_bitfield().
void(*volatile flashcdw_wait_until_ready)(void) |
Pointer to the function used by the driver when it needs to wait until the FLASHCDW is ready to run a new command.
The default function is flashcdw_default_wait_until_ready. The user may change this pointer to use another implementation.
Referenced by flashcdw_issue_command().