This is the documentation for the TWIS Module driver.
This example demonstrates how to use the TWI interface with TWIS modules.
This software is written for GNU GCC for AVR32 and for IAR Embedded Workbench for Atmel AVR32. Other compilers may or may not work.
All AVR32 devices with a TWIS can be used.
This example has been tested with the following configuration:
For further information, visit Atmel AVR32.