#include "dsp.h"
Macros | |
#define | DEFAULT_FILTER_FUNCTION dsp16_filt_lpfirdesign_windowed_sinc |
#define | DEFAULT_WINDOW_FUNCTION dsp16_win_hann |
#define | DSP16_RESAMPLING_FILTER(x_num, data) sum += ph[(x_num+data)] * pvect2[-(x_num+data)]; |
#define | DSP16_RESAMPLING_FUNCTION_NAME(x_num, data) TPASTE2(dsp16_resampling_kernel_x, x_num), |
#define | DSP16_RESAMPLING_KERNEL_X_FCT(x_num, data) |
#define | DSP16_RESAMPLING_NO_LOOP_FUNCTION_NAME(x_num, data) TPASTE2(dsp16_resampling_no_loop_kernel_x, x_num), |
#define | DSP16_RESAMPLING_NO_LOOP_KERNEL_X_FCT(x_num, data) |
#define | LOOP_UNROLL 6 |
#define | LOOP_UNROLL_PLUS_ONE 7 |
#define | NB_PTS_TO_INTERPOLATE 3 |
Functions | |
void | dsp16_resampling_compute (dsp_resampling_t *dsp_resampling, dsp16_t *output, dsp16_t *input, int channel) |
The re-sampling computation function. More... | |
void | dsp16_resampling_free (dsp_resampling_t *dsp_resampling, free_fct_t free_fct) |
Function used to free the previously allocated structure issued by the dsp16_resampling_setup function. More... | |
int | dsp16_resampling_get_output_current_buffer_size (dsp_resampling_t *dsp_resampling) |
Returns the current length in sample of the output signal. More... | |
int | dsp16_resampling_get_output_max_buffer_size (dsp_resampling_t *dsp_resampling) |
Returns the maximal length in sample of the output signal. More... | |
bool | dsp16_resampling_link (dsp_resampling_t *dsp_resampling_output, dsp_resampling_t *dsp_resampling_input) |
Link a stream previously re-sampled using the dsp_resampling_input resampling structure with the new re-sampling structure dsp_resampling_output. This is used to keep the continuity with two pieces of a stream re-sampled using two different re-sampling parameters. More... | |
static int | dsp16_resampling_no_loop_kernel_x0 (dsp16_t *vect1, dsp16_t *vect2, int vect2_size, dsp16_t *h, int n_tap, int interpolation_ratio, int decimation_ratio, int *pcounter, int *pn) |
static void | dsp16_resampling_polynomial_interpolation (dsp16_t y[4], dsp16_t output_y[NB_PTS_TO_INTERPOLATE]) |
dsp_resampling_t * | dsp16_resampling_setup (int input_sample_rate, int output_sample_rate, int buffer_size, int filter_order, int nb_channels, malloc_fct_t malloc_fct, dsp16_resampling_options_t *options) |
This function is the 16-bit signal resampling setup function. It has to be called only once at the initialization of the resampling process. More... | |
static int | dsp_op_gcd (int m, int n) |
#define DEFAULT_FILTER_FUNCTION dsp16_filt_lpfirdesign_windowed_sinc |
Referenced by dsp16_resampling_setup().
#define DEFAULT_WINDOW_FUNCTION dsp16_win_hann |
Referenced by dsp16_resampling_setup().
#define DSP16_RESAMPLING_FILTER | ( | x_num, | |
data | |||
) | sum += ph[(x_num+data)] * pvect2[-(x_num+data)]; |
#define DSP16_RESAMPLING_FUNCTION_NAME | ( | x_num, | |
data | |||
) | TPASTE2(dsp16_resampling_kernel_x, x_num), |
Referenced by dsp16_resampling_compute().
#define DSP16_RESAMPLING_KERNEL_X_FCT | ( | x_num, | |
data | |||
) |
#define DSP16_RESAMPLING_NO_LOOP_FUNCTION_NAME | ( | x_num, | |
data | |||
) | TPASTE2(dsp16_resampling_no_loop_kernel_x, x_num), |
Referenced by dsp16_resampling_compute().
#define DSP16_RESAMPLING_NO_LOOP_KERNEL_X_FCT | ( | x_num, | |
data | |||
) |
#define LOOP_UNROLL 6 |
Referenced by dsp16_resampling_compute().
#define LOOP_UNROLL_PLUS_ONE 7 |
Referenced by dsp16_resampling_compute().
#define NB_PTS_TO_INTERPOLATE 3 |
|
static |
References vect1.
|
static |
References NB_PTS_TO_INTERPOLATE.
Referenced by dsp16_resampling_compute().
|
static |
Referenced by dsp16_resampling_setup().