Microchip® Advanced Software Framework

trans_dsp16_twiddle_factors.h File Reference
#include "dsp.h"

Macros

Twiddle factors table
#define DSP16_N_TWIDDLE_FACTORS   1024
 This constant defines the size of the twiddle factors table we want to store in memory.
i.e.: if we want to compute a 1024-point (or less) complex FFT, we will define this constant as follow: More...
 
#define TWIDDLE_FACTORS_PREFIX_TAB
 This constant permits you to add attributes to the twiddle factors table.
It is useful if you want to store the table into another memory for example.
i.e.: More...
 

Variables

TWIDDLE_FACTORS_PREFIX_TAB dsp16_t dsp16_twiddle_factors []
 This table has been generated using the following algorithm: More...
 
TWIDDLE_FACTORS_PREFIX_TAB dsp16_t dsp16_twiddle_factors2 []
 This table has been generated using the following algorithm: More...
 

TWIDDLE_FACTORS_PREFIX_TAB dsp16_t dsp16_twiddle_factors[]

This table has been generated using the following algorithm:

w = exp(-2*PI*%i*k);
end;

It is a one dimensional array containing the real parts (even parts) and imaginary parts (odd parts) of the w value.

Referenced by dsp16_trans_complexfft(), dsp16_trans_complexifft_ex(), and dsp16_trans_realcomplexfft().

TWIDDLE_FACTORS_PREFIX_TAB dsp16_t dsp16_twiddle_factors2[]

This table has been generated using the following algorithm:

w2 = exp(-2*PI*%i*k*2);
w3 = exp(-2*PI*%i*k*3);
end;

It is a one dimensional array containing the real parts (4*i parts) and imaginary parts (4*i+1 parts) of the w2 value and the real parts (4*i+2 parts) and imaginary parts (4*i+3 parts) of the w3 value.

Referenced by dsp16_trans_complexfft(), dsp16_trans_complexifft_ex(), and dsp16_trans_realcomplexfft().