This example demonstrates how to use the 16-bit complex FFT function.
To visualize the result, you may use a terminal configured as described in the section Configuration Information.
Through this page, you can access the DSP Library documentation.
This software is written for GNU GCC for 32-bit AVRs and for IAR Embedded Workbench for Atmel 32-bit AVRs. Other compilers may or may not work.
All 32-bit AVR devices with a USART module can be used. This example has been tested with the following setup:
This example has been tested with the following configuration: