This example demonstrates a way to use the 32-bit NLMS Filter function.
This is an adaptive filter, therefore the output of the function will be a data stream. To change the signal frequency and to see the adaptation of the filter, press the push button PB0 (on EVK1100) or PB2 (on EVK1101).
To visualize the result, you may use a terminal configured as described in the section Configuration Information.
Through this page, you can access the DSP Library documentation.
This software is written for GNU GCC for 32-bit AVRs and for IAR Embedded Workbench for Atmel 32-bit AVRs. Other compilers may or may not work.
All 32-bit AVR devices with a USART module can be used. This example has been tested with the following setup:
This example has been tested with the following configuration: