All the IMA/DVI ADPCM functions implemented in the DSP advanced library.
Functions | |
void | dsp_adpcm_ima_decode (S16 *out, void *in, int size, S16 *step_index, S16 *predicted_value) |
IMA/DVI ADPCM decoder. More... | |
S16 | dsp_adpcm_ima_decode_nibble (S8 nibble, S16 *step_index, S16 *predicted_value) |
IMA/DVI ADPCM sample decoder. More... | |
void | dsp_adpcm_ima_encode (void *out, S16 *in, int size, S16 *step_index, S16 *predicted_value) |
IMA/DVI ADPCM encoder. More... | |
S8 | dsp_adpcm_ima_encode_nibble (S16 nibble, S16 *step_index, S16 *predicted_value) |
IMA/DVI ADPCM sample encoder. More... | |
void dsp_adpcm_ima_decode | ( | S16 * | out, |
void * | in, | ||
int | size, | ||
S16 * | step_index, | ||
S16 * | predicted_value | ||
) |
IMA/DVI ADPCM decoder.
out | A 16-bit data vector that will contain the decoded data. |
in | A 4-bit data vector that contains the IMA/DVI ADPCM encoded data to decode. |
size | The number of data to decode. |
step_index | A pointer on a 16 bits data which contain the current step index of the ADPCM algorithm. |
predicted_value | A pointer on a 16 bits data which contain the current predicted value of the ADPCM algorithm. |
References ADPCM_IMA_DECODE_NIBBLE.
Referenced by main().
IMA/DVI ADPCM sample decoder.
nibble | The sample to decode. It must be a 4-bit data. |
step_index | A pointer on a 16 bits data which contain the previous step index of the ADPCM algorithm. |
predicted_value | A pointer on a 16 bits data which contain the previous predicted value of the ADPCM algorithm. |
References ADPCM_IMA_DECODE_NIBBLE.
void dsp_adpcm_ima_encode | ( | void * | out, |
S16 * | in, | ||
int | size, | ||
S16 * | step_index, | ||
S16 * | predicted_value | ||
) |
IMA/DVI ADPCM encoder.
out | A 4-bit data vector that will contain the encoded data. |
in | A 16-bit data vector that contains the data to encode. |
size | The number of data to encode. |
step_index | A pointer on a 16 bits data which contain the current step index of the ADPCM algorithm. |
predicted_value | A pointer on a 16 bits data which contain the current predicted value of the ADPCM algorithm. |
References ADPCM_IMA_ENCODE_NIBBLE.
Referenced by main().
IMA/DVI ADPCM sample encoder.
nibble | The sample to encode. |
step_index | A pointer on a 16 bits data which contain the current step index of the ADPCM algorithm. |
predicted_value | A pointer on a 16 bits data which contain the current predicted value of the ADPCM algorithm. |
References ADPCM_IMA_ENCODE_NIBBLE.