This example demonstrates how to use the 32-bit FIR Filter function.
To visualize the result, you may set a breakpoint after the sprintf and check the string variable output through Watch Window in AVR Studio 5. Through this page, you can access the DSP Library documentation.
This software was written for the GNU GCC for AVR32.
This example has been tested with the following configuration:
For further information, visit Atmel AVR32.