#include <string.h>
#include "compiler.h"
#include "preprocessor.h"
#include "board.h"
#include "print_funcs.h"
#include "ctrl_access.h"
#include "power_clocks_lib.h"
#include "gpio.h"
#include "usart.h"
#include "spi.h"
#include "conf_at45dbx.h"
#include "fat.h"
#include "file.h"
#include "navigation.h"
Macros | |
#define | AT45DBX_ENABLE_NPCS_PIN(NPCS, unused) {AT45DBX_SPI_NPCS##NPCS##_PIN, AT45DBX_SPI_NPCS##NPCS##_FUNCTION}, |
#define | EXAMPLE_TARGET_PBACLK_FREQ_HZ FOSC0 |
Shell USART Configuration | |
#define | SHL_USART (&AVR32_USART0) |
#define | SHL_USART_RX_PIN AVR32_USART0_RXD_0_0_PIN |
#define | SHL_USART_RX_FUNCTION AVR32_USART0_RXD_0_0_FUNCTION |
#define | SHL_USART_TX_PIN AVR32_USART0_TXD_0_0_PIN |
#define | SHL_USART_TX_FUNCTION AVR32_USART0_TXD_0_0_FUNCTION |
#define | SHL_USART_BAUDRATE 57600 |
Shell Commands | |
#define | CMD_NONE 0x00 |
#define | CMD_MOUNT 0x01 |
#define | CMD_LS 0x02 |
#define | CMD_CD 0x03 |
#define | CMD_CAT 0x04 |
#define | CMD_HELP 0x05 |
#define | CMD_MKDIR 0x06 |
#define | CMD_TOUCH 0x07 |
#define | CMD_RM 0x08 |
#define | CMD_APPEND 0x09 |
#define | CMD_NB_DRIVE 0x0A |
#define | CMD_SET_ID 0x0B |
#define | CMD_GOTO_ID 0x0C |
#define | CMD_CP 0x0D |
#define | CMD_DF 0x0E |
#define | CMD_MV 0x0F |
#define | CMD_FORMAT 0x10 |
#define | CMD_FAT 0x11 |
#define | CMD_FORMAT32 0x12 |
Special Char Values | |
#define | CR '\r' |
#define | LF '\n' |
#define | CRLF "\r\n" |
#define | CTRL_C 0x03 |
#define | CTRL_Q 0x11 |
#define | BKSPACE_CHAR '\b' |
#define | ABORT_CHAR CTRL_C |
#define | QUIT_APPEND CTRL_Q |
#define | HISTORY_CHAR '!' |
String Values for Commands | |
#define | STR_CD "cd" |
#define | STR_MOUNT "mount" |
#define | STR_CP "cp" |
#define | STR_LS "ls" |
#define | STR_RM "rm" |
#define | STR_DF "df" |
#define | STR_MKDIR "mkdir" |
#define | STR_TOUCH "touch" |
#define | STR_APPEND "append" |
#define | STR_CAT "cat" |
#define | STR_DISK "disk" |
#define | STR_MARK "mark" |
#define | STR_GOTO "goto" |
#define | STR_MV "mv" |
#define | STR_A "a:" |
#define | STR_B "b:" |
#define | STR_C "c:" |
#define | STR_D "d:" |
#define | STR_HELP "help" |
#define | STR_FORMAT "format" |
#define | STR_FORMAT32 "format32" |
#define | STR_FAT "fat" |
String Messages | |
#define | MSG_PROMPT "$>" |
#define | MSG_WELCOME |
#define | MSG_ER_CMD_NOT_FOUND "Command not found\r\n" |
#define | MSG_ER_MOUNT "Unable to mount drive\r\n" |
#define | MSG_ER_DRIVE "Drive does not exist\r\n" |
#define | MSG_ER_RM "Can not erase; if the name is a directory, check it is empty\r\n" |
#define | MSG_ER_UNKNOWN_FILE "Unknown file\r\n" |
#define | MSG_ER_MV "Error during move\r\n" |
#define | MSG_ER_FORMAT "Format fails\r\n" |
#define | MSG_APPEND_WELCOME "\r\nSimple text editor, enter char to append, ^q to exit and save\r\n" |
#define | MSG_HELP |
Functions | |
static void | at45dbx_resources_init (void) |
Initializes the dataflash memory AT45DBX resources: GPIO, SPI and AT45DBX. More... | |
static void | fat_example_append_file (void) |
Minimalist file editor to append char to a file. More... | |
static void | fat_example_build_cmd (void) |
Gets the full command line on RS232 input to be interpreted. The cmd_str variable is built with the user inputs. More... | |
static void | fat_example_parse_cmd (void) |
Decodes full command line into command type and arguments. More... | |
static void | init_shl_rs232 (long pba_hz) |
Sets up USART for shell. More... | |
int | main (void) |
Main function. Execution starts here. More... | |
Variables | |
static bool | cmd |
flag for a command presence More... | |
static char | cmd_str [10+2 *MAX_FILE_PATH_LENGTH] |
string for command More... | |
static uint8_t | cmd_type |
command number More... | |
static bool | first_ls |
flag for first ls : mount if set More... | |
static uint8_t | i_str = 0 |
string length More... | |
static char | par_str1 [MAX_FILE_PATH_LENGTH] |
string for first arg More... | |
static char | par_str2 [MAX_FILE_PATH_LENGTH] |
string for second arg More... | |
static char | str_buff [MAX_FILE_PATH_LENGTH] |
buffer for command line More... | |
#define ABORT_CHAR CTRL_C |
Referenced by fat_example_build_cmd().
#define AT45DBX_ENABLE_NPCS_PIN | ( | NPCS, | |
unused | |||
) | {AT45DBX_SPI_NPCS##NPCS##_PIN, AT45DBX_SPI_NPCS##NPCS##_FUNCTION}, |
Referenced by at45dbx_resources_init().
#define BKSPACE_CHAR '\b' |
Referenced by fat_example_build_cmd().
#define CMD_APPEND 0x09 |
Referenced by fat_example_parse_cmd(), and main().
#define CMD_CAT 0x04 |
Referenced by fat_example_parse_cmd(), and main().
#define CMD_CD 0x03 |
Referenced by fat_example_parse_cmd(), and main().
#define CMD_CP 0x0D |
Referenced by fat_example_parse_cmd(), and main().
#define CMD_DF 0x0E |
Referenced by fat_example_parse_cmd(), and main().
#define CMD_FAT 0x11 |
Referenced by fat_example_parse_cmd(), and main().
#define CMD_FORMAT 0x10 |
Referenced by fat_example_parse_cmd(), and main().
#define CMD_FORMAT32 0x12 |
Referenced by fat_example_parse_cmd(), and main().
#define CMD_GOTO_ID 0x0C |
Referenced by fat_example_parse_cmd(), and main().
#define CMD_HELP 0x05 |
Referenced by fat_example_parse_cmd(), and main().
#define CMD_LS 0x02 |
Referenced by fat_example_parse_cmd(), and main().
#define CMD_MKDIR 0x06 |
Referenced by fat_example_parse_cmd(), and main().
#define CMD_MOUNT 0x01 |
Referenced by fat_example_parse_cmd(), and main().
#define CMD_MV 0x0F |
Referenced by fat_example_parse_cmd(), and main().
#define CMD_NB_DRIVE 0x0A |
Referenced by fat_example_parse_cmd(), and main().
#define CMD_NONE 0x00 |
Referenced by main().
#define CMD_RM 0x08 |
Referenced by fat_example_parse_cmd(), and main().
#define CMD_SET_ID 0x0B |
Referenced by fat_example_parse_cmd(), and main().
#define CMD_TOUCH 0x07 |
Referenced by fat_example_parse_cmd(), and main().
#define CR '\r' |
Referenced by fat_example_build_cmd().
#define CRLF "\r\n" |
Referenced by fat_example_build_cmd(), and main().
#define CTRL_C 0x03 |
#define CTRL_Q 0x11 |
#define EXAMPLE_TARGET_PBACLK_FREQ_HZ FOSC0 |
Referenced by at45dbx_resources_init(), and main().
#define HISTORY_CHAR '!' |
#define LF '\n' |
#define MSG_APPEND_WELCOME "\r\nSimple text editor, enter char to append, ^q to exit and save\r\n" |
Referenced by fat_example_append_file().
#define MSG_ER_CMD_NOT_FOUND "Command not found\r\n" |
Referenced by fat_example_parse_cmd(), and main().
#define MSG_ER_DRIVE "Drive does not exist\r\n" |
Referenced by main().
#define MSG_ER_FORMAT "Format fails\r\n" |
Referenced by main().
#define MSG_ER_MOUNT "Unable to mount drive\r\n" |
Referenced by main().
#define MSG_ER_MV "Error during move\r\n" |
Referenced by main().
#define MSG_ER_RM "Can not erase; if the name is a directory, check it is empty\r\n" |
Referenced by main().
#define MSG_ER_UNKNOWN_FILE "Unknown file\r\n" |
Referenced by main().
#define MSG_HELP |
Referenced by main().
#define MSG_PROMPT "$>" |
Referenced by fat_example_build_cmd(), fat_example_parse_cmd(), and main().
#define MSG_WELCOME |
Referenced by main().
#define QUIT_APPEND CTRL_Q |
Referenced by fat_example_append_file().
#define SHL_USART (&AVR32_USART0) |
Referenced by fat_example_append_file(), fat_example_build_cmd(), fat_example_parse_cmd(), init_shl_rs232(), and main().
#define SHL_USART_BAUDRATE 57600 |
Referenced by init_shl_rs232().
#define SHL_USART_RX_FUNCTION AVR32_USART0_RXD_0_0_FUNCTION |
Referenced by init_shl_rs232().
#define SHL_USART_RX_PIN AVR32_USART0_RXD_0_0_PIN |
Referenced by init_shl_rs232().
#define SHL_USART_TX_FUNCTION AVR32_USART0_TXD_0_0_FUNCTION |
Referenced by init_shl_rs232().
#define SHL_USART_TX_PIN AVR32_USART0_TXD_0_0_PIN |
Referenced by init_shl_rs232().
#define STR_A "a:" |
Referenced by fat_example_parse_cmd().
#define STR_APPEND "append" |
Referenced by fat_example_parse_cmd().
#define STR_B "b:" |
Referenced by fat_example_parse_cmd().
#define STR_C "c:" |
Referenced by fat_example_parse_cmd().
#define STR_CAT "cat" |
Referenced by fat_example_parse_cmd().
#define STR_CD "cd" |
Referenced by fat_example_parse_cmd().
#define STR_CP "cp" |
Referenced by fat_example_parse_cmd().
#define STR_D "d:" |
Referenced by fat_example_parse_cmd().
#define STR_DF "df" |
Referenced by fat_example_parse_cmd().
#define STR_DISK "disk" |
Referenced by fat_example_parse_cmd().
#define STR_FAT "fat" |
Referenced by fat_example_parse_cmd().
#define STR_FORMAT "format" |
Referenced by fat_example_parse_cmd().
#define STR_FORMAT32 "format32" |
Referenced by fat_example_parse_cmd().
#define STR_GOTO "goto" |
Referenced by fat_example_parse_cmd().
#define STR_HELP "help" |
Referenced by fat_example_parse_cmd().
#define STR_LS "ls" |
Referenced by fat_example_parse_cmd().
#define STR_MARK "mark" |
Referenced by fat_example_parse_cmd().
#define STR_MKDIR "mkdir" |
Referenced by fat_example_parse_cmd().
#define STR_MOUNT "mount" |
Referenced by fat_example_parse_cmd().
#define STR_MV "mv" |
Referenced by fat_example_parse_cmd().
#define STR_RM "rm" |
Referenced by fat_example_parse_cmd().
#define STR_TOUCH "touch" |
Referenced by fat_example_parse_cmd().
|
static |
Initializes the dataflash memory AT45DBX resources: GPIO, SPI and AT45DBX.
References AT45DBX_ENABLE_NPCS_PIN, at45dbx_init(), AT45DBX_MEM_CNT, AT45DBX_SPI, AT45DBX_SPI_BITS, AT45DBX_SPI_FIRST_NPCS, AT45DBX_SPI_MASTER_SPEED, AT45DBX_SPI_MISO_FUNCTION, AT45DBX_SPI_MISO_PIN, AT45DBX_SPI_MOSI_FUNCTION, AT45DBX_SPI_MOSI_PIN, AT45DBX_SPI_SCK_FUNCTION, AT45DBX_SPI_SCK_PIN, EXAMPLE_TARGET_PBACLK_FREQ_HZ, gpio_enable_module(), MREPEAT, spi_options_t::reg, spi_enable(), spi_initMaster(), and spi_selectionMode().
Referenced by main().
|
static |
Minimalist file editor to append char to a file.
References file_putc(), MSG_APPEND_WELCOME, print(), print_char(), QUIT_APPEND, SHL_USART, usart_read_char(), usart_reset_status(), and USART_SUCCESS.
Referenced by main().
|
static |
Gets the full command line on RS232 input to be interpreted. The cmd_str variable is built with the user inputs.
References ABORT_CHAR, BKSPACE_CHAR, cmd_str, CR, CRLF, fat_example_parse_cmd(), i_str, MSG_PROMPT, print(), print_char(), SHL_USART, usart_read_char(), usart_reset_status(), and USART_SUCCESS.
Referenced by main().
|
static |
Decodes full command line into command type and arguments.
This function allows to set the cmd_type variable to the command type decoded with its respective arguments par_str1 and par_str2.
References cmd, CMD_APPEND, CMD_CAT, CMD_CD, CMD_CP, CMD_DF, CMD_FAT, CMD_FORMAT, CMD_FORMAT32, CMD_GOTO_ID, CMD_HELP, CMD_LS, CMD_MKDIR, CMD_MOUNT, CMD_MV, CMD_NB_DRIVE, CMD_RM, CMD_SET_ID, cmd_str, CMD_TOUCH, cmd_type, i_str, MSG_ER_CMD_NOT_FOUND, MSG_PROMPT, par_str1, par_str2, print(), SHL_USART, STR_A, STR_APPEND, STR_B, STR_C, STR_CAT, STR_CD, STR_CP, STR_D, STR_DF, STR_DISK, STR_FAT, STR_FORMAT, STR_FORMAT32, STR_GOTO, STR_HELP, STR_LS, STR_MARK, STR_MKDIR, STR_MOUNT, STR_MV, STR_RM, and STR_TOUCH.
Referenced by fat_example_build_cmd().
|
static |
Sets up USART for shell.
pba_hz | The current module frequency. |
References usart_options_t::baudrate, gpio_enable_module(), SHL_USART, SHL_USART_BAUDRATE, SHL_USART_RX_FUNCTION, SHL_USART_RX_PIN, SHL_USART_TX_FUNCTION, SHL_USART_TX_PIN, USART_1_STOPBIT, usart_init_rs232(), USART_NO_PARITY, and USART_NORMAL_CHMODE.
Referenced by main().
int main | ( | void | ) |
Main function. Execution starts here.
References at45dbx_resources_init(), cmd, CMD_APPEND, CMD_CAT, CMD_CD, CMD_CP, CMD_DF, CMD_FAT, CMD_FORMAT, CMD_FORMAT32, CMD_GOTO_ID, CMD_HELP, CMD_LS, CMD_MKDIR, CMD_MOUNT, CMD_MV, CMD_NB_DRIVE, CMD_NONE, CMD_RM, CMD_SET_ID, CMD_TOUCH, cmd_type, COPY_BUSY, CRLF, CTRL_GOOD, EXAMPLE_TARGET_PBACLK_FREQ_HZ, fat_example_append_file(), fat_example_build_cmd(), file_close(), file_eof(), file_getc(), file_open(), first_ls, FOPEN_MODE_APPEND, FOPEN_MODE_R, FOSC0, FS_DIR, FS_FILE, FS_FIND_NEXT, FS_FORMAT_DEFAULT, FS_FORMAT_FAT32, FS_NAME_GET, FS_SHIFT_B_TO_SECTOR, FS_TYPE_FAT_12, FS_TYPE_FAT_16, FS_TYPE_FAT_32, init_shl_rs232(), LUN_ID_AT45DBX_MEM, MAX_FILE_PATH_LENGTH, mem_name(), mem_read_capacity(), mem_test_unit_ready(), MSG_ER_CMD_NOT_FOUND, MSG_ER_DRIVE, MSG_ER_FORMAT, MSG_ER_MOUNT, MSG_ER_MV, MSG_ER_RM, MSG_ER_UNKNOWN_FILE, MSG_HELP, MSG_PROMPT, MSG_WELCOME, nav_dir_make(), nav_dir_name(), nav_drive_format(), nav_drive_get(), nav_drive_nb(), nav_drive_set(), nav_file_copy(), nav_file_create(), nav_file_del(), nav_file_isdir(), nav_file_lgt(), nav_file_lgtsector(), nav_file_name(), nav_file_paste_start(), nav_file_paste_state(), nav_file_rename(), nav_filelist_first(), nav_filelist_nb(), nav_filelist_reset(), nav_filelist_set(), nav_getindex(), nav_gotoindex(), nav_partition_freespace(), nav_partition_mount(), nav_partition_space(), nav_partition_type(), nav_reset(), nav_setcwd(), OSC0_STARTUP, par_str1, par_str2, pcl_configure_clocks(), PCL_OSC0, pcl_switch_to_osc(), print(), print_char(), print_ulong(), SHL_USART, and str_buff.
|
static |
flag for a command presence
Referenced by fat_example_parse_cmd(), and main().
|
static |
string for command
Referenced by fat_example_build_cmd(), and fat_example_parse_cmd().
|
static |
command number
Referenced by fat_example_parse_cmd(), and main().
|
static |
string length
Referenced by fat_example_build_cmd(), and fat_example_parse_cmd().
|
static |
string for first arg
Referenced by fat_example_parse_cmd(), and main().
|
static |
string for second arg
Referenced by fat_example_parse_cmd(), and main().
|
static |
buffer for command line
Referenced by main().