Microchip® Advanced Software Framework

fsaccess.h File Reference
#include <stdio.h>
#include "file.h"
#include "navigation.h"
#include "ctrl_access.h"

Macros

#define O_APPEND   0x0008
 
#define O_CREAT   0x0200
 
#define O_RDONLY   0
 
#define O_RDWR   0x0002
 
#define O_WRONLY   0x0001
 

Typedefs

typedef signed int ssize_t
 

Functions

bool b_fsaccess_init (void)
 This function initializes mutex and navigators. More...
 
int close (int fd)
 This function closes a file. More...
 
long fsaccess_alloc_nav_id (void)
 This function returns a free navigator id. More...
 
size_t fsaccess_file_get_size (int fd)
 This function returns the opened file size. More...
 
void fsaccess_free_nav_id (int fd)
 This function frees a navigator id. More...
 
void fsaccess_give_mutex (void)
 This function frees the mutex. More...
 
int8_t fsaccess_IsDirPresent (const char *pcStringDirName)
 Is a directory present? More...
 
void fsaccess_take_mutex (void)
 This function gives the mutex to the caller. More...
 
int open (const char *pathname, int flags,...)
 This function opens a file. More...
 
ssize_t read (int fd, void *buf, size_t count)
 This function reads from a file. More...
 
ssize_t write (int fd, const void *buf, size_t count)
 This function writes to a file. More...
 

#define O_APPEND   0x0008

Referenced by main(), and open().

#define O_CREAT   0x0200

Referenced by main(), and open().

#define O_RDONLY   0
#define O_RDWR   0x0002

Referenced by open().

#define O_WRONLY   0x0001

Referenced by open().

typedef signed int ssize_t

bool b_fsaccess_init ( void  )

This function initializes mutex and navigators.

References nav_reset().

Referenced by main().

int close ( int  fd)

This function closes a file.

Parameters
fdfile descriptor.
Returns
int : -1 if error, 0 otherwise

References file_close(), fsaccess_free_nav_id(), fsaccess_give_mutex(), fsaccess_take_mutex(), and nav_select().

Referenced by fsaccess_example_read(), and fsaccess_example_write().

long fsaccess_alloc_nav_id ( void  )

This function returns a free navigator id.

Returns
long : Id navigator allocated or -1 if none free

References FS_NB_NAVIGATOR, FS_NB_RESERVED_NAV, pvNavUsed, Set_bits, and Tst_bits.

Referenced by fsaccess_IsDirPresent(), and open().

size_t fsaccess_file_get_size ( int  fd)

This function returns the opened file size.

Parameters
fdfile descriptor.
Returns
size_t : size of the file pointed to by the descriptor

References fsaccess_give_mutex(), fsaccess_take_mutex(), nav_file_lgt(), and nav_select().

Referenced by fsaccess_example_read(), and fsaccess_example_write().

void fsaccess_free_nav_id ( int  fd)

This function frees a navigator id.

Parameters
fdfile descriptor.

References Clr_bits, and pvNavUsed.

Referenced by close(), fsaccess_IsDirPresent(), and open().

void fsaccess_give_mutex ( void  )

This function frees the mutex.

Referenced by close(), fsaccess_file_get_size(), fsaccess_IsDirPresent(), open(), read(), and write().

int8_t fsaccess_IsDirPresent ( const char *  pcStringDirName)

Is a directory present?

Parameters
pcStringDirNameInput. Directory name string.
Returns
1 if the directory exists, 0 if the directory doesn't exist, else -1

References false, fsaccess_alloc_nav_id(), fsaccess_free_nav_id(), fsaccess_give_mutex(), fsaccess_take_mutex(), nav_select(), and nav_setcwd().

void fsaccess_take_mutex ( void  )

This function gives the mutex to the caller.

Referenced by close(), fsaccess_file_get_size(), fsaccess_IsDirPresent(), open(), read(), and write().

int open ( const char *  pathname,
int  flags,
  ... 
)

This function opens a file.

Parameters
pathnamepath of the file to open.
flagsflags to give file access rights should be O_CREAT : create file if not exist O_APPEND : add data to the end of file O_RDONLY : Read Only O_WRONLY : Write Only O_RDWR : Read/Write
Returns
int : file descriptor (>= 0 if OK (NavID), -1 otherwise)

This function opens a file.

This function opens a file.

Parameters
pathnamepath of the file to open.
flagsflags to give file access rights should be O_CREAT : create file if not exist O_APPEND : add data to the end of file O_RDONLY : Read Only O_WRONLY : Write Only O_RDWR : Read/Write
Returns
int : file descriptor (>= 0 if OK (NavID), -1 otherwise)

References file_open(), FOPEN_MODE_APPEND, FOPEN_MODE_R, FOPEN_MODE_R_PLUS, FOPEN_MODE_W, fsaccess_alloc_nav_id(), fsaccess_free_nav_id(), fsaccess_give_mutex(), fsaccess_take_mutex(), nav_select(), nav_setcwd(), O_APPEND, O_CREAT, O_RDWR, and O_WRONLY.

Referenced by fsaccess_example_read(), and fsaccess_example_write().

ssize_t read ( int  fd,
void *  buf,
size_t  count 
)

This function reads from a file.

Parameters
fdfile descriptor.
bufpointer for data that are read.
countamount of bytes to read
Returns
ssize_t : amount of data read (-1 if error)

References file_eof(), file_read_buf(), fsaccess_give_mutex(), fsaccess_take_mutex(), and nav_select().

Referenced by fsaccess_example_read(), and fsaccess_example_write().

ssize_t write ( int  fd,
const void *  buf,
size_t  count 
)

This function writes to a file.

Parameters
fdfile descriptor.
bufpointer from where data are written.
countamount of bytes to write
Returns
ssize_t : amount of data written (-1 if error)

References file_write_buf(), fsaccess_give_mutex(), fsaccess_take_mutex(), and nav_select().

Referenced by fsaccess_example_write().