Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
LIN software stack

LIN software stack for 32-bit AVR that supports initializing the LIN bus and to transmit/receive messages.

Data Structures

struct  st_lin_message
 This structure allows to handle a LIN message and, at the end of the received/transmitted message, allows to call a function associated to this message, the update or the capture of "signals". More...
 

Macros

#define LIN_LAST_ERR_LENGHT   0x04
 Default length of the 'lin_last_error[]' array. More...
 
#define LIN_OVERLOAD_INT   ((U16)0x00FF)
 Error report definitions. More...
 
#define NUMBER_OF_LIN_FRAMES_NODE0   8
 
#define NUMBER_OF_LIN_FRAMES_NODE1   8
 

Enumerations

enum  enum_lin_cmd {
  PUBLISH,
  SUBSCRIBE,
  IGNORE
}
 This enumeration is used to select an action for a specific message declared in st_lin_message structure. Note: XXX_STAND_BY keeps the direction (PUBLISH or SUBSCRIBE) for a message that will be IGNORE. When the 'stand_by' will be finished, PUBLISH_STAND_BY would become PUBLISH and SUBSCRIBE_STAND_BY would become SUBSCRIBE. An IGNORE message could become either PUBLISH or SUBSCRIBE. More...
 

Functions

U8 lin_init (bool master, U8 l_node, U16 b_rate, long pba_hz)
 This function initializes the LIN controller and, if needed, the LIN interrupts. More...
 
U8 lin_send_cmd (U8 l_node, U8 l_id, U8 l_len)
 This function commands the sending of the LIN header, MASTER task of MASTER node. More...
 

Variables

volatile st_lin_message lin_descript_list_node0 [NUMBER_OF_LIN_FRAMES_NODE0]
 Array of structure of type:'st_lin_message'. Default: 8 elements. More...
 
volatile st_lin_message lin_descript_list_node1 [NUMBER_OF_LIN_FRAMES_NODE1]
 
volatile U16 lin_error_number_node0
 Counter of LIN error. If an error clearly linked to a message (i.e. time-out) the status of this message is written with the error (LINERR). More...
 
volatile U16 lin_error_number_node1
 
volatile U8 lin_handle_node0
 Index in lin_descript_list[], 'lin_handle' is set after processing IDOK and verified once RXOK or TXOK rises. More...
 
volatile U8 lin_handle_node1
 
volatile U16 lin_last_errors_node0 []
 Last error FIFO: lin_handle | status. Default: 4 elements. More...
 
volatile U16 lin_last_errors_node1 []
 

LIN Versions

#define LIN_2x   0
 Lin 2.x Version. More...
 
#define LIN_1x   1
 Lin 1.x Version. More...
 

#define LIN_1x   1

Lin 1.x Version.

#define LIN_2x   0

Lin 2.x Version.

#define LIN_LAST_ERR_LENGHT   0x04

Default length of the 'lin_last_error[]' array.

Referenced by lin_int_handler_node0(), and lin_int_handler_node1().

#define LIN_OVERLOAD_INT   ((U16)0x00FF)

Error report definitions.

More than ONE interrupt in the same time !

#define NUMBER_OF_LIN_FRAMES_NODE0   8
#define NUMBER_OF_LIN_FRAMES_NODE1   8

This enumeration is used to select an action for a specific message declared in st_lin_message structure. Note: XXX_STAND_BY keeps the direction (PUBLISH or SUBSCRIBE) for a message that will be IGNORE. When the 'stand_by' will be finished, PUBLISH_STAND_BY would become PUBLISH and SUBSCRIBE_STAND_BY would become SUBSCRIBE. An IGNORE message could become either PUBLISH or SUBSCRIBE.

Enumerator
PUBLISH 

The node sends the response.

SUBSCRIBE 

The node receives the response.

IGNORE 

The node is not concerned by the response, it doesn't send or receive.

U8 lin_init ( bool  master,
U8  l_node,
U16  b_rate,
long  pba_hz 
)

This function initializes the LIN controller and, if needed, the LIN interrupts.

Parameters
mastertrue for master, false for slave
b_rateBaudrate Value
l_nodeNode Value
pba_hzPBA Value
Returns
Status PASS / FAIL
Parameters
mastertrue for master, false for slave
l_nodeNode Value
b_rateBaudrate Value
pba_hzPBA Value
Returns
Status PASS / FAIL

Enable Interrupt for Error flags and end ID Reception

Register Interrupt for LIN

Register Interrupt for PDCA Transfer TX

Register Interrupt for PDCA Transfer RX

Enable Interrupt for Error flags and end ID Reception

Register Interrupt for LIN

Register Interrupt for PDCA Transfer TX

Register Interrupt for PDCA Transfer RX

References Disable_global_interrupt, gpio_enable_module(), gpio_enable_pin_pull_up(), INTC_register_interrupt(), lin_int_handler_node0(), lin_int_handler_node1(), lin_pdca_int_rx_handler_node0(), lin_pdca_int_rx_handler_node1(), lin_pdca_int_tx_handler_node0(), lin_pdca_int_tx_handler_node1(), PASS, usart_lin_node0, USART_LIN_NODE0_PDCA_RX_IRQ, USART_LIN_NODE0_PDCA_RX_IRQ_LEVEL, USART_LIN_NODE0_PDCA_TX_IRQ, USART_LIN_NODE0_PDCA_TX_IRQ_LEVEL, USART_LIN_NODE0_RX_PIN, USART_LIN_NODE0_USART_IRQ, USART_LIN_NODE0_USART_IRQ_LEVEL, usart_lin_node1, USART_LIN_NODE1_PDCA_RX_IRQ, USART_LIN_NODE1_PDCA_RX_IRQ_LEVEL, USART_LIN_NODE1_PDCA_TX_IRQ, USART_LIN_NODE1_PDCA_TX_IRQ_LEVEL, USART_LIN_NODE1_RX_PIN, USART_LIN_NODE1_USART_IRQ, and USART_LIN_NODE1_USART_IRQ_LEVEL.

Referenced by main().

U8 lin_send_cmd ( U8  l_node,
U8  l_id,
U8  l_len 
)

This function commands the sending of the LIN header, MASTER task of MASTER node.

Parameters
l_idLIN identifier value. In case of `LIN_1X', the coded length is transported into the LIN identifier.
l_lenTrue length (not coded), number of data bytes transported in the response. This information is not used in `LIN_1X' because it is coded in `l_id'.
l_nodeNode Value
Returns
Status PASS / FAIL
Parameters
l_nodeNode Value
l_idLIN identifier value. In case of `LIN_1X', the coded length is transported into the LIN identifier.
l_lenTrue length (not coded), number of data bytes transported in the response. This information is not used in `LIN_1X' because it is coded in `l_id'.
Returns
Status PASS / FAIL

References FAIL, lin_rx_response(), lin_tx_header_and_response(), NUMBER_OF_LIN_FRAMES_NODE0, NUMBER_OF_LIN_FRAMES_NODE1, PASS, PUBLISH, SUBSCRIBE, usart_lin_node0, usart_lin_node1, and usart_reset_status().

Referenced by lin_master_task_ID12(), and lin_master_task_ID15().

volatile st_lin_message lin_descript_list_node0[NUMBER_OF_LIN_FRAMES_NODE0]

Array of structure of type:'st_lin_message'. Default: 8 elements.

Referenced by lin_master_task_ID12(), lin_master_task_ID15(), and main().

volatile st_lin_message lin_descript_list_node1[NUMBER_OF_LIN_FRAMES_NODE1]
volatile U16 lin_error_number_node0

Counter of LIN error. If an error clearly linked to a message (i.e. time-out) the status of this message is written with the error (LINERR).

Referenced by lin_int_handler_node0().

volatile U16 lin_error_number_node1

Referenced by lin_int_handler_node1().

volatile U8 lin_handle_node0

Index in lin_descript_list[], 'lin_handle' is set after processing IDOK and verified once RXOK or TXOK rises.

Referenced by lin_int_handler_node0(), lin_pdca_int_rx_handler_node0(), and lin_pdca_int_tx_handler_node0().

volatile U16 lin_last_errors_node0[]

Last error FIFO: lin_handle | status. Default: 4 elements.

Referenced by lin_int_handler_node0().

volatile U16 lin_last_errors_node1[]

Referenced by lin_int_handler_node1().