This group contains functions and definitions related to configuring and enabling/disabling on-chip oscillators.
Internal RC-oscillators, external crystal oscillators and external clock generators are supported by this module. What all of these have in common is that they swing at a fixed, nominal frequency which is normally not adjustable.
The following example demonstrates how to enable the external oscillator on XMEGA A and wait for it to be ready to use. The oscillator identifiers are platform-specific, so while the same procedure is used on all platforms, the parameter to osc_enable() will be different from device to device.
If external oscillators are used, the board code must provide the following definitions for each of those:
Macros | |
#define | OSC0_MODE_VALUE UNDEFINED |
Board-dependent value written to the MODE bitfield of PM_OSCCTRL(0) More... | |
#define | OSC0_STARTUP_TIMEOUT UNDEFINED |
Number of slow clock cycles to wait for OSC0 to start. More... | |
#define | OSC0_STARTUP_VALUE UNDEFINED |
Board-dependent value written to the STARTUP bitfield of PM_OSCCTRL(0) More... | |
#define | OSC32_MODE_VALUE OSC32_MODE_XTAL |
#define | OSC32_STARTUP_VALUE OSC32_STARTUP_131072 |
Functions | |
void | osc_priv_disable_osc0 (void) |
void | osc_priv_disable_osc32 (void) |
void | osc_priv_disable_rc120m (void) |
void | osc_priv_disable_rc32k (void) |
void | osc_priv_enable_osc0 (void) |
void | osc_priv_enable_osc32 (void) |
void | osc_priv_enable_rc120m (void) |
void | osc_priv_enable_rc32k (void) |
Oscillator Management | |
static void | osc_wait_ready (uint8_t id) |
Wait until the oscillator identified by id is ready. More... | |
static void | osc_enable (uint8_t id) |
Enable oscillator id. More... | |
static void | osc_disable (uint8_t id) |
Disable oscillator id. More... | |
static bool | osc_is_ready (uint8_t id) |
Determine whether oscillator id is ready. More... | |
static uint32_t | osc_get_rate (uint8_t id) |
Return the frequency of oscillator id in Hz. More... | |
Oscillator identifiers | |
#define | OSC_ID_OSC0 0 |
External Oscillator 0. More... | |
#define | OSC_ID_OSC32 1 |
External 32 kHz oscillator. More... | |
#define | OSC_ID_RC32K 2 |
Internal 32 kHz RC oscillator. More... | |
#define | OSC_ID_RC120M 3 |
Internal 120 MHz RC oscillator. More... | |
#define | OSC_ID_RCSYS 4 |
Internal System RC oscillator. More... | |
OSC0 mode values | |
#define | OSC_MODE_EXTERNAL AVR32_SCIF_OSCCTRL0_MODE_EXT_CLOCK |
External clock connected to XIN. More... | |
#define | OSC_MODE_XTAL AVR32_SCIF_OSCCTRL0_MODE_CRYSTAL |
Crystal connected to XIN/XOUT. More... | |
OSC32 mode values | |
#define | OSC32_MODE_EXTERNAL AVR32_SCIF_OSCCTRL32_MODE_EXT_CLOCK |
External clock connected to XIN32. More... | |
#define | OSC32_MODE_XTAL AVR32_SCIF_OSCCTRL32_MODE_CRYSTAL_AGC |
Crystal connected to XIN32/XOUT32. More... | |
#define | OSC32_MODE_XTAL_HC AVR32_SCIF_OSCCTRL32_MODE_CRYSTAL_NO_AGC |
Crystal connected to XIN32/XOUT32 in high current mode. More... | |
OSC0 startup values | |
#define | OSC_STARTUP_0 AVR32_SCIF_OSCCTRL0_STARTUP_0_RCOSC |
0 cycles More... | |
#define | OSC_STARTUP_64 AVR32_SCIF_OSCCTRL0_STARTUP_64_RCOSC |
64 cycles (560 us) More... | |
#define | OSC_STARTUP_128 AVR32_SCIF_OSCCTRL0_STARTUP_128_RCOSC |
128 cycles (1.1 ms) More... | |
#define | OSC_STARTUP_2048 AVR32_SCIF_OSCCTRL0_STARTUP_2048_RCOSC |
2048 cycles (18 ms) More... | |
#define | OSC_STARTUP_4096 AVR32_SCIF_OSCCTRL0_STARTUP_4096_RCOSC |
4096 cycles (36 ms) More... | |
#define | OSC_STARTUP_8192 AVR32_SCIF_OSCCTRL0_STARTUP_8192_RCOSC |
8192 cycles (71 ms) More... | |
#define | OSC_STARTUP_16384 AVR32_SCIF_OSCCTRL0_STARTUP_16384_RCOSC |
16384 cycles (142 ms) More... | |
OSC32 startup values | |
#define | OSC32_STARTUP_0 AVR32_SCIF_OSCCTRL32_STARTUP_0_RCOSC |
0 cycles More... | |
#define | OSC32_STARTUP_128 AVR32_SCIF_OSCCTRL32_STARTUP_128_RCOSC |
128 cycles (1.1 ms) More... | |
#define | OSC32_STARTUP_8192 AVR32_SCIF_OSCCTRL32_STARTUP_8192_RCOSC |
8192 cycles (72.3 ms) More... | |
#define | OSC32_STARTUP_16384 AVR32_SCIF_OSCCTRL32_STARTUP_16384_RCOSC |
16384 cycles (143 ms) More... | |
#define | OSC32_STARTUP_65536 AVR32_SCIF_OSCCTRL32_STARTUP_65536_RCOSC |
65536 cycles (570 ms) More... | |
#define | OSC32_STARTUP_131072 AVR32_SCIF_OSCCTRL32_STARTUP_131072_RCOSC |
131072 cycles (1.1 s) More... | |
#define | OSC32_STARTUP_262144 AVR32_SCIF_OSCCTRL32_STARTUP_262144_RCOSC |
262144 cycles (2.3 s) More... | |
#define | OSC32_STARTUP_524288 AVR32_SCIF_OSCCTRL32_STARTUP_524288_RCOSC |
524288 cycles (4.6 s) More... | |
Board-specific configuration parameters | |
The following definitions must be provided by the board code for all working oscillators on the board. | |
#define | BOARD_OSC32_HZ 32768 |
Clock frequency of OSC32 in Hz. More... | |
#define | BOARD_OSC32_STARTUP_US 920000 |
Startup time of OSC32 in microseconds. More... | |
#define | BOARD_OSC32_IS_XTAL true |
OSC32 uses a crystal, not an external clock. More... | |
#define | BOARD_OSC32_PINSEL 1 |
If set to 1, use XIN32_2/XOUT32_2 pins for OSC32. More... | |
RC oscillator frequency limits | |
The frequency of the internal RC oscillators may drift a bit as a result of temperature changes. These definitions provide upper and lower limits which may be used to calculate upper and lower limits of timeouts, derived clock frequencies, etc. | |
#define | OSC_RCSYS_NOMINAL_HZ 115000 |
Nominal frequency of RCSYS in Hz. More... | |
#define | OSC_RCSYS_MIN_HZ 100000 |
Minimum frequency of RCSYS in Hz. More... | |
#define | OSC_RCSYS_MAX_HZ 120000 |
Maximum frequency of RCSYS in Hz. More... | |
#define | OSC_RC32K_NOMINAL_HZ 32000 |
Nominal frequency of RC32K in Hz. More... | |
#define | OSC_RC32K_MIN_HZ 20000 |
Minimum frequency of RC32K in Hz. More... | |
#define | OSC_RC32K_MAX_HZ 44000 |
Maximum frequency of RC32K in Hz. More... | |
#define | OSC_RC120M_NOMINAL_HZ 120000000 |
Nominal frequency of RC120M in Hz. More... | |
#define BOARD_OSC32_HZ 32768 |
Clock frequency of OSC32 in Hz.
Referenced by dfll_priv_get_source_hz(), and osc_get_rate().
#define BOARD_OSC32_IS_XTAL true |
OSC32 uses a crystal, not an external clock.
#define BOARD_OSC32_PINSEL 1 |
If set to 1, use XIN32_2/XOUT32_2 pins for OSC32.
If not defined, the primary XIN32/XOUT32 pins are used.
Referenced by ast_init().
#define BOARD_OSC32_STARTUP_US 920000 |
Startup time of OSC32 in microseconds.
#define OSC0_MODE_VALUE UNDEFINED |
Board-dependent value written to the MODE bitfield of PM_OSCCTRL(0)
#define OSC0_STARTUP_TIMEOUT UNDEFINED |
Number of slow clock cycles to wait for OSC0 to start.
This is the number of slow clock cycles corresponding to OSC0_STARTUP_VALUE with an additional 25% safety margin. If the oscillator isn't running when this timeout has expired, it is assumed to have failed to start.
#define OSC0_STARTUP_VALUE UNDEFINED |
Board-dependent value written to the STARTUP bitfield of PM_OSCCTRL(0)
#define OSC32_MODE_EXTERNAL AVR32_SCIF_OSCCTRL32_MODE_EXT_CLOCK |
External clock connected to XIN32.
#define OSC32_MODE_VALUE OSC32_MODE_XTAL |
#define OSC32_MODE_XTAL AVR32_SCIF_OSCCTRL32_MODE_CRYSTAL_AGC |
Crystal connected to XIN32/XOUT32.
#define OSC32_MODE_XTAL_HC AVR32_SCIF_OSCCTRL32_MODE_CRYSTAL_NO_AGC |
Crystal connected to XIN32/XOUT32 in high current mode.
#define OSC32_STARTUP_0 AVR32_SCIF_OSCCTRL32_STARTUP_0_RCOSC |
0 cycles
#define OSC32_STARTUP_128 AVR32_SCIF_OSCCTRL32_STARTUP_128_RCOSC |
128 cycles (1.1 ms)
#define OSC32_STARTUP_131072 AVR32_SCIF_OSCCTRL32_STARTUP_131072_RCOSC |
131072 cycles (1.1 s)
#define OSC32_STARTUP_16384 AVR32_SCIF_OSCCTRL32_STARTUP_16384_RCOSC |
16384 cycles (143 ms)
#define OSC32_STARTUP_262144 AVR32_SCIF_OSCCTRL32_STARTUP_262144_RCOSC |
262144 cycles (2.3 s)
#define OSC32_STARTUP_524288 AVR32_SCIF_OSCCTRL32_STARTUP_524288_RCOSC |
524288 cycles (4.6 s)
#define OSC32_STARTUP_65536 AVR32_SCIF_OSCCTRL32_STARTUP_65536_RCOSC |
65536 cycles (570 ms)
#define OSC32_STARTUP_8192 AVR32_SCIF_OSCCTRL32_STARTUP_8192_RCOSC |
8192 cycles (72.3 ms)
Referenced by ast_init().
#define OSC32_STARTUP_VALUE OSC32_STARTUP_131072 |
#define OSC_ID_OSC0 0 |
External Oscillator 0.
Referenced by dfll_enable_source(), genclk_enable_source(), osc_disable(), osc_enable(), osc_get_rate(), osc_is_ready(), and sysclk_init().
#define OSC_ID_OSC32 1 |
External 32 kHz oscillator.
Referenced by dfll_enable_source(), genclk_enable_source(), osc_disable(), osc_enable(), osc_get_rate(), and osc_is_ready().
#define OSC_ID_RC120M 3 |
Internal 120 MHz RC oscillator.
Referenced by dfll_enable_source(), genclk_enable_source(), osc_disable(), osc_enable(), osc_get_rate(), osc_is_ready(), and sysclk_init().
#define OSC_ID_RC32K 2 |
Internal 32 kHz RC oscillator.
Referenced by dfll_enable_source(), genclk_enable_source(), osc_disable(), osc_enable(), osc_get_rate(), and osc_is_ready().
#define OSC_ID_RCSYS 4 |
Internal System RC oscillator.
Referenced by osc_disable(), osc_enable(), osc_get_rate(), and osc_is_ready().
#define OSC_MODE_EXTERNAL AVR32_SCIF_OSCCTRL0_MODE_EXT_CLOCK |
External clock connected to XIN.
#define OSC_MODE_XTAL AVR32_SCIF_OSCCTRL0_MODE_CRYSTAL |
Crystal connected to XIN/XOUT.
#define OSC_RC120M_NOMINAL_HZ 120000000 |
Nominal frequency of RC120M in Hz.
Referenced by dfll_priv_get_source_hz(), osc_get_rate(), and sysclk_get_main_hz().
#define OSC_RC32K_MAX_HZ 44000 |
Maximum frequency of RC32K in Hz.
#define OSC_RC32K_MIN_HZ 20000 |
Minimum frequency of RC32K in Hz.
#define OSC_RC32K_NOMINAL_HZ 32000 |
Nominal frequency of RC32K in Hz.
Referenced by dfll_priv_get_source_hz(), and osc_get_rate().
#define OSC_RCSYS_MAX_HZ 120000 |
Maximum frequency of RCSYS in Hz.
#define OSC_RCSYS_MIN_HZ 100000 |
Minimum frequency of RCSYS in Hz.
#define OSC_RCSYS_NOMINAL_HZ 115000 |
Nominal frequency of RCSYS in Hz.
Referenced by dfll_priv_get_source_hz(), osc_get_rate(), and sysclk_get_main_hz().
#define OSC_STARTUP_0 AVR32_SCIF_OSCCTRL0_STARTUP_0_RCOSC |
0 cycles
#define OSC_STARTUP_128 AVR32_SCIF_OSCCTRL0_STARTUP_128_RCOSC |
128 cycles (1.1 ms)
#define OSC_STARTUP_16384 AVR32_SCIF_OSCCTRL0_STARTUP_16384_RCOSC |
16384 cycles (142 ms)
#define OSC_STARTUP_2048 AVR32_SCIF_OSCCTRL0_STARTUP_2048_RCOSC |
2048 cycles (18 ms)
#define OSC_STARTUP_4096 AVR32_SCIF_OSCCTRL0_STARTUP_4096_RCOSC |
4096 cycles (36 ms)
#define OSC_STARTUP_64 AVR32_SCIF_OSCCTRL0_STARTUP_64_RCOSC |
64 cycles (560 us)
#define OSC_STARTUP_8192 AVR32_SCIF_OSCCTRL0_STARTUP_8192_RCOSC |
8192 cycles (71 ms)
|
inlinestatic |
Disable oscillator id.
References OSC_ID_OSC0, OSC_ID_OSC32, OSC_ID_RC120M, OSC_ID_RC32K, OSC_ID_RCSYS, osc_priv_disable_osc0(), osc_priv_disable_osc32(), osc_priv_disable_rc120m(), and osc_priv_disable_rc32k().
|
inlinestatic |
Enable oscillator id.
The startup time and mode value is automatically determined based on definitions in the board code.
References OSC_ID_OSC0, OSC_ID_OSC32, OSC_ID_RC120M, OSC_ID_RC32K, OSC_ID_RCSYS, osc_priv_enable_osc0(), osc_priv_enable_osc32(), osc_priv_enable_rc120m(), and osc_priv_enable_rc32k().
Referenced by dfll_enable_source(), genclk_enable_source(), and sysclk_init().
|
inlinestatic |
Return the frequency of oscillator id in Hz.
References BOARD_OSC32_HZ, OSC_ID_OSC0, OSC_ID_OSC32, OSC_ID_RC120M, OSC_ID_RC32K, OSC_ID_RCSYS, OSC_RC120M_NOMINAL_HZ, OSC_RC32K_NOMINAL_HZ, and OSC_RCSYS_NOMINAL_HZ.
|
inlinestatic |
Determine whether oscillator id is ready.
true | Oscillator id is running and ready to use as a clock source. |
false | Oscillator id is not running. |
References OSC_ID_OSC0, OSC_ID_OSC32, OSC_ID_RC120M, OSC_ID_RC32K, and OSC_ID_RCSYS.
Referenced by dfll_enable_source(), genclk_enable_source(), and osc_wait_ready().
void osc_priv_disable_osc0 | ( | void | ) |
Referenced by osc_disable().
void osc_priv_disable_osc32 | ( | void | ) |
Referenced by osc_disable().
void osc_priv_disable_rc120m | ( | void | ) |
References cpu_irq_restore(), and cpu_irq_save().
Referenced by osc_disable().
void osc_priv_disable_rc32k | ( | void | ) |
References cpu_irq_restore(), and cpu_irq_save().
Referenced by osc_disable().
void osc_priv_enable_osc0 | ( | void | ) |
Referenced by osc_enable().
void osc_priv_enable_osc32 | ( | void | ) |
Referenced by osc_enable().
void osc_priv_enable_rc120m | ( | void | ) |
References cpu_irq_restore(), and cpu_irq_save().
Referenced by osc_enable().
void osc_priv_enable_rc32k | ( | void | ) |
References cpu_irq_restore(), and cpu_irq_save().
Referenced by osc_enable().
|
inlinestatic |
Wait until the oscillator identified by id is ready.
This function will busy-wait for the oscillator identified by id to become stable and ready to use as a clock source.
id | A number identifying the oscillator to wait for. |
References osc_is_ready().
Referenced by dfll_enable_source(), genclk_enable_source(), and sysclk_init().