#include "compiler.h"
#include "conf_example.h"
#include "gpio.h"
#include "sysclk.h"
#include "tc.h"
#include "intc.h"
#include "touch_api.h"
#include "QDebug.h"
#include "QDebugTransport.h"
Macros | |
#define | PORTA (((volatile avr32_gpio_port_t *) &AVR32_GPIO) + 0) |
#define | PORTB (((volatile avr32_gpio_port_t *) &AVR32_GPIO) + 1) |
#define | PORTC (((volatile avr32_gpio_port_t *) &AVR32_GPIO) + 2) |
SENSOR STATE CONFIGURATIONS | |
#define | GET_SENSOR_STATE(SENSOR_NUMBER) qt_measure_data.qt_touch_status.sensor_states[(SENSOR_NUMBER/8)] & (1 << (SENSOR_NUMBER % 8)) |
To get the sensor state that it is in detect or not. More... | |
#define | GET_ROTOR_SLIDER_POSITION(ROTOR_SLIDER_NUMBER) qt_measure_data.qt_touch_status.rotor_slider_values[ROTOR_SLIDER_NUMBER] |
To get the rotor angle or slider position. More... | |
Functions | |
static void | config_keys (void) |
prototypes for rotor_slider configuration for various channels More... | |
static void | config_sensors (void) |
Configure the sensors. More... | |
static void | init_timer_isr (void) |
Configures ISR to fire regularly. More... | |
ISR (tc_irq, GRP, LVL) | |
TIMER ISR. More... | |
int | main (void) |
Main Application Code. More... | |
int16_t | qt_get_sensor_delta (uint8_t sensor) |
Get sensor delta values. More... | |
static void | qt_set_parameters (void) |
Initializes configuration data for processing. More... | |
static void | qtouch_init (void) |
Initializes the necessary parameters for QTouch library. More... | |
Variables | |
static volatile uint16_t | current_time_ms_touch = 0u |
qt_touch_lib_measure_data_t * | pqt_measure_data = &qt_measure_data |
Output can be observed in the watch window using this pointer. More... | |
qt_touch_lib_config_data_t | qt_config_data |
This configuration data structure parameters if needs to be changed will be changed in the qt_set_parameters function. More... | |
qt_touch_lib_measure_data_t | qt_measure_data |
Touch Measurement data. More... | |
uint16_t | qt_measurement_period_msec = 25u |
timer period in msec. More... | |
static volatile uint8_t | time_to_measure_touch = 0u |
uint16_t | timestamp1_hword |
Time stamp information. More... | |
uint16_t | timestamp1_lword |
uint16_t | timestamp2_hword |
uint16_t | timestamp2_lword |
uint16_t | timestamp3_hword |
uint16_t | timestamp3_lword |
#define GET_ROTOR_SLIDER_POSITION | ( | ROTOR_SLIDER_NUMBER | ) | qt_measure_data.qt_touch_status.rotor_slider_values[ROTOR_SLIDER_NUMBER] |
To get the rotor angle or slider position.
These values are valid only when the sensor state for corresponding rotor or slider shows in detect.
ROTOR_SLIDER_NUMBER | for which the position to be known |
#define GET_SENSOR_STATE | ( | SENSOR_NUMBER | ) | qt_measure_data.qt_touch_status.sensor_states[(SENSOR_NUMBER/8)] & (1 << (SENSOR_NUMBER % 8)) |
To get the sensor state that it is in detect or not.
SENSOR_NUMBER | for which the state to be detected |
#define PORTA (((volatile avr32_gpio_port_t *) &AVR32_GPIO) + 0) |
#define PORTB (((volatile avr32_gpio_port_t *) &AVR32_GPIO) + 1) |
#define PORTC (((volatile avr32_gpio_port_t *) &AVR32_GPIO) + 2) |
|
static |
prototypes for rotor_slider configuration for various channels
Configure the sensors as keys only.
Configure the sensors for Keys configuration
Referenced by config_sensors().
|
static |
Configure the sensors.
Configure the QTouch sensors.
References config_keys().
Referenced by qtouch_init().
|
static |
Configures ISR to fire regularly.
Function to initialize the Timer/Counter module in Waveform mode.
It fires the ISR at regular intervals to start QTouch Acquisition.
References AVR32_INTC_INT0, tc_waveform_opt_t::channel, tc_interrupt_t::etrgs, irq_initialize_vectors, irq_register_handler, sysclk_get_pba_hz(), TC_CHANNEL, TC_CLOCK, tc_configure_interrupts(), TC_EVT_EFFECT_NOOP, tc_init_waveform(), TC_IRQ, TC_SEL_NO_EDGE, tc_start(), TC_WAVEFORM_SEL_UP_MODE_RC_TRIGGER, and tc_write_rc().
Referenced by main().
TIMER ISR.
tc_irq | is the subroutine function name |
GRP | is the group under which the interrupt lies |
LVL | is the priority level assigned for the group |
References current_time_ms_touch, qt_measurement_period_msec, TC_CHANNEL, tc_read_sr(), and time_to_measure_touch.
int main | ( | void | ) |
Main Application Code.
Initialize the system clock Clock settings are done in cof_clock.h It sets the cpu to run at crystal frequency which uses OSC0 as souce
Initializes the functions necessary for QTouch
Configure the timer ISR to fire regularly for QTouch Acquisition
Address to pass address of user functions
This function is called after the library has made capacitive measurements, but before it has processed them. The user can use this hook to apply filter functions to the measured signal values.(Possibly to fix sensor layout faults)
References cpu_irq_enable, current_time_ms_touch, gpio_clr_gpio_pin(), gpio_set_gpio_pin(), init_timer_isr(), QDebug_Init(), QDebug_ProcessCommands(), QDebug_SendData(), qt_filter_callback, qt_measure_sensors(), tag_qt_touch_lib_measure_data_t::qt_touch_status, QTLIB_BURST_AGAIN, qtouch_init(), tag_qt_touch_status_t::sensor_states, STATUS_LED, sysclk_init(), and time_to_measure_touch.
int16_t qt_get_sensor_delta | ( | uint8_t | sensor | ) |
Get sensor delta values.
Referenced by Transmit_Delta().
|
static |
Initializes configuration data for processing.
Initialize configuration data for processing This will fill the default threshold values in the configuration data structure.But User can change the values of these parameters.
This will fill the default threshold values in the configuration data structure.But User can change the values of these parameters. Values can be changed in "touch_api.h"
Values can be changed in "touch_api.h"
This can be modified by the user to different values
References tag_qt_touch_lib_config_data_t::qt_di, tag_qt_touch_lib_config_data_t::qt_drift_hold_time, tag_qt_touch_lib_config_data_t::qt_max_on_duration, tag_qt_touch_lib_config_data_t::qt_neg_drift_rate, tag_qt_touch_lib_config_data_t::qt_pos_drift_rate, tag_qt_touch_lib_config_data_t::qt_pos_recal_delay, and tag_qt_touch_lib_config_data_t::qt_recal_threshold.
Referenced by qtouch_init().
|
static |
Initializes the necessary parameters for QTouch library.
Initialize QTouch Configuration and sensors.
Configures sensors for rotor, slider or for button based on the options given in the SYMBOLS
References config_sensors(), qt_init_sensing, and qt_set_parameters().
Referenced by main().
qt_touch_lib_measure_data_t* pqt_measure_data = &qt_measure_data |
Output can be observed in the watch window using this pointer.
qt_touch_lib_config_data_t qt_config_data |
This configuration data structure parameters if needs to be changed will be changed in the qt_set_parameters function.
Referenced by Set_Global_Config(), and Transmit_Global_Config().
qt_touch_lib_measure_data_t qt_measure_data |
Touch Measurement data.
Referenced by Transmit_Ref(), Transmit_Signals(), and Transmit_State().
uint16_t timestamp1_hword |
Time stamp information.
Referenced by Transmit_Time_Stamps().
uint16_t timestamp1_lword |
Referenced by Transmit_Time_Stamps().
uint16_t timestamp2_hword |
Referenced by Transmit_Time_Stamps().
uint16_t timestamp2_lword |
Referenced by Transmit_Time_Stamps().
uint16_t timestamp3_hword |
Referenced by Transmit_Time_Stamps().
uint16_t timestamp3_lword |
Referenced by Transmit_Time_Stamps().