Macros | |
#define | _STATIC_PORT_PIN_CONF_ 1 |
#define | INTRABURST_1 0 |
#define | INTRABURST_2 0 |
#define | QTOUCH_SNS_PORT_COUNT 1 |
QTOUCH LIBRARY CONFIGURATION | |
#define | _ROTOR_SLIDER_ |
Rotor/slider can be added to the design, if this macro is enabled. More... | |
#define _ROTOR_SLIDER_ |
Rotor/slider can be added to the design, if this macro is enabled.
Defined in the Symbols in Project Properties
#define _STATIC_PORT_PIN_CONF_ 1 |
#define INTRABURST_1 0 |
#define INTRABURST_2 0 |
#define QTOUCH_SNS_PORT_COUNT 1 |