Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
USB task entry point module

Modules

 USB software Events Management
 Macros to manage USB events detected under interrupt.
 
 Standard requests defines
 

Macros

#define g_usb_mode   USB_MODE_DEVICE
 
#define USB_HIGH_SPEED_SUPPORT   false
 
#define USB_MODE_DEVICE   0x01
 
#define USB_MODE_HOST   0x02
 
#define USB_MODE_UNDEFINED   0x00
 

Functions

U32 host_get_timeout (void)
 
void usb_task (void)
 Entry point of the USB mamnagement. More...
 
void usb_task_init (void)
 This function initializes the USB process. More...
 

Variables

volatile U16 g_usb_event
 Public: U16 g_usb_event usb_connected is used to store USB events detected upon USB general interrupt subroutine Its value is managed by the following macros (See usb_task.h file) Usb_send_event(x) Usb_ack_event(x) Is_usb_event(x) Usb_clear_all_event() More...
 

#define g_usb_mode   USB_MODE_DEVICE

Referenced by usb_general_interrupt(), and usb_task().

#define USB_HIGH_SPEED_SUPPORT   false
#define USB_MODE_DEVICE   0x01

Referenced by usb_general_interrupt(), and usb_task().

#define USB_MODE_HOST   0x02

Referenced by usb_general_interrupt(), and usb_task().

#define USB_MODE_UNDEFINED   0x00

Referenced by usb_task().

U32 host_get_timeout ( void  )
void usb_task ( void  )

Entry point of the USB mamnagement.

Depending on the mode supported (HOST/DEVICE/DUAL_ROLE) the function calls the corresponding USB management function

Entry point of the USB mamnagement.

Depending on the USB mode supported (HOST/DEVICE/DUAL_ROLE) the function calls the corresponding USB management function.

References Enable_global_interrupt, g_usb_mode, Is_usb_id_device, usb_device_task(), usb_device_task_init(), Usb_enable_id_interrupt, USB_MODE_DEVICE, USB_MODE_HOST, and USB_MODE_UNDEFINED.

Referenced by main(), and usb_task_init().

void usb_task_init ( void  )

This function initializes the USB process.

This function enables the USB controller and init the USB interrupts. The aim is to allow the USB connection detection in order to send the appropriate USB event to the operating mode manager. Depending on the mode supported (HOST/DEVICE/DUAL_ROLE) the function calls the corresponding USB mode initialization function

Depending on the mode supported (HOST/DEVICE/DUAL_ROLE) the function calls the corresponding USB mode initialization function

References usb_task().

Referenced by main().

volatile U16 g_usb_event

Public: U16 g_usb_event usb_connected is used to store USB events detected upon USB general interrupt subroutine Its value is managed by the following macros (See usb_task.h file) Usb_send_event(x) Usb_ack_event(x) Is_usb_event(x) Usb_clear_all_event()