Microchip® Advanced Software Framework

S_usb_in_ter_descriptor Struct Reference

Class-Specific Input Terminal Descriptor.

#include <usb_descriptors.h>

Data Fields

uint8_t bAssocTerminal
 
uint8_t bDescriptorSubType
 
uint8_t bDescriptorType
 
uint8_t bLenght
 
uint8_t bNrChannels
 
uint8_t bTerminalID
 
uint8_t iChannelNames
 
uint8_t iTerminal
 
uint16_t wChannelConfig
 
uint16_t wTerminalType
 

uint8_t S_usb_in_ter_descriptor::bAssocTerminal
uint8_t S_usb_in_ter_descriptor::bDescriptorSubType
uint8_t S_usb_in_ter_descriptor::bDescriptorType
uint8_t S_usb_in_ter_descriptor::bLenght
uint8_t S_usb_in_ter_descriptor::bNrChannels
uint8_t S_usb_in_ter_descriptor::bTerminalID
uint8_t S_usb_in_ter_descriptor::iChannelNames
uint8_t S_usb_in_ter_descriptor::iTerminal
uint16_t S_usb_in_ter_descriptor::wChannelConfig
uint16_t S_usb_in_ter_descriptor::wTerminalType