#include <stdio.h>
#include "conf_usb.h"
#include "conf_audio_player.h"
#include "audio_mixer.h"
#include "usb_drv.h"
#include "usb_stream_player.h"
#include "cycle_counter.h"
#include "gpio.h"
#include "debug.h"
Macros | |
#define | BROKEN_STREAM_TIMER 4000 |
Functions | |
void | dac_sample_sent_cb (void) |
This callback function is called when the DAC interrupt has sent the buffer 'n-1' and switches to buffer 'n'. More... | |
void | dac_underflow_cb (void) |
This callback function is called when the PWM DAC interrupt does not have any more audio samples (i.e. More... | |
void | player_init (void) |
void | player_shutdown (void) |
uint32_t | usb_stream_get_buffer_level () |
This function returns the number of full buffers. More... | |
uint16_t | usb_stream_get_counter () |
This function returns the internal audio counter. More... | |
uint16_t | usb_stream_get_stream_status () |
This function returns the audio status. More... | |
void | usb_stream_init (uint32_t sample_rate_hz, uint8_t num_channels, uint8_t bits_per_sample, bool swap_channels) |
This function initializes the USB Stream driver. More... | |
int | usb_stream_input (usb_stream_side_t side, uint8_t pipe_in, uint32_t *pFifoCount) |
This function takes the stream coming from the selected USB pipe and sends it to the DAC driver. More... | |
bool | usb_stream_new_sample_rate (uint32_t sample_rate) |
Sync the sample rate of the audio output stream with the USB stream. More... | |
int32_t | usb_stream_ppm_get (void) |
This function returns the PPM differences between the input audio stream frequency and the DAC output frequency. More... | |
void | usb_stream_resync (void) |
This function monitors the buffering level and set a timer for the resynchronization. More... | |
Variables | |
static t_cpu_time | broken_stream_timer |
uint32_t | buf_trace [] |
volatile uint16_t | usb_stream_cnt =0 |
usb_stream_context_t * | usb_stream_context = NULL |
t_cpu_time | usb_stream_monitor_timer |
static uint32_t | usb_stream_real_sample_freq =0 |
static bool | usb_stream_resync_b_acting =false |
static uint16_t | usb_stream_resync_last_room =0 |
static int16_t | usb_stream_resync_ppm =0 |
t_cpu_time | usb_stream_resync_timer |
#define BROKEN_STREAM_TIMER 4000 |
Referenced by usb_stream_init(), and usb_stream_input().
void dac_sample_sent_cb | ( | void | ) |
This callback function is called when the DAC interrupt has sent the buffer 'n-1' and switches to buffer 'n'.
The aim of this function is thus to prepare the buffer 'n+1'; so that there is always a pending buffer for the interrupt.
References audio_mixer_dacs_output_direct(), usb_stream_context_t::bits_per_sample, usb_stream_context_t::channel_count, usb_stream_context_t::status, usb_stream_context_t::synchronized, USB_STREAM_ERROR_NOT_SYNCHRONIZED, usb_stream_fifo_get(), usb_stream_fifo_get_used_room(), and usb_stream_fifo_pull().
void dac_underflow_cb | ( | void | ) |
This callback function is called when the PWM DAC interrupt does not have any more audio samples (i.e.
"famine").
References usb_stream_context_t::status, usb_stream_context_t::synchronized, and USB_STREAM_ERROR_NOT_SYNCHRONIZED.
void player_init | ( | void | ) |
Referenced by device_audio_task_init().
void player_shutdown | ( | void | ) |
References audio_mixer_dacs_flush_direct().
uint32_t usb_stream_get_buffer_level | ( | void | ) |
This function returns the number of full buffers.
References usb_stream_fifo_get_used_room().
uint16_t usb_stream_get_counter | ( | void | ) |
This function returns the internal audio counter.
References usb_stream_cnt.
uint16_t usb_stream_get_stream_status | ( | void | ) |
This function returns the audio status.
References usb_stream_context_t::status.
void usb_stream_init | ( | uint32_t | sample_rate_hz, |
uint8_t | num_channels, | ||
uint8_t | bits_per_sample, | ||
bool | swap_channels | ||
) |
This function initializes the USB Stream driver.
References usb_stream_context_t::audio_buffer_size, audio_mixer_dacs_setup_direct(), bits_per_sample, usb_stream_context_t::bits_per_sample, BROKEN_STREAM_TIMER, usb_stream_context_t::channel_count, cpu_ms_2_cy(), cpu_set_timeout(), cpu_stop_timeout(), FCPU_HZ, num_channels, usb_stream_context_t::rd_id, usb_stream_context_t::sample_rate, sample_rate_hz, usb_stream_context_t::synchronized, USB_STREAM_BUFFER_NUMBER, usb_stream_resync_b_acting, and usb_stream_context_t::wr_id.
Referenced by audio_speaker_set_sample_freq(), device_audio_task_init(), and usb_stream_new_sample_rate().
int usb_stream_input | ( | usb_stream_side_t | side, |
uint8_t | pipe_in, | ||
uint32_t * | pFifoCount | ||
) |
This function takes the stream coming from the selected USB pipe and sends it to the DAC driver.
Moreover, it ensures that both input and output stream keep synchronized by adding or deleting samples.
side | USB_STREAM_HOST for USB host, USB_STREAM_DEVICE for device. |
pipe_in | Number of the addressed pipe/endpoint |
pFifoCount | (return parameter) NULL or pointer to the number of used buffers at this time |
References abs, audio_mixer_dacs_output_direct(), usb_stream_context_t::bits_per_sample, BROKEN_STREAM_TIMER, usb_stream_context_t::channel_count, cpu_is_timeout(), cpu_is_timer_stopped(), cpu_ms_2_cy(), cpu_set_timeout(), cpu_stop_timeout(), cpu_us_2_cy(), FCPU_HZ, Host_byte_count, Host_reset_pipe_fifo_access, UnionPtr::s16ptr, UnionPtr::s32ptr, UnionPtr::s8ptr, usb_stream_context_t::sample_rate, usb_stream_context_t::status, swap16, swap32, usb_stream_context_t::synchronized, TIMER_USB_STREAM_MONITOR, Usb_byte_count, usb_read_ep_rxpacket(), Usb_reset_endpoint_fifo_access, USB_STREAM_BUFFER_NUMBER, usb_stream_cnt, USB_STREAM_DEVICE, USB_STREAM_ERROR_BROKEN_STREAM, USB_STREAM_ERROR_NO_DATA, USB_STREAM_ERROR_NONE, USB_STREAM_ERROR_NOT_SYNCHRONIZED, USB_STREAM_ERROR_OVERFLOW, usb_stream_fifo_get(), usb_stream_fifo_get_buffer(), usb_stream_fifo_get_used_room(), usb_stream_fifo_pull(), usb_stream_fifo_push(), USB_STREAM_HOST, USB_STREAM_REAL_BUFFER_SIZE, usb_stream_real_sample_freq, usb_stream_resync(), usb_stream_resync_b_acting, usb_stream_resync_last_room, usb_stream_resync_ppm, and usb_stream_context_t::wr_id.
Referenced by device_audio_task().
bool usb_stream_new_sample_rate | ( | uint32_t | sample_rate | ) |
Sync the sample rate of the audio output stream with the USB stream.
false | The new sample rate already matches the current settings. |
true | The output sample rate was changed. |
References audio_mixer_dacs_flush_direct(), and usb_stream_init().
int32_t usb_stream_ppm_get | ( | void | ) |
This function returns the PPM differences between the input audio stream frequency and the DAC output frequency.
Note that this information should only be considered as an indication, for debug or visual effect for example.
References usb_stream_resync_ppm.
Referenced by mmi_activity_display().
void usb_stream_resync | ( | void | ) |
This function monitors the buffering level and set a timer for the resynchronization.
This will ensures that no underflow/underflow will never occur by inserting/removing samples.
References abs, cpu_is_timeout(), cpu_ms_2_cy(), cpu_set_timeout(), FCPU_HZ, PPM_ADD, usb_stream_context_t::sample_rate, usb_stream_context_t::synchronized, TIMER_USB_STREAM_MONITOR, USB_STREAM_BUFFER_NUMBER, usb_stream_fifo_get_used_room(), usb_stream_real_sample_freq, usb_stream_resync_b_acting, usb_stream_resync_last_room, usb_stream_resync_ppm, and USB_STREAM_RESYNC_PPM_STEPS.
Referenced by device_audio_task(), and usb_stream_input().
|
static |
uint32_t buf_trace[] |
volatile uint16_t usb_stream_cnt =0 |
Referenced by usb_stream_get_counter(), and usb_stream_input().
usb_stream_context_t* usb_stream_context = NULL |
t_cpu_time usb_stream_monitor_timer |
|
static |
Referenced by usb_stream_input(), and usb_stream_resync().
Referenced by usb_stream_init(), usb_stream_input(), and usb_stream_resync().
|
static |
Referenced by usb_stream_input(), and usb_stream_resync().
|
static |
Referenced by usb_stream_input(), usb_stream_ppm_get(), and usb_stream_resync().
t_cpu_time usb_stream_resync_timer |