![]() | |
![]() ![]() | Defines to enable device or host USB operating modes supported by the application |
![]() ![]() | |
![]() ![]() ![]() | |
![]() ![]() | |
![]() ![]() ![]() | |
![]() | |
![]() | See Quick start guide for First-In-First-Out Buffer (FIFO) |
![]() | |
![]() | |
![]() | |
![]() ![]() | Macros to manage USB events detected under interrupt |
![]() ![]() | |
![]() | USBB low-level driver module |
![]() ![]() | Identifiers of USBB endpoints (USBB device operating mode) |
![]() ![]() | Identifiers of USBB pipes (USBB host operating mode) |
![]() ![]() | List of the standard types used in USBB |
![]() ![]() | These macros give access to IP properties |
![]() ![]() | These macros manage the USBB controller |
![]() ![]() | These macros manage the USBB Device controller |
![]() ![]() | These macros manage the common features of the endpoints |
![]() ![]() | These macros manage the common features of the endpoint DMA channels |
![]() ![]() | These macros manage the USBB Host controller |
![]() ![]() | These macros manage the common features of the pipes |
![]() ![]() | These macros manage the common features of the pipe DMA channels |
![]() | Compiler abstraction layer and code utilities for 32-bit AVR |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() | This collection of macros identify which series and families that the various Atmel parts belong to |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() ![]() | |
![]() | This is a driver for global enabling and disabling of interrupts |
![]() ![]() | |
![]() | The Power Manager (PM) controls the oscillators and PLLs, and generates the clocks and resets in the device |
![]() ![]() | |
![]() | This is a stub on the AVR UC3 Power Manager(PM) for the sleepmgr service |
![]() | FLASHC interfaces a flash block with the 32-bit internal HSB bus |
![]() | |
![]() | |
![]() ![]() | Defines for device state coding |
![]() | This driver adds functionality to print debug strings and data through a dedicated USART |
![]() | Driver for the USART (Universal Synchronous Asynchronous Receiver Transmitter) |
![]() | GPIO gives access to the MCU pins |
![]() | This is a software module to register interrupt handlers at any specified interrupt level to any interrupt line managed by the INTC module in AVR UC3 devices |
![]() | A 5-way joystick (left, right, up, down, press) interface using 5 GPIOs |
![]() | CPU Cycle Counter provides an interface to the COUNT and COMPARE registers |
![]() | The generic board support module includes board-specific definitions and function prototypes, such as the board initialization function |