Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
USB host enumeration functions module

Data Structures

struct  S_interface
 Interface. More...
 
struct  S_usb_setup_data
 USB Setup Data. More...
 

Macros

#define CONTROL_CRC16   0x10
 
#define CONTROL_DATA_PID   0x02
 
#define CONTROL_DATA_TOGGLE   0x01
 
#define CONTROL_GOOD   0x00
 
#define CONTROL_NO_DEVICE   0x40
 
#define CONTROL_PID   0x04
 
#define CONTROL_STALL   0x20
 
#define CONTROL_TIMEOUT   0x08
 
#define Get_altset_nb(s_interface)   (interface_supported[(s_interface)].altset_nb)
 Number of alternate settings associated with a supported interface. More...
 
#define Get_class(s_interface)   (interface_supported[(s_interface)].uclass)
 USB class associated with the supported interface. More...
 
#define Get_ep_nbr(s_interface, n_ep)   (Host_get_pipe_endpoint_number(Get_ep_pipe(s_interface, n_ep)))
 Endpoint number associated with the supported interface. More...
 
#define Get_ep_pipe(s_interface, n_ep)   (interface_supported[(s_interface)].ep_pipe[(n_ep)])
 Endpoint pipe associated with the supported interface. More...
 
#define Get_ep_type(s_interface, n_ep)   (Host_get_pipe_type(Get_ep_pipe(s_interface, n_ep)))
 Endpoint type associated with the supported interface. More...
 
#define Get_interface_number(s_interface)   (interface_supported[(s_interface)].interface_nb)
 Number of interfaces associated with a supported interface. More...
 
#define Get_maxpower()   (maxpower)
 Maximal power consumption ot the connected device (unit is 2 mA) More...
 
#define Get_nb_ep(s_interface)   (interface_supported[(s_interface)].nb_ep)
 Number of endpoints associated with a supported interface. More...
 
#define Get_nb_supported_interface()   (nb_interface_supported)
 Number of supported interfaces in the connected device. More...
 
#define Get_PID()   (device_PID)
 PID of the connected device. More...
 
#define Get_pipe_token(ep_addr)   ((Get_desc_ep_dir(ep_addr)) ? TOKEN_IN : TOKEN_OUT)
 Extract token information from endpoint address. More...
 
#define Get_protocol(s_interface)   (interface_supported[(s_interface)].protocol)
 USB protocol associated with the supported interface. More...
 
#define Get_subclass(s_interface)   (interface_supported[(s_interface)].subclass)
 USB subclass associated with the supported interface. More...
 
#define Get_VID()   (device_VID)
 VID of the connected device. More...
 
#define host_clear_endpoint_feature(ep)
 Send a "clear endpoint feature" request. More...
 
#define host_get_configuration()
 Send a "get configuration" request. More...
 
#define host_get_configuration_descriptor(cfg_ix)
 Send a "get device configuration descriptor" request The configuration descriptor received is stored in the data_stage array. More...
 
#define host_get_device_descriptor()
 Send a "get device descriptor" request The descriptor received is stored in the data_stage array. More...
 
#define host_get_device_descriptor_incomplete()
 Send an incomplete "get device descriptor" request The descriptor received is stored in the data_stage array. More...
 
#define host_ms_get_max_lun()
 Send the mass-storage specific request "get max LUN". More...
 
#define host_set_address(addr)
 Send a "set address" request. More...
 
#define host_set_configuration(cfg_nb)
 Send a "set configuration" request. More...
 
#define host_set_feature_remote_wakeup()
 Send a "set feature" "device remote wake-up". More...
 
#define host_set_interface(interface_nb, alt_setting)
 Send a "set interface" request to specify an alternate setting for an interface. More...
 
#define Is_device_self_powered()   (Tst_bits(bmattributes, SELF_POWERED_MASK))
 true if the connected device is self-powered More...
 
#define Is_device_supports_remote_wakeup()   (Tst_bits(bmattributes, REMOTE_WAKEUP_MASK))
 true if the connected device supports remote wake-up More...
 
#define Is_ep_in(s_interface, n_ep)   (Host_get_pipe_token(Get_ep_pipe(s_interface, n_ep)) == TOKEN_IN)
 true if the endpoint direction associated with the supported interface is IN More...
 
#define OFFSET_DESCRIPTOR_LENGTH   0
 Offsets common to all descriptor types. More...
 
#define OFFSET_FIELD_ALT   3
 
#define OFFSET_FIELD_BMATTRIBUTES   7
 
#define OFFSET_FIELD_CLASS   5
 
#define OFFSET_FIELD_CONFIGURATION_NB   5
 
#define OFFSET_FIELD_DESCRIPTOR_TYPE   1
 
#define OFFSET_FIELD_EP_ADDR   2
 Offsets in endpoint descriptors. More...
 
#define OFFSET_FIELD_EP_INTERVAL   6
 
#define OFFSET_FIELD_EP_SIZE   4
 
#define OFFSET_FIELD_EP_TYPE   3
 
#define OFFSET_FIELD_INTERFACE_NB   2
 Offsets in interface descriptors. More...
 
#define OFFSET_FIELD_MAXPACKETSIZE   7
 Offsets in device descriptors. More...
 
#define OFFSET_FIELD_MAXPOWER   8
 
#define OFFSET_FIELD_NB_CONFIGURATION   17
 
#define OFFSET_FIELD_NB_INTERFACE   4
 
#define OFFSET_FIELD_NB_OF_EP   4
 
#define OFFSET_FIELD_PID   10
 
#define OFFSET_FIELD_PROTOCOL   7
 
#define OFFSET_FIELD_SUB_CLASS   6
 
#define OFFSET_FIELD_TOTAL_LENGTH   2
 Offsets in configuration descriptors. More...
 
#define OFFSET_FIELD_VID   8
 
#define REMOTE_WAKEUP_BIT   5
 
#define REMOTE_WAKEUP_MASK   (1 << REMOTE_WAKEUP_BIT)
 
#define SELF_POWERED_BIT   6
 
#define SELF_POWERED_MASK   (1 << SELF_POWERED_BIT)
 

Functions

bool host_check_class (void)
 This function checks if the device class is supported. More...
 
bool host_check_VID_PID (void)
 This function checks if the VID and the PID are supported (if the VID & PID belong to the VID_PID table). More...
 
Status_t host_transfer_control (void *data_pointer)
 This function is the generic control pipe management function. More...
 

Variables

volatile U8 bmattributes
 bmAttributes byte of connected device More...
 
volatile U16 device_PID
 PID of connected device. More...
 
volatile U16 device_VID
 VID of connected device. More...
 
volatile S_interface interface_supported [MAX_INTERFACE_SUPPORTED]
 Supported interfaces. More...
 
volatile U8 maxpower
 maxpower byte of connected device (unit is 2 mA) More...
 
volatile U8 nb_interface_supported
 Number of interfaces the host is able to support in the connected device. More...
 

#define CONTROL_CRC16   0x10
#define CONTROL_DATA_PID   0x02
#define CONTROL_DATA_TOGGLE   0x01
#define CONTROL_GOOD   0x00
#define CONTROL_NO_DEVICE   0x40
#define CONTROL_PID   0x04
#define CONTROL_STALL   0x20

Referenced by host_transfer_control().

#define CONTROL_TIMEOUT   0x08

Referenced by host_transfer_control().

#define Get_altset_nb (   s_interface)    (interface_supported[(s_interface)].altset_nb)

Number of alternate settings associated with a supported interface.

Parameters
s_interfaceU8: The supported interface number
Returns
U8: Number of alternate settings
#define Get_class (   s_interface)    (interface_supported[(s_interface)].uclass)

USB class associated with the supported interface.

Parameters
s_interfaceU8: The supported interface number
Returns
U8: Class

Referenced by host_cdc_task().

#define Get_ep_nbr (   s_interface,
  n_ep 
)    (Host_get_pipe_endpoint_number(Get_ep_pipe(s_interface, n_ep)))

Endpoint number associated with the supported interface.

Parameters
s_interfaceU8: The supported interface number
n_epU8: The endpoint number in this interface
Returns
U8: Endpoint number
#define Get_ep_pipe (   s_interface,
  n_ep 
)    (interface_supported[(s_interface)].ep_pipe[(n_ep)])

Endpoint pipe associated with the supported interface.

Parameters
s_interfaceU8: The supported interface number
n_epU8: The endpoint number in this interface
Returns
U8: Endpoint pipe

Referenced by host_cdc_task().

#define Get_ep_type (   s_interface,
  n_ep 
)    (Host_get_pipe_type(Get_ep_pipe(s_interface, n_ep)))

Endpoint type associated with the supported interface.

Parameters
s_interfaceU8: The supported interface number
n_epU8: The endpoint number in this interface
Returns
U8: Endpoint type
#define Get_interface_number (   s_interface)    (interface_supported[(s_interface)].interface_nb)

Number of interfaces associated with a supported interface.

Parameters
s_interfaceU8: The supported interface number
Returns
U8: Number of interfaces
#define Get_maxpower ( )    (maxpower)

Maximal power consumption ot the connected device (unit is 2 mA)

Returns
U8: Maximal power
#define Get_nb_ep (   s_interface)    (interface_supported[(s_interface)].nb_ep)

Number of endpoints associated with a supported interface.

Parameters
s_interfaceU8: The supported interface number
Returns
U8: Number of endpoints
#define Get_nb_supported_interface ( )    (nb_interface_supported)

Number of supported interfaces in the connected device.

Returns
U8: Number of supported interfaces

Referenced by host_cdc_task().

#define Get_PID ( )    (device_PID)

PID of the connected device.

Returns
U16: PID
#define Get_pipe_token (   ep_addr)    ((Get_desc_ep_dir(ep_addr)) ? TOKEN_IN : TOKEN_OUT)

Extract token information from endpoint address.

Parameters
ep_addrU8: Endpoint address
Returns
TOKEN_IN/TOKEN_OUT: Pipe token

Referenced by host_check_class().

#define Get_protocol (   s_interface)    (interface_supported[(s_interface)].protocol)

USB protocol associated with the supported interface.

Parameters
s_interfaceU8: The supported interface number
Returns
U8: protocol

Referenced by host_cdc_task().

#define Get_subclass (   s_interface)    (interface_supported[(s_interface)].subclass)

USB subclass associated with the supported interface.

Parameters
s_interfaceU8: The supported interface number
Returns
U8: Subclass
#define Get_VID ( )    (device_VID)

VID of the connected device.

Returns
U16: VID
#define host_clear_endpoint_feature (   ep)
Value:
(\
)
U8 bmRequestType
Characteristics of the request.
Definition: usb_host_enum.h:73
U8 bRequest
Specific request.
Definition: usb_host_enum.h:74
U16 wValue
Field that varies according to request.
Definition: usb_host_enum.h:75
volatile S_usb_setup_data usb_request
For control requests management over control pipe.
Definition: usb_host_task.c:94
#define FEATURE_ENDPOINT_HALT
Definition: usb_task.h:134
Status_t host_transfer_control(void *data_pointer)
This function is the generic control pipe management function.
Definition: usb_host_enum.c:309
#define CLEAR_FEATURE
Definition: usb_task.h:101
U16 wLength
Number of bytes to transfer if Data.
Definition: usb_host_enum.h:77
bool incomplete_read
true: only one read
Definition: usb_host_enum.h:78
U8 data_stage[SIZEOF_DATA_STAGE]
Public: U8 data_stage[SIZEOF_DATA_STAGE] Internal RAM buffer for USB data stage content This buffer i...
Definition: usb_host_task.c:104
U16 wIndex
Field that varies according to request.
Definition: usb_host_enum.h:76

Send a "clear endpoint feature" request.

Parameters
epU8: Target endpoint
Returns
Status
#define host_get_configuration ( )
Value:
(\
)
U8 bmRequestType
Characteristics of the request.
Definition: usb_host_enum.h:73
U8 bRequest
Specific request.
Definition: usb_host_enum.h:74
#define GET_CONFIGURATION
Definition: usb_task.h:107
U16 wValue
Field that varies according to request.
Definition: usb_host_enum.h:75
volatile S_usb_setup_data usb_request
For control requests management over control pipe.
Definition: usb_host_task.c:94
Status_t host_transfer_control(void *data_pointer)
This function is the generic control pipe management function.
Definition: usb_host_enum.c:309
U16 wLength
Number of bytes to transfer if Data.
Definition: usb_host_enum.h:77
bool incomplete_read
true: only one read
Definition: usb_host_enum.h:78
U8 data_stage[SIZEOF_DATA_STAGE]
Public: U8 data_stage[SIZEOF_DATA_STAGE] Internal RAM buffer for USB data stage content This buffer i...
Definition: usb_host_task.c:104
U16 wIndex
Field that varies according to request.
Definition: usb_host_enum.h:76

Send a "get configuration" request.

Returns
Status
#define host_get_configuration_descriptor (   cfg_ix)
Value:
(\
)
#define GET_DESCRIPTOR
Definition: usb_task.h:105
U8 bmRequestType
Characteristics of the request.
Definition: usb_host_enum.h:73
U8 bRequest
Specific request.
Definition: usb_host_enum.h:74
U16 wValue
Field that varies according to request.
Definition: usb_host_enum.h:75
volatile S_usb_setup_data usb_request
For control requests management over control pipe.
Definition: usb_host_task.c:94
#define CONFIGURATION_DESCRIPTOR
Definition: usb_task.h:125
Status_t host_transfer_control(void *data_pointer)
This function is the generic control pipe management function.
Definition: usb_host_enum.c:309
#define SIZEOF_DATA_STAGE
The size of RAM buffer reserved for descriptor handling.
Definition: conf_usb.h:106
U16 wLength
Number of bytes to transfer if Data.
Definition: usb_host_enum.h:77
bool incomplete_read
true: only one read
Definition: usb_host_enum.h:78
U8 data_stage[SIZEOF_DATA_STAGE]
Public: U8 data_stage[SIZEOF_DATA_STAGE] Internal RAM buffer for USB data stage content This buffer i...
Definition: usb_host_task.c:104
U16 wIndex
Field that varies according to request.
Definition: usb_host_enum.h:76

Send a "get device configuration descriptor" request The configuration descriptor received is stored in the data_stage array.

Parameters
cfg_ixU8: Index of the configuration descriptor to get
Returns
Status

Referenced by usb_host_task().

#define host_get_device_descriptor ( )
Value:
(\
)
#define GET_DESCRIPTOR
Definition: usb_task.h:105
U8 bmRequestType
Characteristics of the request.
Definition: usb_host_enum.h:73
U8 bRequest
Specific request.
Definition: usb_host_enum.h:74
U16 wValue
Field that varies according to request.
Definition: usb_host_enum.h:75
volatile S_usb_setup_data usb_request
For control requests management over control pipe.
Definition: usb_host_task.c:94
Status_t host_transfer_control(void *data_pointer)
This function is the generic control pipe management function.
Definition: usb_host_enum.c:309
#define DEVICE_DESCRIPTOR
Definition: usb_task.h:124
U16 wLength
Number of bytes to transfer if Data.
Definition: usb_host_enum.h:77
bool incomplete_read
true: only one read
Definition: usb_host_enum.h:78
U8 data_stage[SIZEOF_DATA_STAGE]
Public: U8 data_stage[SIZEOF_DATA_STAGE] Internal RAM buffer for USB data stage content This buffer i...
Definition: usb_host_task.c:104
U16 wIndex
Field that varies according to request.
Definition: usb_host_enum.h:76

Send a "get device descriptor" request The descriptor received is stored in the data_stage array.

Returns
Status

Referenced by usb_host_task().

#define host_get_device_descriptor_incomplete ( )
Value:
(\
)
#define GET_DESCRIPTOR
Definition: usb_task.h:105
U8 bmRequestType
Characteristics of the request.
Definition: usb_host_enum.h:73
U8 bRequest
Specific request.
Definition: usb_host_enum.h:74
U16 wValue
Field that varies according to request.
Definition: usb_host_enum.h:75
volatile S_usb_setup_data usb_request
For control requests management over control pipe.
Definition: usb_host_task.c:94
Status_t host_transfer_control(void *data_pointer)
This function is the generic control pipe management function.
Definition: usb_host_enum.c:309
#define DEVICE_DESCRIPTOR
Definition: usb_task.h:124
U16 wLength
Number of bytes to transfer if Data.
Definition: usb_host_enum.h:77
bool incomplete_read
true: only one read
Definition: usb_host_enum.h:78
U8 data_stage[SIZEOF_DATA_STAGE]
Public: U8 data_stage[SIZEOF_DATA_STAGE] Internal RAM buffer for USB data stage content This buffer i...
Definition: usb_host_task.c:104
U16 wIndex
Field that varies according to request.
Definition: usb_host_enum.h:76

Send an incomplete "get device descriptor" request The descriptor received is stored in the data_stage array.

The received descriptors are limited to the length of the control pipe.

Returns
Status

Referenced by usb_host_task().

#define host_ms_get_max_lun ( )
Value:
(\
usb_request.bRequest = MS_GET_MAX_LUN,\
)
U8 bmRequestType
Characteristics of the request.
Definition: usb_host_enum.h:73
U8 bRequest
Specific request.
Definition: usb_host_enum.h:74
U16 wValue
Field that varies according to request.
Definition: usb_host_enum.h:75
volatile S_usb_setup_data usb_request
For control requests management over control pipe.
Definition: usb_host_task.c:94
Status_t host_transfer_control(void *data_pointer)
This function is the generic control pipe management function.
Definition: usb_host_enum.c:309
U16 wLength
Number of bytes to transfer if Data.
Definition: usb_host_enum.h:77
bool incomplete_read
true: only one read
Definition: usb_host_enum.h:78
U8 data_stage[SIZEOF_DATA_STAGE]
Public: U8 data_stage[SIZEOF_DATA_STAGE] Internal RAM buffer for USB data stage content This buffer i...
Definition: usb_host_task.c:104
U16 wIndex
Field that varies according to request.
Definition: usb_host_enum.h:76

Send the mass-storage specific request "get max LUN".

Returns
Status
#define host_set_address (   addr)
Value:
(\
usb_request.wValue = (addr),\
)
U8 bmRequestType
Characteristics of the request.
Definition: usb_host_enum.h:73
U8 bRequest
Specific request.
Definition: usb_host_enum.h:74
U16 wValue
Field that varies according to request.
Definition: usb_host_enum.h:75
volatile S_usb_setup_data usb_request
For control requests management over control pipe.
Definition: usb_host_task.c:94
Status_t host_transfer_control(void *data_pointer)
This function is the generic control pipe management function.
Definition: usb_host_enum.c:309
#define SET_ADDRESS
Definition: usb_task.h:104
U16 wLength
Number of bytes to transfer if Data.
Definition: usb_host_enum.h:77
bool incomplete_read
true: only one read
Definition: usb_host_enum.h:78
U8 data_stage[SIZEOF_DATA_STAGE]
Public: U8 data_stage[SIZEOF_DATA_STAGE] Internal RAM buffer for USB data stage content This buffer i...
Definition: usb_host_task.c:104
U16 wIndex
Field that varies according to request.
Definition: usb_host_enum.h:76

Send a "set address" request.

Parameters
addrU8: Address assigned to the device
Returns
Status

Referenced by usb_host_task().

#define host_set_configuration (   cfg_nb)
Value:
(\
usb_request.wValue = (cfg_nb),\
)
U8 bmRequestType
Characteristics of the request.
Definition: usb_host_enum.h:73
U8 bRequest
Specific request.
Definition: usb_host_enum.h:74
U16 wValue
Field that varies according to request.
Definition: usb_host_enum.h:75
volatile S_usb_setup_data usb_request
For control requests management over control pipe.
Definition: usb_host_task.c:94
Status_t host_transfer_control(void *data_pointer)
This function is the generic control pipe management function.
Definition: usb_host_enum.c:309
#define SET_CONFIGURATION
Definition: usb_task.h:108
U16 wLength
Number of bytes to transfer if Data.
Definition: usb_host_enum.h:77
bool incomplete_read
true: only one read
Definition: usb_host_enum.h:78
U8 data_stage[SIZEOF_DATA_STAGE]
Public: U8 data_stage[SIZEOF_DATA_STAGE] Internal RAM buffer for USB data stage content This buffer i...
Definition: usb_host_task.c:104
U16 wIndex
Field that varies according to request.
Definition: usb_host_enum.h:76

Send a "set configuration" request.

Parameters
cfg_nbU8: Configuration to activate
Returns
Status

Referenced by usb_host_task().

#define host_set_feature_remote_wakeup ( )
Value:
(\
)
U8 bmRequestType
Characteristics of the request.
Definition: usb_host_enum.h:73
#define SET_FEATURE
Definition: usb_task.h:103
U8 bRequest
Specific request.
Definition: usb_host_enum.h:74
U16 wValue
Field that varies according to request.
Definition: usb_host_enum.h:75
volatile S_usb_setup_data usb_request
For control requests management over control pipe.
Definition: usb_host_task.c:94
Status_t host_transfer_control(void *data_pointer)
This function is the generic control pipe management function.
Definition: usb_host_enum.c:309
U16 wLength
Number of bytes to transfer if Data.
Definition: usb_host_enum.h:77
bool incomplete_read
true: only one read
Definition: usb_host_enum.h:78
U8 data_stage[SIZEOF_DATA_STAGE]
Public: U8 data_stage[SIZEOF_DATA_STAGE] Internal RAM buffer for USB data stage content This buffer i...
Definition: usb_host_task.c:104
U16 wIndex
Field that varies according to request.
Definition: usb_host_enum.h:76

Send a "set feature" "device remote wake-up".

Returns
Status

Referenced by usb_host_task().

#define host_set_interface (   interface_nb,
  alt_setting 
)
Value:
(\
usb_request.wValue = (alt_setting),\
usb_request.wIndex = (interface_nb),\
)
U8 bmRequestType
Characteristics of the request.
Definition: usb_host_enum.h:73
U8 bRequest
Specific request.
Definition: usb_host_enum.h:74
#define SET_INTERFACE
Definition: usb_task.h:110
U16 wValue
Field that varies according to request.
Definition: usb_host_enum.h:75
volatile S_usb_setup_data usb_request
For control requests management over control pipe.
Definition: usb_host_task.c:94
Status_t host_transfer_control(void *data_pointer)
This function is the generic control pipe management function.
Definition: usb_host_enum.c:309
U16 wLength
Number of bytes to transfer if Data.
Definition: usb_host_enum.h:77
bool incomplete_read
true: only one read
Definition: usb_host_enum.h:78
U8 data_stage[SIZEOF_DATA_STAGE]
Public: U8 data_stage[SIZEOF_DATA_STAGE] Internal RAM buffer for USB data stage content This buffer i...
Definition: usb_host_task.c:104
U16 wIndex
Field that varies according to request.
Definition: usb_host_enum.h:76

Send a "set interface" request to specify an alternate setting for an interface.

Parameters
interface_nbU8: Interface
alt_settingU8: Alternate setting
Returns
Status
#define Is_device_self_powered ( )    (Tst_bits(bmattributes, SELF_POWERED_MASK))

true if the connected device is self-powered

Returns
bool: Self-powered?
#define Is_device_supports_remote_wakeup ( )    (Tst_bits(bmattributes, REMOTE_WAKEUP_MASK))

true if the connected device supports remote wake-up

Returns
bool: Remote wake-up supported?

Referenced by usb_host_task().

#define Is_ep_in (   s_interface,
  n_ep 
)    (Host_get_pipe_token(Get_ep_pipe(s_interface, n_ep)) == TOKEN_IN)

true if the endpoint direction associated with the supported interface is IN

Parameters
s_interfaceU8: The supported interface number
n_epU8: The endpoint number in this interface
Returns
bool: Endpoint direction IN?

Referenced by host_cdc_task().

#define OFFSET_DESCRIPTOR_LENGTH   0

Offsets common to all descriptor types.

Referenced by host_check_class().

#define OFFSET_FIELD_ALT   3

Referenced by host_check_class().

#define OFFSET_FIELD_BMATTRIBUTES   7

Referenced by host_check_class().

#define OFFSET_FIELD_CLASS   5

Referenced by host_check_class().

#define OFFSET_FIELD_CONFIGURATION_NB   5
#define OFFSET_FIELD_DESCRIPTOR_TYPE   1

Referenced by host_check_class().

#define OFFSET_FIELD_EP_ADDR   2

Offsets in endpoint descriptors.

Referenced by host_check_class().

#define OFFSET_FIELD_EP_INTERVAL   6

Referenced by host_check_class().

#define OFFSET_FIELD_EP_SIZE   4

Referenced by host_check_class().

#define OFFSET_FIELD_EP_TYPE   3

Referenced by host_check_class().

#define OFFSET_FIELD_INTERFACE_NB   2

Offsets in interface descriptors.

Referenced by host_check_class().

#define OFFSET_FIELD_MAXPACKETSIZE   7

Offsets in device descriptors.

Referenced by usb_host_task().

#define OFFSET_FIELD_MAXPOWER   8

Referenced by host_check_class().

#define OFFSET_FIELD_NB_CONFIGURATION   17
#define OFFSET_FIELD_NB_INTERFACE   4
#define OFFSET_FIELD_NB_OF_EP   4

Referenced by host_check_class().

#define OFFSET_FIELD_PID   10

Referenced by host_check_VID_PID().

#define OFFSET_FIELD_PROTOCOL   7

Referenced by host_check_class().

#define OFFSET_FIELD_SUB_CLASS   6

Referenced by host_check_class().

#define OFFSET_FIELD_TOTAL_LENGTH   2

Offsets in configuration descriptors.

Referenced by host_check_class().

#define OFFSET_FIELD_VID   8

Referenced by host_check_VID_PID().

#define REMOTE_WAKEUP_BIT   5
#define REMOTE_WAKEUP_MASK   (1 << REMOTE_WAKEUP_BIT)
#define SELF_POWERED_BIT   6
#define SELF_POWERED_MASK   (1 << SELF_POWERED_BIT)

bool host_check_class ( void  )

This function checks if the device class is supported.

The function looks in all interfaces declared in the received descriptors if one of them matches an entry of the CLASS/SUB_CLASS/PROTOCOL table. If HOST_AUTO_CFG_ENDPOINT is enabled, a pipe is configured for each endpoint of supported interfaces.

Returns
bool: Status

References S_interface::altset_nb, bmattributes, CONFIGURATION_DESCRIPTOR, data_stage, Disable_global_interrupt, DOUBLE_BANK, Enable_global_interrupt, ENDPOINT_DESCRIPTOR, S_interface::ep_pipe, Get_desc_ep_nbr, Get_pipe_token, Host_clear_configured, Host_configure_pipe, Host_configure_pipe_int_req_freq, Host_disable_pipe, Host_enable_ping, Host_enable_pipe, Host_get_pipe_token, Host_get_pipe_type, Host_set_configured, Host_unallocate_memory, Host_user_check_class_action, INTERFACE_DESCRIPTOR, S_interface::interface_nb, Is_host_pipe_enabled, Is_usb_full_speed_mode, MAX_EP_PER_INTERFACE, MAX_INTERFACE_SUPPORTED, MAX_PEP_NB, maxpower, min, S_interface::nb_ep, nb_interface_supported, OFFSET_DESCRIPTOR_LENGTH, OFFSET_FIELD_ALT, OFFSET_FIELD_BMATTRIBUTES, OFFSET_FIELD_CLASS, OFFSET_FIELD_DESCRIPTOR_TYPE, OFFSET_FIELD_EP_ADDR, OFFSET_FIELD_EP_INTERVAL, OFFSET_FIELD_EP_SIZE, OFFSET_FIELD_EP_TYPE, OFFSET_FIELD_INTERFACE_NB, OFFSET_FIELD_MAXPOWER, OFFSET_FIELD_NB_OF_EP, OFFSET_FIELD_PROTOCOL, OFFSET_FIELD_SUB_CLASS, OFFSET_FIELD_TOTAL_LENGTH, P_1, S_interface::protocol, REG_CLASS_CNT, registered_class, SINGLE_BANK, SIZEOF_DATA_STAGE, S_interface::subclass, TOKEN_OUT, TRANSFER_TYPE_MASK, TYPE_BULK, TYPE_INTERRUPT, TYPE_ISOCHRONOUS, S_interface::uclass, and usb_format_usb_to_mcu_data.

Referenced by usb_host_task().

bool host_check_VID_PID ( void  )

This function checks if the VID and the PID are supported (if the VID & PID belong to the VID_PID table).

Returns
bool: Status

References data_stage, device_PID, device_VID, OFFSET_FIELD_PID, OFFSET_FIELD_VID, REG_VID_PID_CNT, registered_VID_PID, and usb_format_usb_to_mcu_data.

Referenced by usb_host_task().

Status_t host_transfer_control ( void *  data_pointer)

This function is the generic control pipe management function.

This function is used to send and receive control requests over control pipe.

Todo:
Fix all time-out errors and disconnections in active wait loop.
Parameters
data_pointervoid *: Pointer to data to transfer
Returns
Status_t: Status
Note
This function uses the usb_request global structure. Hence, this structure should be filled before calling this function.

References S_usb_setup_data::bmRequestType, S_usb_setup_data::bRequest, CONTROL_GOOD, CONTROL_STALL, CONTROL_TIMEOUT, Disable_global_interrupt, Enable_global_interrupt, EVT_HOST_SOF, Host_ack_all_errors, Host_ack_control_in_received, Host_ack_control_in_received_free, Host_ack_control_out_ready, Host_ack_control_out_ready_send, Host_ack_setup_ready, Host_ack_sof, Host_ack_stall, Host_byte_count, Host_configure_pipe_token, Host_disable_continuous_in_mode, Host_disable_sof_interrupt, Host_enable_sof_interrupt, Host_error_status, Host_free_control_in, Host_freeze_pipe, Host_get_pipe_size, host_get_timeout(), host_read_p_rxpacket(), Host_reset_pipe, Host_reset_pipe_fifo_access, Host_send_control_out, Host_send_setup, Host_unfreeze_pipe, host_write_p_txpacket(), Host_write_pipe_data, S_usb_setup_data::incomplete_read, Is_global_interrupt_enabled, Is_host_control_in_received, Is_host_control_out_ready, Is_host_emergency_exit, Is_host_pipe_error, Is_host_setup_ready, Is_host_sof_interrupt_enabled, Is_host_stall, Is_usb_event, Is_usb_low_speed_mode, P_CONTROL, private_sof_counter, TOKEN_IN, TOKEN_OUT, TOKEN_SETUP, Usb_ack_event, usb_format_mcu_to_usb_data, usb_request, S_usb_setup_data::wIndex, S_usb_setup_data::wLength, and S_usb_setup_data::wValue.

Referenced by host_cdc_get_encapsulated_response(), host_cdc_get_line_coding(), host_cdc_send_encapsulated_command(), and host_cdc_set_line_coding().

volatile U8 bmattributes

bmAttributes byte of connected device

Referenced by host_check_class().

volatile U16 device_PID

PID of connected device.

Referenced by host_check_VID_PID().

volatile U16 device_VID

VID of connected device.

Referenced by host_check_VID_PID().

volatile S_interface interface_supported[MAX_INTERFACE_SUPPORTED]

Supported interfaces.

volatile U8 maxpower

maxpower byte of connected device (unit is 2 mA)

Referenced by host_check_class().

volatile U8 nb_interface_supported

Number of interfaces the host is able to support in the connected device.

Referenced by host_check_class(), and usb_host_task().