Driver for the USART (Universal Synchronous Asynchronous Receiver Transmitter).
The driver supports the following modes: RS232, RS485, SPI, LIN and ISO7816.
Data Structures | |
struct | usart_iso7816_options_t |
Input parameters when initializing ISO7816 mode. More... | |
struct | usart_options_t |
Input parameters when initializing RS232 and similar modes. More... | |
Macros | |
#define | USART_DEFAULT_TIMEOUT 10000 |
Default time-out value (number of attempts). More... | |
Return Values | |
#define | USART_SUCCESS 0 |
Successful completion. More... | |
#define | USART_FAILURE -1 |
Failure because of some unspecified reason. More... | |
#define | USART_INVALID_INPUT 1 |
Input value out of range. More... | |
#define | USART_INVALID_ARGUMENT -1 |
Argument value out of range. More... | |
#define | USART_TX_BUSY 2 |
Transmitter was busy. More... | |
#define | USART_RX_EMPTY 3 |
Nothing was received. More... | |
#define | USART_RX_ERROR 4 |
Transmission error occurred. More... | |
#define | USART_MODE_FAULT 5 |
USART not in the appropriate mode. More... | |
Parity Settings | |
#define | USART_EVEN_PARITY AVR32_USART_MR_PAR_EVEN |
Use even parity on character transmission. More... | |
#define | USART_ODD_PARITY AVR32_USART_MR_PAR_ODD |
Use odd parity on character transmission. More... | |
#define | USART_SPACE_PARITY AVR32_USART_MR_PAR_SPACE |
Use a space as parity bit. More... | |
#define | USART_MARK_PARITY AVR32_USART_MR_PAR_MARK |
Use a mark as parity bit. More... | |
#define | USART_NO_PARITY AVR32_USART_MR_PAR_NONE |
Don't use a parity bit. More... | |
#define | USART_MULTIDROP_PARITY AVR32_USART_MR_PAR_MULTI |
Parity bit is used to flag address characters. More... | |
Stop Bits Settings | |
#define | USART_1_STOPBIT AVR32_USART_MR_NBSTOP_1 |
Use 1 stop bit. More... | |
#define | USART_1_5_STOPBITS AVR32_USART_MR_NBSTOP_1_5 |
Use 1.5 stop bits. More... | |
#define | USART_2_STOPBITS AVR32_USART_MR_NBSTOP_2 |
Use 2 stop bits (for more, just give the number of bits). More... | |
Channel Modes | |
#define | USART_NORMAL_CHMODE AVR32_USART_MR_CHMODE_NORMAL |
Normal communication. More... | |
#define | USART_AUTO_ECHO AVR32_USART_MR_CHMODE_ECHO |
Echo data. More... | |
#define | USART_LOCAL_LOOPBACK AVR32_USART_MR_CHMODE_LOCAL_LOOP |
Local loopback. More... | |
#define | USART_REMOTE_LOOPBACK AVR32_USART_MR_CHMODE_REMOTE_LOOP |
Remote loopback. More... | |
Initialization Functions | |
void | usart_reset (volatile avr32_usart_t *usart) |
Resets the USART and disables TX and RX. More... | |
int | usart_init_rs232 (volatile avr32_usart_t *usart, const usart_options_t *opt, long pba_hz) |
Sets up the USART to use the standard RS232 protocol. More... | |
int | usart_init_rs232_tx_only (volatile avr32_usart_t *usart, const usart_options_t *opt, long pba_hz) |
Sets up the USART to use the standard RS232 protocol in TX-only mode. More... | |
int | usart_init_hw_handshaking (volatile avr32_usart_t *usart, const usart_options_t *opt, long pba_hz) |
Sets up the USART to use hardware handshaking. More... | |
int | usart_init_modem (volatile avr32_usart_t *usart, const usart_options_t *opt, long pba_hz) |
Sets up the USART to use the modem protocol, activating dedicated inputs/outputs. More... | |
int | usart_init_sync_master (volatile avr32_usart_t *usart, const usart_options_t *opt, long pba_hz) |
Sets up the USART to use a synchronous RS232-like protocol in master mode. More... | |
int | usart_init_sync_slave (volatile avr32_usart_t *usart, const usart_options_t *opt, long pba_hz) |
Sets up the USART to use a synchronous RS232-like protocol in slave mode. More... | |
int | usart_init_rs485 (volatile avr32_usart_t *usart, const usart_options_t *opt, long pba_hz) |
Sets up the USART to use the RS485 protocol. More... | |
int | usart_init_IrDA (volatile avr32_usart_t *usart, const usart_options_t *opt, long pba_hz, unsigned char irda_filter) |
Sets up the USART to use the IrDA protocol. More... | |
int | usart_init_iso7816 (volatile avr32_usart_t *usart, const usart_iso7816_options_t *opt, int t, long pba_hz) |
Sets up the USART to use the ISO7816 T=0 or T=1 smartcard protocols. More... | |
Read and Reset Error Status Bits | |
static __always_inline void | usart_reset_status (volatile avr32_usart_t *usart) |
Resets the error status. More... | |
static __always_inline int | usart_parity_error (volatile avr32_usart_t *usart) |
Checks if a parity error has occurred since last status reset. More... | |
static __always_inline int | usart_framing_error (volatile avr32_usart_t *usart) |
Checks if a framing error has occurred since last status reset. More... | |
static __always_inline int | usart_overrun_error (volatile avr32_usart_t *usart) |
Checks if an overrun error has occurred since last status reset. More... | |
ISO7816 Control Functions | |
static __always_inline void | usart_iso7816_enable_receiver (volatile avr32_usart_t *usart) |
Enables the ISO7816 receiver. More... | |
static __always_inline void | usart_iso7816_enable_transmitter (volatile avr32_usart_t *usart) |
Enables the ISO7816 transmitter. More... | |
Transmit/Receive Functions | |
int | usart_send_address (volatile avr32_usart_t *usart, int address) |
Addresses a receiver. More... | |
static __always_inline int | usart_tx_ready (volatile avr32_usart_t *usart) |
Tests if the USART is ready to transmit a character. More... | |
int | usart_write_char (volatile avr32_usart_t *usart, int c) |
Writes the given character to the TX buffer if the transmitter is ready. More... | |
static __always_inline void | usart_bw_write_char (volatile avr32_usart_t *usart, int c) |
An active wait writing a character to the USART. More... | |
int | usart_putchar (volatile avr32_usart_t *usart, int c) |
Sends a character with the USART. More... | |
static __always_inline int | usart_tx_empty (volatile avr32_usart_t *usart) |
Tests if all requested USART transmissions are over. More... | |
static __always_inline int | usart_test_hit (volatile avr32_usart_t *usart) |
Tests if the USART contains a received character. More... | |
int | usart_read_char (volatile avr32_usart_t *usart, int *c) |
Checks the RX buffer for a received character, and stores it at the given memory location. More... | |
int | usart_getchar (volatile avr32_usart_t *usart) |
Waits until a character is received, and returns it. More... | |
void | usart_write_line (volatile avr32_usart_t *usart, const char *string) |
Writes one character string to the USART. More... | |
int | usart_get_echo_line (volatile avr32_usart_t *usart) |
Gets and echoes characters until end of line (detected by a CR character). More... | |
#define USART_1_5_STOPBITS AVR32_USART_MR_NBSTOP_1_5 |
Use 1.5 stop bits.
Referenced by cdc_set_line_coding().
#define USART_1_STOPBIT AVR32_USART_MR_NBSTOP_1 |
Use 1 stop bit.
Referenced by cdc_set_line_coding(), and init_dbg_rs232_ex().
#define USART_2_STOPBITS AVR32_USART_MR_NBSTOP_2 |
Use 2 stop bits (for more, just give the number of bits).
Referenced by cdc_set_line_coding(), usart_init_rs232(), usart_init_rs232_tx_only(), usart_init_sync_master(), and usart_init_sync_slave().
#define USART_AUTO_ECHO AVR32_USART_MR_CHMODE_ECHO |
Echo data.
#define USART_DEFAULT_TIMEOUT 10000 |
Default time-out value (number of attempts).
Referenced by usart_putchar().
#define USART_EVEN_PARITY AVR32_USART_MR_PAR_EVEN |
Use even parity on character transmission.
Referenced by cdc_set_line_coding().
#define USART_FAILURE -1 |
Failure because of some unspecified reason.
Referenced by usart_get_echo_line(), usart_getchar(), and usart_putchar().
#define USART_INVALID_ARGUMENT -1 |
Argument value out of range.
#define USART_INVALID_INPUT 1 |
Input value out of range.
Referenced by usart_init_hw_handshaking(), usart_init_IrDA(), usart_init_iso7816(), usart_init_modem(), usart_init_rs232(), usart_init_rs232_tx_only(), usart_init_rs485(), usart_init_sync_master(), usart_init_sync_slave(), usart_set_async_baudrate(), usart_set_iso7816_clock(), and usart_set_sync_master_baudrate().
#define USART_LOCAL_LOOPBACK AVR32_USART_MR_CHMODE_LOCAL_LOOP |
Local loopback.
#define USART_MARK_PARITY AVR32_USART_MR_PAR_MARK |
Use a mark as parity bit.
Referenced by cdc_set_line_coding().
#define USART_MODE_FAULT 5 |
USART not in the appropriate mode.
Referenced by usart_send_address().
#define USART_MULTIDROP_PARITY AVR32_USART_MR_PAR_MULTI |
Parity bit is used to flag address characters.
#define USART_NO_PARITY AVR32_USART_MR_PAR_NONE |
Don't use a parity bit.
Referenced by cdc_set_line_coding(), and init_dbg_rs232_ex().
#define USART_NORMAL_CHMODE AVR32_USART_MR_CHMODE_NORMAL |
Normal communication.
Referenced by cdc_set_line_coding(), and init_dbg_rs232_ex().
#define USART_ODD_PARITY AVR32_USART_MR_PAR_ODD |
Use odd parity on character transmission.
Referenced by cdc_set_line_coding().
#define USART_REMOTE_LOOPBACK AVR32_USART_MR_CHMODE_REMOTE_LOOP |
Remote loopback.
#define USART_RX_EMPTY 3 |
Nothing was received.
Referenced by usart_getchar(), and usart_read_char().
#define USART_RX_ERROR 4 |
Transmission error occurred.
Referenced by usart_getchar(), and usart_read_char().
#define USART_SPACE_PARITY AVR32_USART_MR_PAR_SPACE |
Use a space as parity bit.
Referenced by cdc_set_line_coding().
#define USART_SUCCESS 0 |
Successful completion.
Referenced by host_cdc_task(), usart_bw_write_char(), usart_get_echo_line(), usart_init_hw_handshaking(), usart_init_IrDA(), usart_init_iso7816(), usart_init_modem(), usart_init_rs232(), usart_init_rs232_tx_only(), usart_init_rs485(), usart_init_sync_master(), usart_init_sync_slave(), usart_putchar(), usart_read_char(), usart_send_address(), usart_set_async_baudrate(), usart_set_iso7816_clock(), usart_set_sync_master_baudrate(), usart_set_sync_slave_baudrate(), and usart_write_char().
#define USART_TX_BUSY 2 |
Transmitter was busy.
Referenced by usart_write_char().
|
static |
An active wait writing a character to the USART.
usart | Base address of the USART instance. |
c | The character (up to 9 bits) to transmit. |
References USART_SUCCESS, and usart_write_char().
Referenced by usart_send_address().
|
static |
Checks if a framing error has occurred since last status reset.
usart | Base address of the USART instance. |
1
if a framing error has been detected, otherwise 0
. int usart_get_echo_line | ( | volatile avr32_usart_t * | usart | ) |
Gets and echoes characters until end of line (detected by a CR character).
usart | Base address of the USART instance. |
USART_SUCCESS | Success. |
USART_FAILURE | Low-level error detected or ETX character received. |
References USART_FAILURE, usart_getchar(), usart_putchar(), USART_SUCCESS, and usart_write_line().
int usart_getchar | ( | volatile avr32_usart_t * | usart | ) |
Waits until a character is received, and returns it.
usart | Base address of the USART instance. |
References USART_FAILURE, usart_read_char(), USART_RX_EMPTY, and USART_RX_ERROR.
Referenced by usart_get_echo_line().
int usart_init_hw_handshaking | ( | volatile avr32_usart_t * | usart, |
const usart_options_t * | opt, | ||
long | pba_hz | ||
) |
Sets up the USART to use hardware handshaking.
usart | Base address of the USART instance. |
opt | Options needed to set up RS232 communication (see usart_options_t). |
pba_hz | USART module input clock frequency (PBA clock, Hz). |
USART_SUCCESS | Mode successfully initialized. |
USART_INVALID_INPUT | One or more of the arguments is out of valid range. |
References usart_init_rs232(), USART_INVALID_INPUT, and USART_SUCCESS.
int usart_init_IrDA | ( | volatile avr32_usart_t * | usart, |
const usart_options_t * | opt, | ||
long | pba_hz, | ||
unsigned char | irda_filter | ||
) |
Sets up the USART to use the IrDA protocol.
usart | Base address of the USART instance. |
opt | Options needed to set up RS232 communication (see usart_options_t). |
pba_hz | USART module input clock frequency (PBA clock, Hz). |
irda_filter | Counter used to distinguish received ones from zeros. |
USART_SUCCESS | Mode successfully initialized. |
USART_INVALID_INPUT | One or more of the arguments is out of valid range. |
References usart_init_rs232(), USART_INVALID_INPUT, and USART_SUCCESS.
int usart_init_iso7816 | ( | volatile avr32_usart_t * | usart, |
const usart_iso7816_options_t * | opt, | ||
int | t, | ||
long | pba_hz | ||
) |
Sets up the USART to use the ISO7816 T=0 or T=1 smartcard protocols.
The receiver is enabled by default. usart_iso7816_enable_receiver and usart_iso7816_enable_transmitter can be called to change the half-duplex communication direction.
usart | Base address of the USART instance. |
opt | Options needed to set up ISO7816 communication (see usart_iso7816_options_t). |
t | ISO7816 mode to use (T=0 or T=1). |
pba_hz | USART module input clock frequency (PBA clock, Hz). |
USART_SUCCESS | Mode successfully initialized. |
USART_INVALID_INPUT | One or more of the arguments is out of valid range. |
References usart_iso7816_options_t::bit_order, usart_iso7816_options_t::dis_suc_nack, usart_iso7816_options_t::fidi_ratio, usart_iso7816_options_t::inhibit_nack, usart_iso7816_options_t::iso7816_hz, usart_iso7816_options_t::max_iterations, usart_iso7816_options_t::paritytype, USART_INVALID_INPUT, usart_iso7816_enable_receiver(), usart_reset(), usart_set_iso7816_clock(), and USART_SUCCESS.
int usart_init_modem | ( | volatile avr32_usart_t * | usart, |
const usart_options_t * | opt, | ||
long | pba_hz | ||
) |
Sets up the USART to use the modem protocol, activating dedicated inputs/outputs.
usart | Base address of the USART instance. |
opt | Options needed to set up RS232 communication (see usart_options_t). |
pba_hz | USART module input clock frequency (PBA clock, Hz). |
USART_SUCCESS | Mode successfully initialized. |
USART_INVALID_INPUT | One or more of the arguments is out of valid range. |
References usart_init_rs232(), USART_INVALID_INPUT, and USART_SUCCESS.
int usart_init_rs232 | ( | volatile avr32_usart_t * | usart, |
const usart_options_t * | opt, | ||
long | pba_hz | ||
) |
Sets up the USART to use the standard RS232 protocol.
usart | Base address of the USART instance. |
opt | Options needed to set up RS232 communication (see usart_options_t). |
pba_hz | USART module input clock frequency (PBA clock, Hz). |
USART_SUCCESS | Mode successfully initialized. |
USART_INVALID_INPUT | One or more of the arguments is out of valid range. |
References usart_options_t::baudrate, usart_options_t::channelmode, usart_options_t::charlength, usart_options_t::paritytype, usart_options_t::stopbits, USART_2_STOPBITS, USART_INVALID_INPUT, usart_reset(), usart_set_async_baudrate(), and USART_SUCCESS.
Referenced by cdc_set_line_coding(), init_dbg_rs232_ex(), usart_init_hw_handshaking(), usart_init_IrDA(), usart_init_modem(), and usart_init_rs485().
int usart_init_rs232_tx_only | ( | volatile avr32_usart_t * | usart, |
const usart_options_t * | opt, | ||
long | pba_hz | ||
) |
Sets up the USART to use the standard RS232 protocol in TX-only mode.
Compared to usart_init_rs232, this function allows very high baud rates (up to pba_hz instead of pba_hz / 8
) at the expense of full duplex.
usart | Base address of the USART instance. |
opt | Options needed to set up RS232 communication (see usart_options_t). |
pba_hz | USART module input clock frequency (PBA clock, Hz). |
USART_SUCCESS | Mode successfully initialized. |
USART_INVALID_INPUT | One or more of the arguments is out of valid range. |
1.5
stop bit is not supported in this mode. References usart_options_t::baudrate, usart_options_t::channelmode, usart_options_t::charlength, usart_options_t::paritytype, usart_options_t::stopbits, USART_2_STOPBITS, USART_INVALID_INPUT, usart_reset(), usart_set_sync_master_baudrate(), and USART_SUCCESS.
int usart_init_rs485 | ( | volatile avr32_usart_t * | usart, |
const usart_options_t * | opt, | ||
long | pba_hz | ||
) |
Sets up the USART to use the RS485 protocol.
usart | Base address of the USART instance. |
opt | Options needed to set up RS232 communication (see usart_options_t). |
pba_hz | USART module input clock frequency (PBA clock, Hz). |
USART_SUCCESS | Mode successfully initialized. |
USART_INVALID_INPUT | One or more of the arguments is out of valid range. |
References usart_init_rs232(), USART_INVALID_INPUT, and USART_SUCCESS.
int usart_init_sync_master | ( | volatile avr32_usart_t * | usart, |
const usart_options_t * | opt, | ||
long | pba_hz | ||
) |
Sets up the USART to use a synchronous RS232-like protocol in master mode.
usart | Base address of the USART instance. |
opt | Options needed to set up RS232 communication (see usart_options_t). |
pba_hz | USART module input clock frequency (PBA clock, Hz). |
USART_SUCCESS | Mode successfully initialized. |
USART_INVALID_INPUT | One or more of the arguments is out of valid range. |
References usart_options_t::baudrate, usart_options_t::channelmode, usart_options_t::charlength, usart_options_t::paritytype, usart_options_t::stopbits, USART_2_STOPBITS, USART_INVALID_INPUT, usart_reset(), usart_set_sync_master_baudrate(), and USART_SUCCESS.
int usart_init_sync_slave | ( | volatile avr32_usart_t * | usart, |
const usart_options_t * | opt, | ||
long | pba_hz | ||
) |
Sets up the USART to use a synchronous RS232-like protocol in slave mode.
usart | Base address of the USART instance. |
opt | Options needed to set up RS232 communication (see usart_options_t). |
pba_hz | USART module input clock frequency (PBA clock, Hz). |
USART_SUCCESS | Mode successfully initialized. |
USART_INVALID_INPUT | One or more of the arguments is out of valid range. |
References usart_options_t::channelmode, usart_options_t::charlength, usart_options_t::paritytype, usart_options_t::stopbits, USART_2_STOPBITS, USART_INVALID_INPUT, usart_reset(), usart_set_sync_slave_baudrate(), and USART_SUCCESS.
|
static |
Enables the ISO7816 receiver.
The ISO7816 transmitter is disabled.
usart | Base address of the USART instance. |
Referenced by usart_init_iso7816().
|
static |
Enables the ISO7816 transmitter.
The ISO7816 receiver is disabled.
usart | Base address of the USART instance. |
|
static |
Checks if an overrun error has occurred since last status reset.
usart | Base address of the USART instance. |
1
if a overrun error has been detected, otherwise 0
.
|
static |
Checks if a parity error has occurred since last status reset.
usart | Base address of the USART instance. |
1
if a parity error has been detected, otherwise 0
. int usart_putchar | ( | volatile avr32_usart_t * | usart, |
int | c | ||
) |
Sends a character with the USART.
usart | Base address of the USART instance. |
c | Character to write. |
USART_SUCCESS | The character was written. |
USART_FAILURE | The function timed out before the USART transmitter became ready to send. |
References USART_DEFAULT_TIMEOUT, USART_FAILURE, USART_SUCCESS, and usart_write_char().
Referenced by host_cdc_task(), print_char(), usart_get_echo_line(), and usart_write_line().
int usart_read_char | ( | volatile avr32_usart_t * | usart, |
int * | c | ||
) |
Checks the RX buffer for a received character, and stores it at the given memory location.
usart | Base address of the USART instance. |
c | Pointer to the where the read character should be stored (must be at least short in order to accept 9-bit characters). |
USART_SUCCESS | The character was read successfully. |
USART_RX_EMPTY | The RX buffer was empty. |
USART_RX_ERROR | An error was detected. |
References USART_RX_EMPTY, USART_RX_ERROR, USART_SUCCESS, and usart_test_hit().
Referenced by host_cdc_task(), and usart_getchar().
void usart_reset | ( | volatile avr32_usart_t * | usart | ) |
Resets the USART and disables TX and RX.
usart | Base address of the USART instance. |
References cpu_irq_disable, cpu_irq_enable, and cpu_irq_is_enabled.
Referenced by usart_init_iso7816(), usart_init_rs232(), usart_init_rs232_tx_only(), usart_init_sync_master(), and usart_init_sync_slave().
|
static |
Resets the error status.
This function resets the status bits indicating that a parity error, framing error or overrun has occurred. The RXBRK bit, indicating a start/end of break condition on the RX line, is also reset.
usart | Base address of the USART instance. |
Referenced by host_cdc_task().
int usart_send_address | ( | volatile avr32_usart_t * | usart, |
int | address | ||
) |
Addresses a receiver.
While in RS485 mode, receivers only accept data addressed to them. A packet/char with the address tag set has to precede any data. This function is used to address a receiver. This receiver should read all the following data, until an address packet addresses another receiver.
usart | Base address of the USART instance. |
address | Address of the target device. |
USART_SUCCESS | Address successfully sent (if current mode is RS485). |
USART_MODE_FAULT | Wrong operating mode. |
References usart_bw_write_char(), USART_MODE_FAULT, usart_mode_is_multidrop(), and USART_SUCCESS.
|
static |
Tests if the USART contains a received character.
usart | Base address of the USART instance. |
1
if the USART Receive Holding Register is full, otherwise 0
. Referenced by host_cdc_task(), and usart_read_char().
|
static |
Tests if all requested USART transmissions are over.
usart | Base address of the USART instance. |
1
if the USART Transmit Shift Register and the USART Transmit Holding Register are free, otherwise 0
.
|
static |
Tests if the USART is ready to transmit a character.
usart | Base address of the USART instance. |
1
if the USART Transmit Holding Register is free, otherwise 0
. Referenced by device_cdc_task(), and usart_write_char().
int usart_write_char | ( | volatile avr32_usart_t * | usart, |
int | c | ||
) |
Writes the given character to the TX buffer if the transmitter is ready.
usart | Base address of the USART instance. |
c | The character (up to 9 bits) to transmit. |
USART_SUCCESS | The transmitter was ready. |
USART_TX_BUSY | The transmitter was busy. |
References USART_SUCCESS, USART_TX_BUSY, and usart_tx_ready().
Referenced by device_cdc_task(), usart_bw_write_char(), and usart_putchar().
void usart_write_line | ( | volatile avr32_usart_t * | usart, |
const char * | string | ||
) |
Writes one character string to the USART.
usart | Base address of the USART instance. |
string | String to be written. |
References usart_putchar().
Referenced by print(), and usart_get_echo_line().