Microchip® Advanced Software Framework

usb_task.c File Reference
#include "compiler.h"
#include "intc.h"
#include "FreeRTOS.h"
#include "task.h"
#include "semphr.h"
#include "conf_usb.h"
#include "usb_drv.h"
#include "usb_task.h"
#include "cycle_counter.h"
#include "usb_descriptors.h"
#include "usb_device_task.h"
#include "usb_host_task.h"
#include "pm_uc3c.h"

Functions

U32 host_get_timeout (void)
 
void host_suspend_action (void)
 
static void usb_general_interrupt (void)
 USB interrupt routine. More...
 
static portBASE_TYPE usb_general_interrupt_non_naked (void)
 Entry point of the USB management. More...
 
void usb_suspend_action (void)
 
void usb_task (void *pvParameters)
 Entry point of the USB mamnagement. More...
 
void usb_task_init (void)
 This function initializes the USB process. More...
 

Variables

static volatile U8 g_old_usb_mode
 
volatile U16 g_usb_event = 0
 Public: U16 g_usb_event usb_connected is used to store USB events detected upon USB general interrupt subroutine Its value is managed by the following macros (See usb_task.h file) Usb_send_event(x) Usb_ack_event(x) Is_usb_event(x) Usb_clear_all_event() More...
 
volatile U8 g_usb_mode = USB_MODE_UNDEFINED
 Public: U8 g_usb_mode Used in dual-role application (both device/host) to store the current mode the USB controller is operating. More...
 
static const char log_device_disconnected [] = "Device disconnected\r\n"
 
static const char log_pin_id_changed [] = "Pin Id changed\r\n"
 
volatile U32 private_sof_counter
 Private: U8 private_sof_counter Incremented by host SOF interrupt subroutine This counter is used to detect time-out in host requests. More...
 
volatile bool usb_connected
 Public: bool usb_connected usb_connected is set to true when VBus has been detected usb_connected is set to false otherwise Used with USB_DEVICE_FEATURE == true only. More...
 
xTaskHandle usb_device_tsk
 Handle to the USB Device task. More...
 
xTaskHandle usb_host_tsk
 Handle to the USB Host task. More...
 
static xSemaphoreHandle usb_tsk_semphr = NULL
 Handle to the USB task semaphore. More...
 

static void usb_general_interrupt ( void  )
static

USB interrupt routine.

When FreeRTOS is used, the USB interrupt routine may trigger task switches, so it must use special OS prologue and epilogue. This function must be naked in order to have no stack frame. usb_general_interrupt_non_naked is therefore used for the required stack frame of the interrupt routine.

References usb_general_interrupt_non_naked().

Referenced by usb_task().

static portBASE_TYPE usb_general_interrupt_non_naked ( void  )
static

Entry point of the USB management.

Depending on the USB mode supported (HOST/DEVICE/DUAL_ROLE) the function calls the corresponding USB management function. USB interrupt routine

This function is called each time a USB interrupt occurs. The following USB DEVICE events are taken in charge:

  • VBus On / Off
  • Start-of-Frame
  • Suspend
  • Wake-Up
  • Resume
  • Reset

The following USB HOST events are taken in charge:

  • Device connection
  • Device Disconnection
  • Start-of-Frame
  • ID pin change
  • SOF (or Keep alive in low-speed) sent
  • Wake-up on USB line detected
  • Pipe events

For each event, the user can launch an action by completing the associated #define (see the conf_usb.h file to add actions on events).

Note: Only interrupt events that are enabled are processed.

Warning: If device and host tasks are not tasks in an RTOS, rough events like ID transition, VBus transition, device disconnection, etc. that need to kill then restart these tasks may lead to an undefined state if they occur just before something is activated in the USB macro (e.g. pipe/endpoint transfer...).

Returns
Nothing in the standalone configuration; a boolean indicating whether a task switch is required in the FreeRTOS configuration
Todo:
ID pin hot state change!!!
Todo:
Implement this on the silicon version

References device_state, DEVICE_UNATTACHED, S_pipe_int::enable, EVT_HOST_DISCONNECTION, EVT_HOST_HWUP, EVT_HOST_SOF, EVT_USB_DEVICE_FUNCTION, EVT_USB_HOST_FUNCTION, EVT_USB_POWERED, EVT_USB_RESET, EVT_USB_RESUME, EVT_USB_SUSPEND, EVT_USB_UNPOWERED, EVT_USB_WAKE_UP, g_old_usb_mode, g_usb_mode, S_pipe_int::handler, Host_ack_device_connection, Host_ack_device_disconnection, Host_ack_hwup, Host_ack_sof, Host_device_connection_action, Host_device_disconnection_action, host_disable_all_pipes(), Host_disable_hwup_interrupt, Host_disable_sof_interrupt, Host_get_interrupt_pipe_number, Host_get_pipe_type, Host_hwup_action, Host_reset_pipe, Host_sof_action, Is_host_attached, Is_host_device_connection, Is_host_device_connection_interrupt_enabled, Is_host_device_disconnection, Is_host_device_disconnection_interrupt_enabled, Is_host_hwup, Is_host_hwup_interrupt_enabled, Is_host_sof, Is_host_sof_interrupt_enabled, Is_usb_clock_frozen, Is_usb_device, Is_usb_full_speed_mode, Is_usb_id_device, Is_usb_id_interrupt_enabled, Is_usb_id_transition, Is_usb_reset, Is_usb_reset_interrupt_enabled, Is_usb_resume, Is_usb_resume_interrupt_enabled, Is_usb_sof, Is_usb_sof_interrupt_enabled, Is_usb_suspend, Is_usb_suspend_interrupt_enabled, Is_usb_vbus_high, Is_usb_vbus_interrupt_enabled, Is_usb_vbus_transition, Is_usb_wake_up, Is_usb_wake_up_interrupt_enabled, log_device_disconnected, log_pin_id_changed, LOG_STR, MAX_PEP_NB, pdFALSE, PIPE_DELAY_TIMEOUT, private_sof_counter, S_pipe_int::status, taskENTER_CRITICAL, taskEXIT_CRITICAL, TIMEOUT_DELAY, TYPE_INTERRUPT, Usb_ack_id_transition, Usb_ack_reset, Usb_ack_resume, Usb_ack_sof, Usb_ack_suspend, Usb_ack_vbus_transition, Usb_ack_wake_up, usb_configuration_nb, usb_connected, Usb_detach, Usb_disable, Usb_disable_otg_pad, Usb_disable_resume_interrupt, Usb_disable_wake_up_interrupt, Usb_enable_wake_up_interrupt, Usb_freeze_clock, Usb_id_transition_action, usb_init_device(), USB_MODE_DEVICE, USB_MODE_HOST, Usb_reset_action, Usb_resume_action, Usb_send_event, Usb_sof_action, usb_start_device(), Usb_suspend_action, Usb_unfreeze_clock, Usb_vbus_off_action, Usb_vbus_on_action, Usb_wake_up_action, and xSemaphoreGiveFromISR.

Referenced by usb_general_interrupt().

volatile U8 g_old_usb_mode
static
const char log_device_disconnected[] = "Device disconnected\r\n"
static
const char log_pin_id_changed[] = "Pin Id changed\r\n"
static
volatile bool usb_connected

Public: bool usb_connected usb_connected is set to true when VBus has been detected usb_connected is set to false otherwise Used with USB_DEVICE_FEATURE == true only.

Public: bool usb_connected usb_connected is set to true when VBus has been detected usb_connected is set to false otherwise Used with USB_DEVICE_FEATURE == true only.

Referenced by usb_device_task(), usb_device_task_init(), usb_general_interrupt_non_naked(), and usb_start_device().

xTaskHandle usb_device_tsk

Handle to the USB Device task.

Referenced by usb_device_task_init(), and usb_task().

xTaskHandle usb_host_tsk

Handle to the USB Host task.

Referenced by usb_host_task_init(), and usb_task().

xSemaphoreHandle usb_tsk_semphr = NULL
static

Handle to the USB task semaphore.